TI Log Tool User's Guide
Table of Contents
SimpleLink Instrumentation and Logging Kit
Introduction
This subfolder contains the host-side logger tooling, used to capture and interpret log messages. This tool supports several input/transport modules for capturing, and modules for outputting logs. A list of available log handling modules is displayed in the list below.
List of Transport and Output Modules
Transport modules
- itm
- uart
- from-replayfile
Output modules
- stdout
- wireshark (requires configuration)
- to-replayfile
Please note there is no support for Linux in this version of the logging tool. Also note that some log sinks (for example, LogSinkBuf) don’t require this host-side tool to capture and view log messages.
Quick Start Guide
This section will briefly explain the steps needed to setup and use the logger tool. For more details about each transport/output module, please refer to their respective sections in this document.
Install Python (3.8.10) from python.org, and if you want to use the Wireshark output module, install the application from wireshark.org.
Install tilogger
command line tool
The logger modules can be installed in a local “virtualenv” so that the global Python install is not affected, or it can simply be installed to the global Python library.
Note: If you have several versions of Python installed, it is important that the tilogger is run with the correct version (3.8). On Windows, this can be controlled via the py launcher. To see a list of installed versions, run py -0p
. The instructions below will assume there are multiple versions available, but will also work if only 3.8 is available.
Create and activate a venv (optional)
# Create a virtualenv (local copy of python + packages)
$ py -3.8 -m venv .venv
# Activate virtualenv.
$ .\.venv\Scripts\activate.ps1 (or .bat)
When you install to a virtualenv you must activate
it again each time you open a new command line terminal window.
Installing the tilogger
command line interface tool
If you are behind a proxy, you need to either have this configured in the global environment variables http_proxy
and https_proxy
(and no_proxy
), or you can add --proxy yourproxy.com
after install
in the pip
calls below.
Install tilogger in one of the following ways:
Installing the tilogger tool in the virtual environment
If you are using a virtual environment as created above, the py launcher should not be used to install tilogger. Use instead the following command
# Install the tilogger tool in the virtual environment created above
$ python3 -m pip install [--proxy yourproxy.com] -r requirements.txt
Installing the tilogger tool globally
If you wish to install the tilogger tool globally, change directory to <SDK_INSTALL_DIR>/tools/log/tiutils/
, and use the following command
# Install the tilogger tool in the virtual environment created above (optional)
$ py -3.8 -m pip install [--proxy yourproxy.com] -r requirements.txt
If you install globally, python
must be available on PATH for these scripts to work, and the Scripts
folder for the Python version you use to install must also be on the PATH.
After installing you can use the tilogger
command. Try it!
Using the tilogger
command line interface tool
The most up to date documentation about the options and commands is available by running tilogger --help
. Running tilogger <command> --help
will display help about the command, for example tilogger uart --help
.
$ tilogger --help
Usage: tilogger [OPTIONS] COMMAND1 [ARGS]... [COMMAND2 [ARGS]...]...
Parse LogSinkITM and LogSinkUART log output, or use replay file
functionality to store/replay log streams.
This tool may be used to instantiate a serial port parser for the ITM and
UART Log Sinks. The tool receives logs generated with the Log.h API and
reconstructs and displays the log output by using the encoded metadata in
the toolchain-generated ELF output.
A simple invocation (provided Wireshark is installed) is
tilogger --elf path/to/elf.out itm COM3 12000000 wireshark --start
Options:
--elf PATH Symbol file path (elf/out file) shared by all input
parsers [default: ]
--install-completion Install completion for the current shell.
--show-completion Show completion for the current shell, to copy it or
customize the installation.
--help Show this message and exit.
Commands:
from-replayfile Replay a sequence of logs from a replay file.
itm Add ITM transport as input to log.
stdout Add log output as standard output stream.
to-replayfile Store log outputs to a replay file.
uart Add UART transport as input to log.
wireshark Add Wireshark to log outputs.
Extracting Logs
The tools must be started in sequence:
- Start a terminal session in the
<SDK_INSTALL_DIR>/tools/log/tiutils/
folder - If using a virtual environment, run
.venv/Scripts/activate
to get into the virtual environment - Run
tilogger [transport cmd] [transport arguments] [output cmd] [output module]
to launch the logger tool with specified transport(s) and output(s).- Example for UART to stdout:
> tilogger uart --elf myelf.out COM4 3000000 stdout
- Example for UART to stdout:
- Flash your log-enabled firmware and reset the device.
You should now be capturing and interpreting log messages with the specified transport and output modules.
Please refer to each module’s respective sections in this document for specific considerations.
ELF Files Specification
Non-logging related sections from your elf.out file may be removed as they may contain sensitive information. To do this, use the utilities found in your toolchain to run the appropriate command below:
- GCC
arm-none-eabi-objcopy --only-section=.log_data --only-section=.log_ptr input.out output.out
- TICLANG and IAR projects
tiarmobjcopy --only-section=.log_data --only-section=.log_ptr input.out output.out
You can provide ELF files containing Log-string information either globally (to all transports you add) if you have just one device or if the devices run the same firmware, and you can provide the ELF files to each transport individually.
Examples
Below are more examples for launching the logger tool. These examples use uart, but itm transport is invoked in the same way.
- Listen for UART input and pipe output to stdout.
tilogger --elf myelf.out uart --alias BestDevice COM4 3000000 stdout
- Listen for UART input and pipe output to wireshark.
tilogger --elf myelf.out uart --alias BestDevice COM4 3000000 wireshark
- Listen for UART input and pipe output to wireshark, trying to start wireshark and configure it to understand the tilogger protocol.
tilogger --elf myelf.out uart --alias BestDevice COM4 3000000 wireshark --start
- Listen for ITM and UART inputs and pipe outputs to stdout.
tilogger itm --elf myelf.out COM3 12000000 uart --elf myelf.out COM4 3000000 stdout
- Start two UART listeners, each using a different log statement database, and both will be logging to the wireshark instance that is automatically started.
tilogger uart --alias dev0 --elf dev0.out COM3 3000000 uart --alias dev1 --elf dev1.out COM4 3000000 wireshark --start
Transport Modules
ITM Transport
$ tilogger itm --help
Usage: tilogger itm [OPTIONS] PORT BAUDRATE
Add ITM transport as input to log.
You need to specify a serial port and a baudrate (ITM driver module
configures this). The baudrate is often quite high, such as 12000000
(12MHz).
You also need to specify .out/.elf files that contain symbol information
needed to parse the log, but this may also be provided globally before
adding transports.
Arguments:
PORT Serial port (eg COM12) [required]
BAUDRATE TPIU baudrate [required]
Options:
--elf PATH Symbol file path (elf/out file) [default: ]
--alias TEXT Alias for this device in the log
--help Show this message and exit.
ITM Transport Considerations
Use Device Manager to choose the correct COM port.
Be aware that when when using XDS110 Debug Probe you must use the “Auxiliary Data Port”.
tilogger
will not begin recording until it has seen a reset frame, which is only generated on startup.
Viewing RAW ITM Streams
The tilogger_itm_transport
package also provides a raw ITM viewer, which can for example support the use of TI’s ITM
driver directly. Follow the setup guidelines above to create an environment and install the ITM package. You can ignore any instructions for Wireshark.
The command line for the ITM viewer is > tilogger_itm_viewer [COM PORT] [BAUDRATE]
. Example: > tilogger_itm_viewer COM5 115200
UART Transport
$ tilogger uart --help
Usage: tilogger uart [OPTIONS] PORT BAUDRATE
Add UART transport as input to log.
You need to specify a serial port and a baudrate (UART LogSink module
configures this). The baudrate is often quite high, such as 3000000
(3 MHz).
You also need to specify .out/.elf files that contain symbol information
needed to parse the log, but this may also be provided globally before
adding transports.
Arguments:
PORT Serial port (eg COM11) [required]
BAUDRATE UART baudrate [required]
Options:
--elf PATH Symbol file path (elf/out file) [default: ]
--alias TEXT Alias for this device in the log
--help Show this message and exit.
UART Transport Considerations
Use Device Manager to choose the correct COM port.
Be aware that when when using XDS110 Debug Probe you must use the “Application/User UART”.
Waiting for a reset frame is not necessary for UART transport, in this case
tilogger
can attach to a running data stream.
From Replay File Transport
$ tilogger from-replayfile --help
Usage: tilogger from-replayfile [OPTIONS] FILE
Replay a sequence of logs from a replay file.
You need to specify path to a replay file (JSON file) and an output mode
(stdout or wireshark).
A simple invocation that loads from replay file and outputs to stdout is
tilogger from-replayfile path/to/replayFile.json stdout
Arguments:
FILE Replay file path (JSON file) [required]
Options:
--help Show this message and exit.
Replay File Transport Considerations
- Providing an
--elf
argument is not necessary when using replay file transport. The replay file already contains the parsed log messages.
Output Modules
Stdout Output
$ tilogger stdout --help
Usage: tilogger stdout [OPTIONS]
Add log output as standard output stream.
If custom format is wanted, use --format "<FORMAT_SPEC>" with desired
format specifiers.
Supported Specifiers
{I}: Identifier (for example COM7, or the provided alias)
{T}: Timestamp
{M}: Module (for example LogMod_App1)
{L}: Log level (for example Log_INFO)
{F}: File and line number (for example path/log.c:134)
{D}: Log data
Options:
-f, --format TEXT [default: "{I} | {T} | {M} | {L} | {F} | {D}"]
--disable-column-alignment Disable dynamic column alignment
--help Show this message and exit.
Wireshark Output
Configuration of Wireshark is needed for the logs to be displayed correctly. See Configure Wireshark.
$ tilogger wireshark --help
Usage: tilogger wireshark [OPTIONS]
Add Wireshark to log outputs.
If you don't want to start wireshark via this tool you must configure it
manually
Open Capture -> Options -> Manage Interfaces -> Pipes -> +, then type in
`\\.\pipe\tilogger-wireshark` or your own choice of pipe name.
Add protocol parsing via Edit -> Preferences -> Protocols -> DLT_USER ->
Edit..., then add new row for DLT=147 and use `tilogger` as payload
protocol.
Options:
-s, --start [default: False]
--pipe TEXT [default: \\.\pipe\tilogger-wireshark]
--help Show this message and exit.
Configure Wireshark
Copy streams/wireshark/tilog_dissector.lua
to [Wireshark install dir]/plugins/x.y/tilogger_dissector.lua
. This will teach Wireshark to understand the TI Logger’s packet format.
Warning: If you have previously used an older version of the TI logger tool, make sure to remove the previous
dissector.lua
containing the old TI Logger from Wireshark.
To automatically start wireshark when starting the logger, supply --start
to the wireshark
command. tilogger
adds columns to the default view for Filename, Line-number, Level, Module and Format string. To modify these or add new columns, right click the column headers and choose Column Preferences
. Note that the field type should be ‘Custom’.
This has been tested with Wireshark 3.4.x, but should work with later versions as well.
To Replay File Output
$ tilogger to-replayfile --help
Usage: tilogger to-replayfile [OPTIONS]
Store log outputs to a replay file.
You need to specify path to a JSON file. A replay file will be generated
by storing the captured LogPackets in the specified JSON file. If a path
to an existing JSON file is provided, the file will be overwritten.
A invocation storing an ITM stream parsed with the provided ELF file to
replayfile.json:
tilogger --elf path/to/elf.out itm COM6 12000000 to-replayfile --file
path/to/replayfile.json
To replay the log events, use
tilogger from-replayfile <FILE> <OUTPUT>
Options:
--file TEXT Replay file path (JSON file) [required]
--verbose Print updates in terminal while writing to file
--help Show this message and exit.
User format modules
User format modules are functional in this beta, but there are no examples provided. You will need to create a Python package with a class that inherits from one of the abstract base classes (ABCs) in core/tilogger/interface.py
. Your package must register an entry point (this is documented in the interface classes). If placed in a subfolder of modules/, it will be installed into the virtual environment automatically when you call one of the setup scripts.