46 #ifndef EXT_FLASH_LAYOUT_H 47 #define EXT_FLASH_LAYOUT_H 67 #define OAD_EFL_MAGIC \ 69 'O', 'A', 'D', ' ', 'N', 'V', 'M', '1' \ 76 #define OAD_EFL_MAGIC_SZ 8 82 #define EFL_ADDR_META 0x00000 88 #define EFL_SIZE_META EFL_PAGE_SIZE 94 #define EFL_META_PG_INVALID 0xFF 100 #define EFL_FACT_IMG_META_PG 0 105 #define EFL_ADDR_META_FACT_IMG EFL_ADDR_META 110 #define EFL_META_COPY_SZ offsetof(ExtImageInfo_t, fixedHdr.rfu) + sizeof(((ExtImageInfo_t){0}).fixedHdr.rfu) 115 #define EFL_METADATA_LEN sizeof(ExtImageInfo_t) 121 #define EFL_IMG_STR_ADDR_OFFSET offsetof(ExtImageInfo_t, extFlAddr) 126 #define EFL_META_COUNTER_OFFSET offsetof(ExtImageInfo_t, counter) 132 TYPEDEF_STRUCT_PACKED
imgFixedHdr_t fixedHdr
This is the core image header.
Definition: ext_flash_layout.h:134
Definition: oad_image_header.h:689
uint32_t extFlAddr
Location of the image in ext flash.
Definition: ext_flash_layout.h:135
Definition: ext_flash_layout.h:132
uint32_t counter
Timestamp/counter of image.
Definition: ext_flash_layout.h:136