Zigbee Coordinator Thermostat Sink Example App
- Introduction
- Hardware Prerequisites
- Software Prerequisites
- Functional Description
- Configuration With SysConfig
- Example Usage
Introduction
This document discusses how to use the Zigbee Thermostat Example App and the different parts that compose it. Zigbee Thermostat Application is an example which exercises different features of TI Z-Stack. This example has the same behavior as the Zigbee Thermostat but with addition of Green Power (GP) Sink functionality to process Green Power Device Temperature Sensor commands.
Some of the features exercised include:
- Base Device Behavior attribute configuration.
- Green Power Sink functionality enabled for a temperature sensor application.
- Thermostat device that acts as Target of Finding and Binding.
- Receive and process Attribute reports.
Hardware Prerequisites
- The Launchpad which is used by this particular project.
Software Prerequisites
Code Composer Studio™ (CCS) v10.3 or newer
Functional Description
Software Overview
This section describes the software components and the corresponding source files.
Application Files
- zcl_samplethermostat.c/.h: Contains the application's event loop, device initialization function calls (for timers, peripherals, Nvm, LEDs, Switches, Serial interface), Zigbee stack notifications and all thermostat specific logic.
- zcl_samplethermostat_data.c: Contains the endpoint, cluster and attribute definitions for this sample application.
- main.c: Defines the application task and the application stack size.
- bdb_interface.h: Defines commissioning parameters to be used and configured in the application upon calling commissioning methods (see zclSampleThermostat_initParameters()).
Configuration With SysConfig
SysConfig is a GUI configuration tool that allows for TI driver and stack configurations.
To configure using SysConfig, import the SysConfig-enabled project into CCS. Double click the *.syscfg file from the CCS project explorer, where * is the name of the example project. The SysConfig GUI window will appear, where Zigbee stack and TI driver configurations can be adjusted. These settings will be reflected in the generated files.
The example project comes with working default settings for SysConfig. For the purposes of this README, it is not recommended to change the default driver settings, as any changes may impact the functionality of the example. The Zigbee stack settings may be changed as required for your use case.
Note that some Z-Stack settings are stored in non-volatile storage, and Z-Stack prioritizes stored settings over SysConfig settings. To guarantee SysConfig settings are applied, perform a factory reset of the device to clear non-volatile storage.
Example Usage
This section describes how to use this sample application.
Buttons
BTN-1: Starts the commissioning process.BTN-2: If hold after reset, perform Factory New reset (erase network and application persistent data)
LEDs
DIO6: Reflects the state of the Heating/Cooling system mode. When LED is On, the system is currently in Heating mode. When LED is Blinking, the system is currently in Cooling mode. When LED is Off, the system is shut off.
Serial interface
- Open a serial session (e.g. PuTTY, etc.) to the appropriate COM port.
- The COM port can be determined via Device Manager in Windows or via
ls /dev/tty*in Linux.
- The COM port can be determined via Device Manager in Windows or via
The connection will have the following settings:
Baud-rate: 115200
Data bits: 8
Stop bits: 1
Parity: None
Flow Control: None
Note: The serial output is known to be formatted incorrectly in Tera Term and in the CCS Terminal.
The serial interface allows you to control the commissioning configuration as well as application behavior. The commissioning interface is common for all applications and is implemented in the module zcl_sampleapps_ui.c/.h. Any application specific behavior of the serial interface is implemented in the example application files.
The serial interface implements a common set of menus described in 'Application Overview' within the Zigbee docs in this SDK. This common menu can be used to commission the device into a network.
Commissioning the Device Into the Network
Zigbee coordinators can only create networks and other devices must join the network. This is done using the common interface by enabling Formation Mode and executing the commissioning process in the Commissioning Screen. This sample application uses the stack notifications (zstackmsg_CmdIDs_BDB_NOTIFICATION) on a successful network formation process to open the network and allow new devices to join, even if the Steering Mode is not enabled from the common user interface. If the network is closed, it can be opened again by enabling the Steering Mode and executing the commissioning process in the Commissioning Screen.
Interfacing with the Green Power Device Temperature Sensor Example App
Once the Thermostat Sink and another routing device are in the same network, put the Thermostat Sink in GP Commissioning Mode from the App Menu in the Green Power Sink Commissioning Screen. Executing this screen will change the GPS Commissioning status from 'DISABLED' to 'ENABLED'
Send the Commissioning GPDF from the Green Power Device Temperature Sensor. Then from the Green Power Sink Commissioning Screen disable the GP commissioning mode.
Once the GP commissioning mode is disabled, sending the Attribute Reporting GPDF with the Green Power Device Temperature Sensor will update the remote temperature value in the application status line.
NOTE: If the temperature is not updated just repeat the commissioning process and try again.
Interfacing with the Temperature Sensor Example App
Once the Temperature Sensor and Thermostat are in the same network, enable the Finding and Binding Mode and execute it from the Commissioning Screen. When Finding and Binding is executed, the Thermostat device is set in Identify mode for 180 seconds. During this time the Temperature Sensor device must perform Finding and Binding as well to find the Thermostat device in Identify mode and create a bind to it. The status of the Identify process is shown in the BDB status line.
Finding and binding status in the BDB status line
IdXXX shows the remaining XXX seconds in Identify mode, SrchYYY/ZZ shows the remaining YYY seconds searching for devices in Identify mode and ZZ the number of binds created during this process.
Once the Temperature Sensor device has the bind to the Thermostat, it will periodically send Reporting Attribute commands according to the reporting configuration set by Zstackapi_bdbRepAddAttrCfgRecordDefaultToListReq(). The Thermostat will process those reporting attributes by updating zclSampleThermostat_LocalTemperature (which is actually the temperature of the remote device) which will also be displayed in the application status line.
Remote temperature received screen in Thermostat device
Note: The temperature displayed by Remote Temperature may lie (inclusively) between SAMPLETEMPERATURESENSOR_MIN_MEASURED_VALUE and SAMPLETEMPERATURESENSOR_MAX_MEASURED_VALUE (these values are defined in zcl_sampletemperaturesensor_data.c).
The temperature reported will also control the state of the heating and cooling system of the Thermostat device as described in LEDs section. The state of the heating cooling system is also displayed at the end of the application status line. The heating and cooling set point can be set in the Application menu of the user interface:
Heating setpoint screen in Thermostat device
Cooling setpoint screen in Thermostat device