BLE5-Stack 1.01.00 to BLE5-Stack 1.01.02¶
This section will describe a way to migrate a project from BLE5-Stack 1.01.00 to a BLE5-Stack 1.01.02 project.
For this migration guide, simple_peripheral from BLE5-Stack 1.01.00 will be ported over to BLE5-Stack 1.01.02. Because the directory structure is nearly identical between the two releases, the recommended approach is to start with a BLE5-Stack 1.01.02 project that contains the same base functionality as the porting target project and merge in any custom functionality.
Choose a BLE5-Stack 1.01.02 example project that contains your target project’s base functionality.
For reference, see available sample projects that start with simple_
In this example, we’re going to use simple_peripheral as the starting BLE5-Stack 1.01.02 sample project.
Transfer all modified application files from BLE5-Stack 1.01.00 into the BLE5-Stack 1.01.02 example project.
In this example, the following files from BLE5-Stack 1.01.00 were moved into simple_peripheral BLE5-Stack 1.01.02 example:
simple_peripheral.c
simple_peripheral.h
simple_gatt_profile.c
simple_gatt_profile.h
Modify
main.c
in the BLE5-Stack 1.01.02 example if additional tasks were added in the BLE5-Stack 1.01.00 project.Note that address mode and random address are now set from
GAP_DeviceInit
The
GAP_DeviceInit()
function now includes parameters for setting the address mode and for setting a pointer to a random address when that mode is used./** * GAP Device Initialization * * Setup the device. Can only be called once per reset. In order to change * the address mode / random address, it is necessary to reset the device * and call this API again. In the case where the address mode or random address * is different than it was for the last initialization, all bonds and local * information stored in NV will be erased. * * @par Corresponding Events: * @ref GAP_DEVICE_INIT_DONE_EVENT of type @ref gapDeviceInitDoneEvent_t * * @param profileRole GAP Profile Roles: @ref GAP_Profile_Roles * @param taskID end application task to receive unprocessed GAP events. * @param addrMode Own address mode. If always using Resolvable Private Address, * set this to either @ref ADDRMODE_RP_WITH_PUBLIC_ID or * @ref ADDRMODE_RP_WITH_RANDOM_ID. If always using Identity * Address, set this to either @ref ADDRMODE_PUBLIC or * @ref ADDRMODE_RANDOM. * @param pRandomAddr Pointer to 6-byte Random Static Address of this device * that will be copied to the stack. Valid only if addrMode * is @ref ADDRMODE_RANDOM or @ref ADDRMODE_RP_WITH_RANDOM_ID and can * not be NULL in these cases. Ignored for other address types. * * @return @ref SUCCESS : initialization started * @return @ref INVALIDPARAMETER : invalid profile role, role combination, * or invalid Random Static Address, * @return @ref bleIncorrectMode : initialization has already occurred * @return @ref bleInternalError : error erasing NV */ extern bStatus_t GAP_DeviceInit(uint8_t profileRole, uint8_t taskID, GAP_Addr_Modes_t addrMode, uint8_t* pRandomAddr);
Any calls to
GAP_DeviceInit()
should be modified to pass a parameter addrMode of typeGAP_Addr_Modes_t
.// Address mode of the local device #define DEFAULT_ADDRESS_MODE ADDRMODE_PUBLIC
// Address mode static GAP_Addr_Modes_t addrMode = DEFAULT_ADDRESS_MODE;
//Initialize GAP layer for Peripheral role and register to receive GAP events GAP_DeviceInit(GAP_PROFILE_PERIPHERAL, selfEntity, addrMode, NULL);
Additionally, remove all code using
GAP_ConfigDeviceAddr()
because the address mode and random address are now only able to be set fromGAP_DeviceInit()
.GAP_DeviceInit()
can only be called once after a reset, so any functions related to change the address mode on the fly should be removed.Removal of HCI Extension notice commands:
- The following HCI Extension commands have been removed:
HCI_EXT_ConnEventNoticeCmd()
HCI_EXT_AdvEventNoticeCmd()
HCI_EXT_ScanEventNoticeCmd()
HCI_EXT_ScanReqRptCmd()
Any calls to these commands should be removed as well as references to events related to these commands.
For
HCI_EXT_ConnEventNoticeCmd()
,Gap_RegisterConnEventCb
is now provided as an option instead as a way to handle connection events.If necessary, update the project to use the newer TI-RTOS drivers that are supplied with the SimpleLink CC2640R2 SDK.
The following drivers have changed from BLE5-Stack 1.01.00. Please see the changes to these drivers by comparing the supplied headers between them in simplelink_cc2640r2_sdk_1_50_00_71 and those in the SimpleLink CC2640R2 SDK.
- LCD: Driver is found in source/ti/display/lcd instead of previous ti/mw/lcd/
Refer to the Upgrade and Compatibility Information for additional information and the TI-RTOS examples included with SimpleLink CC2640R2 SDK.
For additional information on how BLE5-Stack 1.01.02 uses TI-RTOS see TI-RTOS (RTOS Kernel) Overview
For any utilized TI Drivers, review TI-RTOS Kernel Users Guide and Driver APIs.