TI BLE-Stack for Bluetooth API Documentation  3.03.03.00
hci_tl.h
Go to the documentation of this file.
1 /******************************************************************************
2 
3  Group: WCS, BTS
4  $Target Device: DEVICES $
5 
6  ******************************************************************************
7  $License: TISD 2009 $
8  ******************************************************************************
9  $Release Name: PACKAGE NAME $
10  $Release Date: PACKAGE RELEASE DATE $
11  *****************************************************************************/
12 
21 #ifndef HCI_TL_H
22 #define HCI_TL_H
23 
24 #ifdef __cplusplus
25 extern "C"
26 {
27 #endif
28 
29 /*******************************************************************************
30  * INCLUDES
31  */
32 
33 #include "hci.h"
34 #include "osal.h"
35 #include "hci_data.h"
36 #include "hci_event.h"
37 
39 extern uint8 hciTaskID;
40 extern uint8 hciTestTaskID;
41 extern uint8 hciGapTaskID;
42 extern uint8 hciL2capTaskID;
43 extern uint8 hciSmpTaskID;
45 
46 /*******************************************************************************
47  * MACROS
48  */
49 
51 #define HCI_ASSERT(condition) HAL_ASSERT(condition)
52  // end of HCI
54 
55 /*******************************************************************************
56  * CONSTANTS
57  */
58 
64 // OSAL Task Events
65 #define HCI_TX_PROCESS_EVENT 0x0001
66 #define HCI_TEST_UART_SEND_EVENT 0x0002
67 #define HCI_ADV_NOTICE_EVENT 0x0004
68 #define HCI_SCAN_NOTICE_EVENT 0x0008
69 #define HCI_BDADDR_UPDATED_EVENT 0x4000
70 
71 // OSAL Message Header Events
72 #define HCI_CTRL_TO_HOST_EVENT 0x01
73 #define HCI_HOST_TO_CTRL_CMD_EVENT 0x02
74 #define HCI_HOST_TO_CTRL_DATA_EVENT 0x03
75 
76 #define HCI_BDADDR_LEN 6
77 
78 // Max Allowed HCI Packet
79 #define HCI_MAX_CMD_PKT_SIZE 0xFF
80 #define HCI_MAX_DATA_PKT_SIZE 0xFFFF
81 
82 // Max Data Length in Packet
83 #define HCI_DATA_MAX_DATA_LENGTH 27
84 
85 
91 #define HCI_CMD_MIN_LENGTH 4
92 
99 #define HCI_EVENT_MIN_LENGTH 3
100 
101 
108 #define HCI_DATA_MIN_LENGTH 5
109 
110 #define HCI_MAX_NUM_CONNECTIONS 0x03
111 
112 #define HCI_TX_DATA_ANY_CONNECTION 0xFF
113 
114 // HCI Packet Types
115 #define HCI_CMD_PACKET 0x01
116 #define HCI_ACL_DATA_PACKET 0x02
117 #define HCI_SCO_DATA_PACKET 0x03
118 #define HCI_EVENT_PACKET 0x04
119 
120 
121 // States for Command and Data packet parser
122 #define HCI_PARSER_STATE_PKT_TYPE 0
123 #define HCI_CMD_PARSER_STATE_OPCODE 1
124 #define HCI_CMD_PARSER_STATE_LENGTH 2
125 #define HCI_CMD_PARSER_STATE_DATA 3
126 #define HCI_DATA_PARSER_STATE_HANDLE 4
127 #define HCI_DATA_PARSER_STATE_LENGTH 5
128 #define HCI_DATA_PARSER_STATE_DATA 6
129 
130 // HCI Command Subgroup
131 #define HCI_OPCODE_CSG_LINK_LAYER 0
132 #define HCI_OPCODE_CSG_CSG_L2CAP 1
133 #define HCI_OPCODE_CSG_CSG_ATT 2
134 #define HCI_OPCODE_CSG_CSG_GATT 3
135 #define HCI_OPCODE_CSG_CSG_GAP 4
136 #define HCI_OPCODE_CSG_CSG_SM 5
137 #define HCI_OPCODE_CSG_CSG_Reserved 6
138 #define HCI_OPCODE_CSG_CSG_USER_PROFILE 7
139 
140 // Vendor Specific OGF
141 #define VENDOR_SPECIFIC_OGF 0x3F
142 
143 /*
144 ** HCI Command Opcodes
145 */
146 
147 // Link Control Commands
148 #define HCI_DISCONNECT 0x0406
149 #define HCI_READ_REMOTE_VERSION_INFO 0x041D
150 
151 // Controller and Baseband Commands
152 #define HCI_SET_EVENT_MASK 0x0C01
153 #define HCI_RESET 0x0C03
154 #define HCI_READ_TRANSMIT_POWER 0x0C2D
155 #define HCI_SET_CONTROLLER_TO_HOST_FLOW_CONTROL 0x0C31
157 #define HCI_HOST_BUFFER_SIZE 0x0C33
158 #define HCI_HOST_NUM_COMPLETED_PACKETS 0x0C35
160 #define HCI_SET_EVENT_MASK_PAGE_2 0x0C63
161 #define HCI_READ_AUTH_PAYLOAD_TIMEOUT 0x0C7B
162 #define HCI_WRITE_AUTH_PAYLOAD_TIMEOUT 0x0C7C
163 
164 // Information Parameters
165 #define HCI_READ_LOCAL_VERSION_INFO 0x1001
166 #define HCI_READ_LOCAL_SUPPORTED_COMMANDS 0x1002
167 #define HCI_READ_LOCAL_SUPPORTED_FEATURES 0x1003
168 #define HCI_READ_BDADDR 0x1009
169 
170 // Status Parameters
171 #define HCI_READ_RSSI 0x1405
172 
173 // LE Commands
174 // V4.0
175 #define HCI_LE_SET_EVENT_MASK 0x2001
176 #define HCI_LE_READ_BUFFER_SIZE 0x2002
177 #define HCI_LE_READ_LOCAL_SUPPORTED_FEATURES 0x2003
178 #define HCI_LE_SET_RANDOM_ADDR 0x2005
179 #define HCI_LE_SET_ADV_PARAM 0x2006
180 #define HCI_LE_READ_ADV_CHANNEL_TX_POWER 0x2007
181 #define HCI_LE_SET_ADV_DATA 0x2008
182 #define HCI_LE_SET_SCAN_RSP_DATA 0x2009
183 #define HCI_LE_SET_ADV_ENABLE 0x200A
184 #define HCI_LE_SET_SCAN_PARAM 0x200B
185 #define HCI_LE_SET_SCAN_ENABLE 0x200C
186 #define HCI_LE_CREATE_CONNECTION 0x200D
187 #define HCI_LE_CREATE_CONNECTION_CANCEL 0x200E
188 #define HCI_LE_READ_WHITE_LIST_SIZE 0x200F
189 #define HCI_LE_CLEAR_WHITE_LIST 0x2010
190 #define HCI_LE_ADD_WHITE_LIST 0x2011
191 #define HCI_LE_REMOVE_WHITE_LIST 0x2012
192 #define HCI_LE_CONNECTION_UPDATE 0x2013
193 #define HCI_LE_SET_HOST_CHANNEL_CLASSIFICATION 0x2014
194 #define HCI_LE_READ_CHANNEL_MAP 0x2015
195 #define HCI_LE_READ_REMOTE_USED_FEATURES 0x2016
196 #define HCI_LE_ENCRYPT 0x2017
197 #define HCI_LE_RAND 0x2018
198 #define HCI_LE_START_ENCRYPTION 0x2019
199 #define HCI_LE_LTK_REQ_REPLY 0x201A
200 #define HCI_LE_LTK_REQ_NEG_REPLY 0x201B
201 #define HCI_LE_READ_SUPPORTED_STATES 0x201C
202 #define HCI_LE_RECEIVER_TEST 0x201D
203 #define HCI_LE_TRANSMITTER_TEST 0x201E
204 #define HCI_LE_TEST_END 0x201F
205 // V4.1
206 #define HCI_LE_REMOTE_CONN_PARAM_REQ_REPLY 0x2020
207 #define HCI_LE_REMOTE_CONN_PARAM_REQ_NEG_REPLY 0x2021
208 // V4.2
209 #define HCI_LE_SET_DATA_LENGTH 0x2022
210 #define HCI_LE_READ_SUGGESTED_DEFAULT_DATA_LENGTH 0x2023
211 #define HCI_LE_WRITE_SUGGESTED_DEFAULT_DATA_LENGTH 0x2024
212 #define HCI_LE_READ_LOCAL_P256_PUBLIC_KEY 0x2025
213 #define HCI_LE_GENERATE_DHKEY 0x2026
214 #define HCI_LE_ADD_DEVICE_TO_RESOLVING_LIST 0x2027
215 #define HCI_LE_REMOVE_DEVICE_FROM_RESOLVING_LIST 0x2028
216 #define HCI_LE_CLEAR_RESOLVING_LIST 0x2029
217 #define HCI_LE_READ_RESOLVING_LIST_SIZE 0x202A
218 #define HCI_LE_READ_PEER_RESOLVABLE_ADDRESS 0x202B
219 #define HCI_LE_READ_LOCAL_RESOLVABLE_ADDRESS 0x202C
220 #define HCI_LE_SET_ADDRESS_RESOLUTION_ENABLE 0x202D
221 #define HCI_LE_SET_RESOLVABLE_PRIVATE_ADDRESS_TIMEOUT 0x202E
222 #define HCI_LE_READ_MAX_DATA_LENGTH 0x202F
223 
224 // V5.0
226 #define HCI_LE_READ_PHY 0x2030
227 #define HCI_LE_SET_DEFAULT_PHY 0x2031
228 #define HCI_LE_SET_PHY 0x2032
229 #define HCI_LE_ENHANCED_RECEIVER_TEST 0x2033
230 #define HCI_LE_ENHANCED_TRANSMITTER_TEST 0x2034
231 // LE Vendor Specific LL Extension Commands
233 #define HCI_EXT_SET_RX_GAIN 0xFC00
234 #define HCI_EXT_SET_TX_POWER 0xFC01
235 #define HCI_EXT_ONE_PKT_PER_EVT 0xFC02
236 #define HCI_EXT_CLK_DIVIDE_ON_HALT 0xFC03
238 #define HCI_EXT_DECLARE_NV_USAGE 0xFC04
239 #define HCI_EXT_DECRYPT 0xFC05
241 #define HCI_EXT_SET_LOCAL_SUPPORTED_FEATURES 0xFC06
242 #define HCI_EXT_SET_FAST_TX_RESP_TIME 0xFC07
243 #define HCI_EXT_MODEM_TEST_TX 0xFC08
244 #define HCI_EXT_MODEM_HOP_TEST_TX 0xFC09
245 #define HCI_EXT_MODEM_TEST_RX 0xFC0A
246 #define HCI_EXT_END_MODEM_TEST 0xFC0B
247 #define HCI_EXT_SET_BDADDR 0xFC0C
248 #define HCI_EXT_SET_SCA 0xFC0D
249 #define HCI_EXT_ENABLE_PTM 0xFC0E
250 #define HCI_EXT_SET_FREQ_TUNE 0xFC0F
251 #define HCI_EXT_SAVE_FREQ_TUNE 0xFC10
252 #define HCI_EXT_SET_MAX_DTM_TX_POWER 0xFC11
253 #define HCI_EXT_MAP_PM_IO_PORT 0xFC12
255 #define HCI_EXT_DISCONNECT_IMMED 0xFC13
257 #define HCI_EXT_PER 0xFC14
258 #define HCI_EXT_PER_BY_CHAN 0xFC15
259 #define HCI_EXT_EXTEND_RF_RANGE 0xFC16
261 #define HCI_EXT_ADV_EVENT_NOTICE 0xFC17
263 #define HCI_EXT_HALT_DURING_RF 0xFC19
265 #define HCI_EXT_OVERRIDE_SL 0xFC1A
267 #define HCI_EXT_BUILD_REVISION 0xFC1B
268 #define HCI_EXT_DELAY_SLEEP 0xFC1C
270 #define HCI_EXT_RESET_SYSTEM 0xFC1D
272 #define HCI_EXT_OVERLAPPED_PROCESSING 0xFC1E
274 #define HCI_EXT_NUM_COMPLETED_PKTS_LIMIT 0xFC1F
276 #define HCI_EXT_GET_CONNECTION_INFO 0xFC20
277 #define HCI_EXT_SET_MAX_DATA_LENGTH 0xFC21
278 #define HCI_EXT_SCAN_EVENT_NOTICE 0xFC22
279 #define HCI_EXT_SCAN_REQ_REPORT 0xFC23
280 #define HCI_EXT_GET_ACTIVE_CONNECTION_INFO 0xFC24
281 
282 #define HCI_EXT_LL_TEST_MODE 0xFC70
284 
286 /*
287 ** HCI Event Codes
288 */
289 
290 // BT Events
291 #define HCI_DISCONNECTION_COMPLETE_EVENT_CODE 0x05
292 #define HCI_ENCRYPTION_CHANGE_EVENT_CODE 0x08
293 #define HCI_READ_REMOTE_INFO_COMPLETE_EVENT_CODE 0x0C
294 #define HCI_COMMAND_COMPLETE_EVENT_CODE 0x0E
295 #define HCI_COMMAND_STATUS_EVENT_CODE 0x0F
296 #define HCI_BLE_HARDWARE_ERROR_EVENT_CODE 0x10
297 #define HCI_NUM_OF_COMPLETED_PACKETS_EVENT_CODE 0x13
298 #define HCI_DATA_BUFFER_OVERFLOW_EVENT 0x1A
299 #define HCI_KEY_REFRESH_COMPLETE_EVENT_CODE 0x30
300 #define HCI_APTO_EXPIRED_EVENT_CODE 0x57
301 
302 // LE Event Code (for LE Meta Events)
303 #define HCI_LE_EVENT_CODE 0x3E
304 
305 // LE Meta Event Codes
306 #define HCI_BLE_CONNECTION_COMPLETE_EVENT 0x01
307 #define HCI_BLE_ADV_REPORT_EVENT 0x02
308 #define HCI_BLE_CONN_UPDATE_COMPLETE_EVENT 0x03
309 #define HCI_BLE_READ_REMOTE_FEATURE_COMPLETE_EVENT 0x04
310 #define HCI_BLE_LTK_REQUESTED_EVENT 0x05
311 // V4.1
312 #define HCI_BLE_REMOTE_CONN_PARAM_REQUEST_EVENT 0x06
313 // V4.2
314 #define HCI_BLE_DATA_LENGTH_CHANGE_EVENT 0x07
315 #define HCI_BLE_READ_LOCAL_P256_PUBLIC_KEY_COMPLETE_EVENT 0x08
316 #define HCI_BLE_GENERATE_DHKEY_COMPLETE_EVENT 0x09
317 #define HCI_BLE_ENHANCED_CONNECTION_COMPLETE_EVENT 0x0A
318 #define HCI_BLE_DIRECT_ADVERTISING_REPORT_EVENT 0x0B
319 // V5.0
320 #define HCI_BLE_PHY_UPDATE_COMPLETE_EVENT 0x0C
321 // VS Meta Event Codes - Texas Instruments Inc specific!
322 #define HCI_BLE_SCAN_REQ_REPORT_EVENT 0x80
323 #define HCI_BLE_CHANNEL_MAP_UPDATE_EVENT 0x81
324 
325 #define HCI_VE_EVENT_CODE 0xFF
326 
327 // LE Vendor Specific LL Extension Events
328 #define HCI_EXT_SET_RX_GAIN_EVENT 0x0400
329 #define HCI_EXT_SET_TX_POWER_EVENT 0x0401
330 #define HCI_EXT_ONE_PKT_PER_EVT_EVENT 0x0402
331 #define HCI_EXT_CLK_DIVIDE_ON_HALT_EVENT 0x0403
333 #define HCI_EXT_DECLARE_NV_USAGE_EVENT 0x0404
334 #define HCI_EXT_DECRYPT_EVENT 0x0405
336 #define HCI_EXT_SET_LOCAL_SUPPORTED_FEATURES_EVENT 0x0406
337 #define HCI_EXT_SET_FAST_TX_RESP_TIME_EVENT 0x0407
338 #define HCI_EXT_MODEM_TEST_TX_EVENT 0x0408
339 #define HCI_EXT_MODEM_HOP_TEST_TX_EVENT 0x0409
340 #define HCI_EXT_MODEM_TEST_RX_EVENT 0x040A
341 #define HCI_EXT_END_MODEM_TEST_EVENT 0x040B
342 #define HCI_EXT_SET_BDADDR_EVENT 0x040C
343 #define HCI_EXT_SET_SCA_EVENT 0x040D
344 #define HCI_EXT_ENABLE_PTM_EVENT 0x040E
345 #define HCI_EXT_SET_FREQ_TUNE_EVENT 0x040F
346 #define HCI_EXT_SAVE_FREQ_TUNE_EVENT 0x0410
347 #define HCI_EXT_SET_MAX_DTM_TX_POWER_EVENT 0x0411
348 #define HCI_EXT_MAP_PM_IO_PORT_EVENT 0x0412
350 #define HCI_EXT_DISCONNECT_IMMED_EVENT 0x0413
352 #define HCI_EXT_PER_EVENT 0x0414
353 #define HCI_EXT_PER_BY_CHAN_EVENT 0x0415
354 #define HCI_EXT_EXTEND_RF_RANGE_EVENT 0x0416
356 #define HCI_EXT_ADV_EVENT_NOTICE_EVENT 0x0417
358 #define HCI_EXT_HALT_DURING_RF_EVENT 0x0419
360 #define HCI_EXT_OVERRIDE_SL_EVENT 0x041A
361 #define HCI_EXT_BUILD_REVISION_EVENT 0x041B
363 #define HCI_EXT_DELAY_SLEEP_EVENT 0x041C
365 #define HCI_EXT_RESET_SYSTEM_EVENT 0x041D
367 #define HCI_EXT_OVERLAPPED_PROCESSING_EVENT 0x041E
369 #define HCI_EXT_NUM_COMPLETED_PKTS_LIMIT_EVENT 0x041F
371 #define HCI_EXT_GET_CONNECTION_INFO_EVENT 0x0420
372 #define HCI_EXT_SET_MAX_DATA_LENGTH_EVENT 0x0421
373 #define HCI_EXT_SCAN_EVENT_NOTICE_EVENT 0x0422
374 #define HCI_EXT_SCAN_REQ_REPORT_EVENT 0x0423
375 #define HCI_EXT_GET_ACTIVE_CONNECTION_INFO_EVENT 0x0424
376 #define HCI_EXT_LL_TEST_MODE_EVENT 0x0470
378 
380  // end of HCI_Constants
382 
383 /*******************************************************************************
384  * TYPEDEFS
385  */
386 
387 /*******************************************************************************
388  * LOCAL VARIABLES
389  */
390 
391 /*******************************************************************************
392  * GLOBAL VARIABLES
393  */
394 
395 /*
396 ** HCI OSAL API
397 */
398 
400 
408 extern void HCI_Init( uint8 taskID );
409 
410 
419 extern void HCI_TL_getCmdResponderID( uint8 taskID );
420 
421 
432 extern uint16 HCI_ProcessEvent( uint8 task_id,
433  uint16 events );
434 
435 
437 
438 #ifdef __cplusplus
439 }
440 #endif
441 
442 #endif /* HCI_TL_H */
This API allows the software components in the Z-Stack to be written independently of the specifics o...
HCI layer interface.
© Copyright 1995-2020, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale