81 #ifndef ti_display_DisplayHost__include 82 #define ti_display_DisplayHost__include 129 uint8_t column,
char *fmt, va_list va);
void DisplayHost_clear(Display_Handle handle)
unsigned int DisplayHost_getType(void)
int dummy
Definition: DisplayHost.h:113
uint16_t strBufLen
Definition: DisplayHost.h:103
DisplayHost Object.
Definition: DisplayHost.h:111
Display Parameters.
Definition: Display.h:493
void DisplayHost_vprintf(Display_Handle handle, uint8_t line, uint8_t column, char *fmt, va_list va)
struct DisplayHost_HWAttrs DisplayHost_HWAttrs
DisplayHost Attributes.
Display_Handle DisplayHost_open(Display_Handle, Display_Params *params)
Generic interface for text output.
DisplayHost Attributes.
Definition: DisplayHost.h:98
struct DisplayHost_Object DisplayHost_Object
DisplayHost Object.
The definition of a Display function table that contains the required set of functions to control a s...
Definition: Display.h:552
struct DisplayHost_Object * DisplayHost_Handle
void DisplayHost_clearLines(Display_Handle handle, uint8_t fromLine, uint8_t toLine)
char * strBuf
Definition: DisplayHost.h:101
Display Global configuration.
Definition: Display.h:575
void DisplayHost_close(Display_Handle)
const Display_FxnTable DisplayHost_fxnTable
int DisplayHost_control(Display_Handle handle, unsigned int cmd, void *arg)
void DisplayHost_init(Display_Handle handle)