Example Summary
Example that uses the Instrumentation Trace Macrocell (ITM) hardware to write software instrumentation messages to the PC.
These messages can be read using a suite of tools available in CCS, IAR, or standalone tools.
Peripherals Exercised
Board_GPIO_LED0- Indicates that the board was initialized withinmain()
Resources & Jumper Settings
If you’re using an IDE (such as CCS or IAR), please refer to Board.html in your project directory for resources used and board-specific jumper settings. Otherwise, you can find Board.html in the directory <SDK_INSTALL_DIR>/source/ti/boards/<BOARD>.
If using CC32xx, then the device must be debugged in SWD mode and the SOP jumper must be placed in position 0 in order to send ITM messages on the SWO pin.
If using CC13XX/26XX the SWO jumper must be connected on the LaunchPad.
Example Usage
Use Device Manager to check the value of the XDS110 Class Auxiliary Data Port. Do not use the “Application/User UART” port. This should be a value like
COM22.Follow the setup instructions under the “Install Python Modules” heading in <SDK_INSTALL_DIR>tools/log/tiutils/Readme.html to generate a virtual environment. This will setup the ITM reader’s python environment. You do not need Wireshark for this example, and instructions for it should be ignored. Stop at the end of “Install Python Modules” and move on to the next step in this document.
Start a terminal in the <SDK_INSTALL_DIR>tools/log/tiutils/ folder and activate the virtual environment from the previous step by running
> ./.venv/Scripts/activate. Some terminals will now display an extra note with the prompt (e.g.(.venv)in PowerShell) indicating that a venv is active.In the same terminal, start the tool:
tilogger_itm_viewer <PORT> 12000000where<PORT>is the COM port from the first step (for exampletilogger_itm_viewer COM22 12000000).Build and flash the example using CCS or another tool. Once the firmware is flashed, disconnect the debugger. ITM output will not display if the debugger is connected.
NOTE: For CC13X4/26X4 boards, ITM will only output data while a debugger is connected. For these devices, it is necessary to launch a debug session instead of simply flashing the target. While remaining in the debug session, the device can be reset to output the reset-frame over ITM using the debugger. In CCS this can done from the menu
Run -> Reset -> Board Reset (automatic connect/disconnect).Reset the board.
Board_GPIO_LED0turns ON to indicate driver initialization is complete. The ITM tool will not begin printing until it receives a reset frame.The target will write a string message to the ITM software port: “Hello World from ITM”. Each write to the ITM stream will appear in the tool. See below for expected output and how this string appears in the data stream.
A clock function is setup that will update a global variable. This variable’s address is also setup as a DWT watch point. Every time the clock function runs the variable will update and
Board_GPIO_LED0will toggle.
Expected Output
When running the tool and resetting the board, this is an example of expected output:
> tilogger_itm_viewer COM62 12000000
INFO:Serial Rx:Serial port \\.\COM62 @ 12000000 opened
SW SWIT at +0, port STIM_DRIVER: 0xBB 0xBB 0xBB 0xBB
SW SWIT at +0, port STIM_RESV0: 0x48 0x65 0x6C 0x6C
TIMESTAMP in sync: + 169 cycles
SW SWIT at +169, port STIM_RESV0: 0x6F 0x20 0x57 0x6F
Unknown/Reserved timestamp header: 16
SW SWIT at +0, port STIM_RESV0: 0x72 0x6C 0x64 0x20
Unknown/Reserved timestamp header: 16
SW SWIT at +0, port STIM_RESV0: 0x66 0x72 0x6F 0x6D
SW SWIT at +0, port STIM_RESV0: 0x20 0x49 0x54 0x4D
SW SWIT at +0, port STIM_RESV0: 0x00
TIMESTAMP packet and timestamp delayed: + 34 cycles
TIMESTAMP in sync: + 1999999 cycles
HW Trace at 1999.999, Read Access, comparator: 0, value : 0x0
TIMESTAMP in sync: + 1030325 cycles
HW Trace at 1030.325, Write Access, comparator: 0, value : 0x1
TIMESTAMP in sync: + 1999999 cycles
HW Trace at 1999.999, Read Access, comparator: 0, value : 0x1
TIMESTAMP in sync: + 1020673 cycles
HW Trace at 1020.673, Write Access, comparator: 0, value : 0x2
TIMESTAMP in sync: + 1999999 cycles
HW Trace at 1999.999, Read Access, comparator: 0, value : 0x2
TIMESTAMP in sync: + 1020757 cycles
HW Trace at 1020.757, Write Access, comparator: 0, value : 0x3
First, we can see the reset frame 0xBB 0xBB 0xBB 0xBB.
Then we see a series of hex values interleaved with timestamps. These values match the expected hex output for “Hello World from ITM”:
H e l l o W o r l d
0x48 0x65 0x6C 0x6C 0x6F 0x20 0x57 0x6F 0x72 0x6C 0x64 0x20
f r o m I T M
0x66 0x72 0x6F 0x6D 0x20 0x49 0x54 0x4D 0x00
After this we see only the HW Trace packets. These are messages from the DWT Watchpoint module, which is tracking accesses to variableToWatch, which is accessed periodically by clockTimeoutFunction.
The lines indicating Unknown/Reserved timestamp are a limitation with the current tooling.
Host Side Tooling
Several IDEs such as IAR or CCS offer ITM focused tooling. These tools will configure the ITM registers directly through the debugger. This example will configure the ITM on device from firmware. For this reason, this example will not be compatible with these tools as the configuration settings may clash.
If it is desired to use these tools, it is recommended to comment out any APIs related to ITM configuration (e.g. ITM_open, ITM_close, ITM_enable*, ITM_disable*) and use ITM_applyPinMux directly to mux out the SWO pin.
From there, the settings and configuration of ITM is configured by the IDE. However the SW message APIs can be used to write to the stimulus ports.
SysConfig
The ITM driver parameters such as serial format, baudrate, and trace port enable can be configured in SysConfig. When enabled, the ITM driver will hook into the Power policy using ITM_flush and ITM_restore to ensure that all pending messages are flushed before the device powers down the CPU domain.
Application Design Details
This example shows how to initialize the ITM driver and use it to produce software messages and DWT messages from the target.
A single thread,
mainThread, configures and accesses the ITM.
FreeRTOS:
- Please view the
FreeRTOSConfig.hheader file for example configuration information.
IAR:
- When using any SensorTag(STK) Board, the XDS110 debugger must be selected with the 4-wire JTAG connection within your projects’ debugger configuration.