CC23x0R5DriverLibrary
hapi.h
Go to the documentation of this file.
1 /******************************************************************************
2  * Copyright (c) 2022-2023 Texas Instruments Incorporated
3  *
4  * Redistribution and use in source and binary forms, with or without
5  * modification, are permitted provided that the following conditions are met:
6  *
7  * 1) Redistributions of source code must retain the above copyright notice,
8  * this list of conditions and the following disclaimer.
9  *
10  * 2) Redistributions in binary form must reproduce the above copyright notice,
11  * this list of conditions and the following disclaimer in the documentation
12  * and/or other materials provided with the distribution.
13  *
14  * 3) Neither the name of the copyright holder nor the names of its
15  * contributors may be used to endorse or promote products derived from this
16  * software without specific prior written permission.
17  *
18  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
19  * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE
20  * IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE
21  * ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT HOLDER OR CONTRIBUTORS BE
22  * LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR
23  * CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF
24  * SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS
25  * INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN
26  * CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE)
27  * ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE
28  * POSSIBILITY OF SUCH DAMAGE.
29  *
30  ******************************************************************************/
31 
32 #ifndef __HAPI_H__
33 #define __HAPI_H__
34 
35 #include <stdint.h>
36 #include "sha256sw.h"
37 
43 #define FLASH_API_KEY 0xB7E3A08F
44 
46 typedef struct
47 {
48  // 0: Enter standby power state (from privileged thread mode with MSP as call stack)
49  void (*enterStandby)(const uint32_t *copyList);
50  // 1: [Utility] Calculate CRC32 over nBytes bytes at data
51  uint32_t (*crc32)(const uint8_t *data, uint32_t nBytes);
52  // 2: Apply copy list
53  void (*applyCopyList)(const uint32_t *list);
54  // 3: Erase (main) flash sector
55  uint32_t (*flashSectorErase)(uint32_t key, uint32_t sectorAddress);
56  // 4: Erase (main) flash bank
57  uint32_t (*flashBankErase)(uint32_t key);
58  // 5: Program (main) flash sector
59  uint32_t (*flashProgram)(uint32_t key, const uint8_t *dataBuffer, uint32_t address, uint32_t nBytes);
60  // 6: [Utility] Hamming weight of 32b word (number of bits set)
61  uint32_t (*countBits)(uint32_t word);
62  // 7: [Utility] Perform SECDED encoding on array of 64b words
63  void (*secdedEncode)(uint8_t *parity, const uint64_t *data, uint32_t nWords64);
64  // 8: [Utility] Perform SECDED detection/correction on array of 64b words and parity bytes
65  int32_t (*secdedDecode)(uint64_t *data, const uint8_t *parity, uint32_t nWords64);
66  // 9: Function to be called from boot code or bootloader to enter application properly
67  void (*enterApplication)();
68  // 10: SHA256: hash single block of data and produce digest
69  int_fast16_t (*sha256SwHashData)(SHA256SW_Handle handle,
70  SHA2SW_HashType hashType, // Only SHA2SW_HASH_TYPE_256 supported
71  const void *data,
72  size_t length,
73  uint32_t digest[8]);
74  // 11: SHA256: initialize hash state
75  int_fast16_t (*sha256SwStart)(SHA256SW_Handle handle,
76  SHA2SW_HashType hashType // Only SHA2SW_HASH_TYPE_256 supported
77  );
78  // 12: SHA256: update hash with data
79  int_fast16_t (*sha256SwAddData)(SHA256SW_Handle handle, const void *data, size_t length);
80  // 13: SHA256: finalize and produce digest
81  int_fast16_t (*sha256SwFinalize)(SHA256SW_Handle handle, uint32_t digest[8]);
82  // 14: [Utility] Reset device
83  void (*resetDevice)(void);
84  // 15: SHA256: Process Block
85  void (*sha256SwProcessBlock)(uint32_t digest[8], uint32_t Ws[16]);
86  // 16: SHA256: Round constants
87  const uint32_t (*sha256SW_K256)[64];
88  // 17: SHA256: Initial constants
89  const uint32_t (*sha256SW_initialDigest256)[8];
90  // 18: Busy loop that waits for nUs microseconds
91  void (*waitUs)(uint32_t nUs);
92  // 19: Count leading zeros
93  uint32_t (*clz)(uint32_t x);
94 } HARD_API_T;
95 
96 // Define address of HAPI table in ROM and macro for pointer to it
97 #define HAPI_TABLE_BASE_ADDR 0x0F00004C
98 #define HAPI_TABLE_POINTER ((const HARD_API_T *)HAPI_TABLE_BASE_ADDR)
99 
100 // ------------------------------------------------------------
101 // Macros used in applications to actually call HAPI functions
102 // ------------------------------------------------------------
103 
104 // void HapiEnterStandby(const uint32_t *copyList)
105 /*****************************************************************************
106  * \brief Enter standby power state
107  * Stores the full state of the CPU to MSP call stack so that it can get
108  * restored once we come back out of standby (at which point CPU is reset).
109  * When exiting standby the CPU will appear to return from this function.
110  *
111  * \param[in] copyList
112  * If non-null, the copy list to apply through ApplyCopyList() in the
113  * AsmExitStandby function while waiting for flash to become ready.
114  *
115  * \pre
116  * - Execution state is privileged and call stack being used is MSP
117  * - MSP call stack must reside in retained SRAM (obviously)
118  * - Interrupts have been turned off with CPSID but interrupts enabled in NVIC
119  * - Wakeup event(s) have been configured in AON event fabric
120  * - SCB.SCR.DSLP_EN=0 (if not, in debug standby exit will enter standby again)
121  * \warning
122  * The preconditions must be followed to the letter or bad things will happen
123  * \note
124  * Clobbers r0-r3 (normal per AAPCS)
125  *****************************************************************************/
126 #define HapiEnterStandby(p) HAPI_TABLE_POINTER->enterStandby((p))
127 
128 // uint32_t HapiCrc32(const uint8_t *data, uint32_t nBytes)
129 /*****************************************************************************
130  * \brief Calculate CRC32 over a data image
131  * CRC32 implementation that uses a 256-entry LUT
132  *
133  * \param[in] data
134  * Pointer to the image data
135  * \param[in] nBytes
136  * Size of image in bytes
137  *
138  * \return
139  * CRC-32 checksum of the image
140  *****************************************************************************/
141 #define HapiCrc32(p, n) HAPI_TABLE_POINTER->crc32((p), (n))
142 
143 // void HapiApplyCopyList(const uint32_t *list)
144 /*****************************************************************************
145  * \brief Process copy list
146  * Processes a copy list in a flexible CopyList format. Used by trims
147  * in FCFG, for user-defined initialization in CCFG and may be used by
148  * peripheral drivers to do HW reinitialization during wakeup from standby.
149  * The copy list is processed as a sequence of 32b command words, followed by
150  * zero or more literal words (LW):
151  *
152  * Command |31:28|27:20 |19:2 |1:0|LW|Description
153  * -------------|-----|---------|----------------------|---|--|-------------------
154  * EOL |0000 |0000_0000|0000_0000_0000_0000_00|00 |0 |End-of-list
155  * WAIT(N) |0001 |0000_0000|nnnn_nnnn_nnnn_nnnn_nn|00 |0 |Wait N/12 us
156  * NOP = WAIT(0)|0001 |0000_0000|0000_0000_0000_0000_00|00 |0 |No operation
157  * CPY(A*,N) |aaaa |nnnn_nnnn|aaaa_aaaa_aaaa_aaaa_aa|00 |N |Copy N literal words to address A*
158  * CPY(A,1) |aaaa |aaaa_aaaa|aaaa_aaaa_aaaa_aaaa_aa|01 |1 |Copy single literal word to full address A
159  * JMP(A) |aaaa |aaaa_aaaa|aaaa_aaaa_aaaa_aaaa_aa|10 |0 |Jump to new list at full address A
160  * CALL(A) |aaaa |aaaa_aaaa|aaaa_aaaa_aaaa_aaaa_aa|11 |0 |Recurse to list at full address A
161  *
162  * A* is a reduced address space that covers all SRAM and peripheral space.
163  * Bits 27:20 of this address will be assumed to be all zero. Full addresses
164  * must have 32b alignment
165  *
166  * \param[in] list
167  * Pointer to the copy list
168  *****************************************************************************/
169 #define HapiApplyCopyList(p) HAPI_TABLE_POINTER->applyCopyList((p))
170 
171 // uint32_t HapiFlashSectorErase(uint32_t key, uint32_t addr);
172 /*****************************************************************************
173  * \brief Erase a flash sector.
174  *
175  * Erase the flash sector that begins at address addr. Function will not return
176  * before erase operation completes or error occurs. Only main sectors and the
177  * CCFG sector is supported and are subject to flash write/erase restrictions.
178  * No default data is written back to CCFG after an erase.
179  *
180  * \warning No accesses to flash may occur during an erase operation. Interrupts
181  * must be disabled prior to calling or care taken that no reads to flash occur.
182  * DMA operations targeting flash must be suspended.
183  *
184  * \param key
185  * Magic number \ref FLASH_API_KEY (0xB7E3A08F) to protect against inadvertent
186  * flash erasures
187  * \param addr
188  * First address of a main sector or the CCFG sector
189  *
190  * \return
191  * Return code
192  * - \ref FAPI_STATUS_SUCCESS (0)
193  * - \ref FAPI_STATUS_ADDRESS_ERROR
194  * - \ref FAPI_STATUS_INVALID_KEY
195  * - \ref FAPI_STATUS_FSM_ERROR
196  *****************************************************************************/
197 #define HapiFlashSectorErase(k, p) HAPI_TABLE_POINTER->flashSectorErase((k), (p))
198 
199 // uint32_t HapiFlashBankErase(uint32_t key);
200 /******************************************************************************
201  * \brief Erase all unprotected sectors in the flash main bank.
202  *
203  * Function will not return before mass erase operation completes or error occurs.
204  *
205  * \warning No accesses to flash may occur during an erase operation. Interrupts
206  * must be disabled prior to calling or care taken that no reads to flash occur.
207  * DMA operations targeting flash must be suspended.
208  *
209  * \param key
210  * Magic number \ref FLASH_API_KEY (0xB7E3A08F) to protect against inadvertent
211  * flash erasures
212  *
213  * \return
214  * Return code
215  * - \ref FAPI_STATUS_SUCCESS (0)
216  * - \ref FAPI_STATUS_INVALID_KEY
217  * - \ref FAPI_STATUS_FSM_ERROR
218  *****************************************************************************/
219 #define HapiFlashBankErase(k) HAPI_TABLE_POINTER->flashBankErase((k))
220 
221 // uint32_t HapiFlashProgram(uint32_t key, const uint8_t *data, uint32_t addr, uint32_t nBytes)
222 /******************************************************************************
223  * \brief Program to flash (MAIN or CCFG)
224  *
225  * This function programs a sequence of bytes into the on-chip flash.
226  * Programming each location consists of the result of an AND operation
227  * of the new data and the existing data; in other words bits that contain
228  * 1 can remain 1 or be changed to 0, but bits that are 0 cannot be changed
229  * to 1. Therefore, a byte can be programmed multiple times as long as these
230  * rules are followed; if a program operation attempts to change a 0 bit to
231  * a 1 bit, that bit will not have its value changed.
232  *
233  * Programming may cross main sector boundaries. This function does not
234  * return until the data has been programmed or a programming error occurs.
235  *
236  * \note It is recommended to disable cache and line buffer before
237  * programming the flash and re-enable/clear cache and line buffer when the
238  * program operation completes.
239  *
240  * \warning Please note that code can not execute in flash while any part of
241  * the flash is being programmed or erased. The application must disable
242  * interrupts that have interrupt routines in flash.
243  *
244  * \warning The \c data pointer can not point to flash.
245  *
246  * \param key
247  * Magic number that must be \ref FLASH_API_KEY. The key protects against
248  * random jumps into the flash API
249  * \param data
250  * Pointer to the byte array of new data to be programmed
251  * \param addr
252  * First byte address in flash to be programmed
253  * \param nBytes
254  * Number of bytes to be programmed
255  *
256  * \return
257  * Return code
258  * - \ref FAPI_STATUS_SUCCESS (0)
259  * - \ref FAPI_STATUS_ADDRESS_ERROR
260  * - \ref FAPI_STATUS_INVALID_KEY
261  * - \ref FAPI_STATUS_INCORRECT_DATABUFFER_LENGTH
262  * - \ref FAPI_STATUS_FSM_ERROR
263  *****************************************************************************/
264 #define HapiFlashProgram(k, s, d, n) HAPI_TABLE_POINTER->flashProgram((k), (s), (d), (n))
265 
266 // uint32_t HapiCountBits(uint32_t word)
267 /*****************************************************************************
268  * \brief Return Hamming weight (# bits that are set) of word
269  *
270  * \param[in] word
271  * 32-bit word to count bits for
272  *
273  * \return
274  * Number of bits set in word (0-32)
275  *****************************************************************************/
276 #define HapiCountBits(w) HAPI_TABLE_POINTER->countBits((w))
277 
278 // void HapiSecdedEncode(uint8_t *parity, const uint64_t *data, uint32_t nWords64)
279 /*****************************************************************************
280  * \brief Perform SECDED encoding over data array and produce parity array
281  * Uses the usual (72,64) SECDED generator matrix:
282  * DDDDDDDD DDDDDDDD DDDDDDDD DDDDDDDD DDDDDDDD DDDDDDDD DDDDDDDD DDDDDDDD PPPPPPPP
283  * 66665555 55555544 44444444 33333333 33222222 22221111 11111100 00000000 00000000
284  * 32109876 54321098 76543210 98765432 10987654 32109876 54321098 76543210 76543210
285  * -------------------------------------------------------------------------------------
286  * P7: 11111111 11111111 11111111 11111111 11111111 11111111 11111111 11111111 01111111
287  * P6: 11111111 11111111 11111111 11111111 11111111 11111111 11111111 11111110 00000000
288  * P5: 11111111 11111111 11111111 11111111 00000000 00000000 00000000 00000001 00000000
289  * P4: 11111111 11111111 00000000 00000000 11111111 11111111 00000000 00000001 00000000
290  * P3: 11111111 00000000 11111111 00000000 11111111 00000000 11111111 00000001 00000000
291  * P2: 11110000 11110000 11110000 11110000 11110000 11110000 11110000 11110001 00000000
292  * P1: 11001100 11001100 11001100 11001100 11001100 11001100 11001100 11001101 00000000
293  * P0: 10101010 10101010 10101010 10101010 10101010 10101010 10101010 10101011 00000000
294  *
295  * \param[out] parity
296  * Pointer to where to store parity bytes (one byte per 64b word of data)
297  * \param[in] data
298  * Pointer to the data (4B aligned)
299  * \param[in] nWords64
300  * Number of 64b words of data / bytes of parity
301  *****************************************************************************/
302 #define HapiSecdedEncode(p, d, n) HAPI_TABLE_POINTER->secdedEncode((p), (d), (n))
303 
304 // int32_t HapiSecdedDecode(uint64_t *data, const uint8_t *parity, uint32_t nWords64)
305 /*****************************************************************************
306  * \brief Perform SECDED correction/detection over data array using parity array
307  * Uses the usual (72,64) SECDED generator matrix.
308  *
309  * \param[inout] data
310  * Pointer to the data (4B aligned)
311  * \param[in] parity
312  * Pointer to the parity bytes (one byte per 64b word of data)
313  * \param[in] nWords64
314  * Number of 64b words of data / bytes of parity
315  *
316  * \return
317  * <0: uncorrectable error detected
318  * >=0: number of bits corrected
319  *****************************************************************************/
320 #define HapiSecdedDecode(d, p, n) HAPI_TABLE_POINTER->secdedDecode((d), (p), (n))
321 
322 // void BootEnterApplication(void)
323 /*****************************************************************************
324  * \brief Called from bootloader to transfer into application
325  * When called from a bootloader this function will apply application security
326  * restrictions and transfer to application (set up VTOR register, setup SP and
327  * jump to entry point as defined by application vector table in CCFG). The
328  * function will never return.
329  *
330  * When called from an application the function will return without doing
331  * anything.
332  *****************************************************************************/
333 #define HapiEnterApplication() HAPI_TABLE_POINTER->enterApplication()
334 
335 // int_fast16_t HapiSha256SwHashData(
336 // SHA256SW_Handle handle,
337 // const void *data,
338 // size_t length,
339 // uint32_t digest[8]
340 // )
341 /*****************************************************************************
342  * \brief Performs a complete SHA256 hash operation, producing a final
343  * digest for the data.
344  *
345  * This function wraps #HapiSha256SwStart(), #HapiSha256SwAddData(), and
346  * #HapiSha256SwFinalize().
347  *
348  * There is no need to call #HapiSha256SwStart() prior to calling this function.
349  *
350  * The total length of data that can be hashed by this implementation
351  * is 512MiB (0x20000000 bytes.)
352  *
353  * \param[in] handle A #SHA256SW_Handle.
354  *
355  * \param[in] data Data (message) to hash. May point to zero.
356  *
357  * \param[in] length The number of bytes (pointed to by \c data parameter)
358  * to add to the hash.
359  *
360  * \param[out] digest Output location for the final digest. Must be
361  * able to hold 32 bytes of output and be 32-bit aligned.
362  *
363  * \retval #SHA2SW_STATUS_SUCCESS (0) The hash operation succeeded.
364  * \retval #SHA2SW_STATUS_ERROR The hash operation failed.
365  * \retval #SHA2SW_STATUS_UNSUPPORTED Requested Hash Type is unsupported.
366  * \retval #SHA2SW_STATUS_LENGTH_TOO_LARGE The requested length of data to hash
367  * is more than the implementation
368  * supports.
369  * \retval #SHA2SW_STATUS_NULL_INPUT One or more of the pointer inputs is
370  * NULL.
371  *****************************************************************************/
372 #define HapiSha256SwHashData(h, d, l, g) HAPI_TABLE_POINTER->sha256SwHashData((h), SHA2SW_HASH_TYPE_256, (d), (l), (g))
373 
374 // int_fast16_t HapiSha256SwStart(SHA256SW_Handle handle)
375 /*****************************************************************************
376  * \brief Initialize a SHA256SW_Handle, preparing for hashing data.
377  *
378  * \param[in] handle A #SHA256SW_Handle.
379  *
380  * \retval #SHA2SW_STATUS_SUCCESS (0) The hash operation succeeded.
381  * \retval #SHA2SW_STATUS_UNSUPPORTED Requested Hash Type is unsupported.
382  * \retval #SHA2SW_STATUS_NULL_INPUT One or more of the pointer inputs is
383  * NULL.
384  *
385  * \sa #HapiSha256SwAddData()
386  * \sa #HapiSha256SwFinalize()
387  *****************************************************************************/
388 #define HapiSha256SwStart(h) HAPI_TABLE_POINTER->sha256SwStart((h), SHA2SW_HASH_TYPE_256)
389 
390 // int_fast16_t HapiSha256SwAddData(SHA256SW_Handle handle, const void *data, size_t length)
391 /*****************************************************************************
392  * \brief Add data to a SHA256 operation.
393  *
394  * Adds data to a hash operation. The \c handle must have been
395  * initialized by a call to HapiSha256SwStart first.
396  *
397  * The total length of data that can be hashed by this implementation
398  * is 512MiB (0x20000000 bytes.)
399  *
400  * After passing in all data to be hashed, call #HapiSha256SwFinalize()
401  * to obtain the final digest.
402  *
403  * \pre handle was previously passed to #HapiSha256SwStart().
404  *
405  * \param[in] handle A #SHA256SW_Handle.
406  *
407  * \param[in] data Data (message) to add to the hash. May point to zero.
408  *
409  * \param[in] length The number of bytes (pointed to by \c data parameter)
410  * to add to the hash.
411  *
412  * \retval #SHA2SW_STATUS_SUCCESS (0) The hash operation succeeded.
413  * \retval #SHA2SW_STATUS_LENGTH_TOO_LARGE The requested length of data to hash
414  * is more than the implementation
415  * supports.
416  * \retval #SHA2SW_STATUS_NULL_INPUT One or more of the pointer inputs is
417  * NULL.
418  *
419  * \sa #HapiSha256SwStart()
420  * \sa #HapiSha256SwFinalize()
421  *****************************************************************************/
422 #define HapiSha256SwAddData(h, d, l) HAPI_TABLE_POINTER->sha256SwAddData((h), (d), (l))
423 
424 // int_fast16_t HapiSha256SwFinalize(SHA256SW_Handle handle, uint32_t digest[8]);
425 /*****************************************************************************
426  * \brief Finalize a SHA256 operation, creating the final digest.
427  *
428  * After calling this function, \c handle should not be used again
429  * until it has been reinitialized via a call to #HapiSha256SwStart().
430  *
431  * \pre handle was previously passed to #HapiSha256SwStart() and data to
432  * be hashed was passed to #HapiSha256SwAddData()
433  *
434  * \param[in] handle A #SHA256SW_Handle.
435  *
436  * \param[out] digest Output location for the final digest. Must be
437  * able to hold 32 bytes of output and be 32-bit aligned.
438  *
439  * \retval #SHA2SW_STATUS_SUCCESS (0) The hash operation succeeded.
440  * \retval #SHA2SW_STATUS_NULL_INPUT One or more of the pointer inputs is
441  * NULL.
442  *
443  * \sa #HapiSha256SwStart()
444  * \sa #HapiSha256SwAddData()
445  *****************************************************************************/
446 #define HapiSha256SwFinalize(h, g) HAPI_TABLE_POINTER->sha256SwFinalize((h), (g))
447 
448 // __noreturn void HapiResetDevice(void)
449 /*****************************************************************************
450  * \brief Perform system reset of the device
451  *
452  * This function will perform a system reset of the device equal to a pin
453  * reset. Software can determine that this was the cause of reset once
454  * rebooted. The function will never return.
455  *****************************************************************************/
456 #define HapiResetDevice() HAPI_TABLE_POINTER->resetDevice()
457 
458 // HAPI entry used for internal purposes
459 #define HapiSha256SWProcessBlock(d, w) HAPI_TABLE_POINTER->pSHA256SWProcessBlock((d), (w))
460 
461 // HAPI entry used for internal purposes
462 #define HapiSha256SW_K256 (*HAPI_TABLE_POINTER->sha256SW_K256)
463 
464 // HAPI entry used for internal purposes
465 #define HapiSha256SW_initialDigest256 (*HAPI_TABLE_POINTER->sha256SW_initialDigest256)
466 
467 // void HapiWaitUs(uint32_t nUs)
468 /*****************************************************************************
469  * \brief Wait function
470  *
471  * \param[in] nUs
472  * Number of microseconds to wait (min: 1 us, max: 2^24 us)
473  *****************************************************************************/
474 #define HapiWaitUs(n) HAPI_TABLE_POINTER->waitUs((n))
475 
476 // uint32_t HapiClz(uint32_t x)
477 /*****************************************************************************
478  * \brief Count leading zeros
479  *
480  * \param[in] x
481  * Value to count leading zeros for
482  * \return
483  * Number of leading zeroes (0 to 32)
484  *****************************************************************************/
485 #define HapiClz(x) HAPI_TABLE_POINTER->clz((x))
486 
487 #endif //__HAPI_H__
SHA256SW Object.
Definition: sha256sw.h:217
Definition: hapi.h:46
SHA2SW_HashType
Enum for the hash types supported by the library.
Definition: sha2sw_common.h:53