44 #ifndef ti_drivers_can_cancc27xx__include 45 #define ti_drivers_can_cancc27xx__include 54 #define CANCC27XX_MRAM_SIZE 4096U 57 #define CANCC27XX_CLK_FREQ_MHZ 80U const CANCC27XX_Config CANCC27XX_config
void CANCC27XX_clearStatus(void)
Clears all CANCC27XX device status flags.
uint32_t CANCC27XX_getMode(void)
Reads the CANCC27XX operational mode.
uint32_t CANCC27XX_getStatus(void)
Reads the CANCC27XX device status flags.
void CANCC27XX_setMode(uint32_t mode)
Sets the CANCC27XX operational mode.
uint32_t clkFreqMHz
Definition: CANCC27XX.h:64
CANCC27XX global configuration.
Definition: CANCC27XX.h:62
void CANCC27XX_disableSleepWakeErrorTimeout(void)
Disables the sleep wake error timeout.