46 #ifndef ti_drivers_comparator_ComparatorLPF3LP__include 47 #define ti_drivers_comparator_ComparatorLPF3LP__include 57 #include <ti/devices/DeviceFamily.h> 58 #include DeviceFamily_constructPath(driverlib/lpcmp.h) uint8_t negativeInputPinMux
Definition: ComparatorLPF3LP.h:188
Definition: ComparatorLPF3LP.h:146
const Comparator_FxnTable ComparatorLPF3LP_fxnTable
Comparator function table for the ComparatorLPF3LP implementation.
The definition of a comparator function table that contains the required set of functions to control ...
Definition: Comparator.h:391
Comparator_Trigger
Comparator interrupt trigger.
Definition: Comparator.h:272
uint8_t positiveInputPinMux
Definition: ComparatorLPF3LP.h:186
uint8_t negativeInputPin
Definition: ComparatorLPF3LP.h:187
HwiP structure.
Definition: HwiP.h:78
uint32_t intNum
Definition: ComparatorLPF3LP.h:178
Definition: ComparatorLPF3LP.h:125
Definition: ComparatorLPF3LP.h:108
Definition: ComparatorLPF3LP.h:110
ComparatorLPF3LP_NegativeInputChannel
ComparatorLPF3LP Negative input channel These fields are intended to serve as the options for the Com...
Definition: ComparatorLPF3LP.h:80
ComparatorLPF3LP Object.
Definition: ComparatorLPF3LP.h:196
HwiP_Struct hwi
Definition: ComparatorLPF3LP.h:198
Semaphore module for the RTOS Porting Interface.
uint32_t intPriority
Definition: ComparatorLPF3LP.h:179
Definition: ComparatorLPF3LP.h:149
ComparatorLPF3LP Hardware attributes.
Definition: ComparatorLPF3LP.h:176
uint32_t intMux
Definition: ComparatorLPF3LP.h:180
ComparatorLPF3LP_PositiveInputChannel
ComparatorLPF3LP Positive input channel.
Definition: ComparatorLPF3LP.h:106
uint8_t positiveInputPin
Definition: ComparatorLPF3LP.h:185
Definition: ComparatorLPF3LP.h:84
ComparatorLPF3LP_VoltageDividerPath
ComparatorLPF3LP Voltage divider path.
Definition: ComparatorLPF3LP.h:123
Definition: ComparatorLPF3LP.h:126
Definition: ComparatorLPF3LP.h:148
ComparatorLPF3LP_VoltageDividerPath voltageDividerPath
Definition: ComparatorLPF3LP.h:183
Comparator_CallBackFxn callbackFxn
Definition: ComparatorLPF3LP.h:199
Definition: ComparatorLPF3LP.h:147
bool isRunning
Definition: ComparatorLPF3LP.h:202
bool isOpen
Definition: ComparatorLPF3LP.h:201
ComparatorLPF3LP_VoltageDividerFactor voltageDividerFactor
Definition: ComparatorLPF3LP.h:184
ComparatorLPF3LP_NegativeInputChannel negativeInputChannel
Definition: ComparatorLPF3LP.h:182
Comparator_Trigger trigger
Definition: ComparatorLPF3LP.h:200
Definition: ComparatorLPF3LP.h:82
Definition: ComparatorLPF3LP.h:85
Definition: ComparatorLPF3LP.h:83
ComparatorLPF3LP_VoltageDividerFactor
ComparatorLPF3LP Voltage divider factor.
Definition: ComparatorLPF3LP.h:144
ComparatorLPF3LP_PositiveInputChannel positiveInputChannel
Definition: ComparatorLPF3LP.h:181
void(* Comparator_CallBackFxn)(Comparator_Handle handle, int_fast16_t returnValue, Comparator_Trigger trigger)
Comparator callback function.
Definition: Comparator.h:320
Definition: ComparatorLPF3LP.h:111
Definition: ComparatorLPF3LP.h:109
Hardware Interrupt module for the RTOS Porting Interface.
Definition: ComparatorLPF3LP.h:150