CC26x2 to CC23xx Porting Guide¶
This section will describe, in general terms, how to port a project developed for the CC26X2 device on the SimpleLink CC13xx and CC26xx SDK to a CC23xx device running the SimpleLink Low Power F3 SDK.
The best way to migrate is to open a new example project with similar functionality in the new SDK and transfer your changes and application code over to the new example.
The following sections discuss the major changes between the CC26x2 devices and the CC23xx devices.
-
-
-
sec-example-simple-peripheral-port-cc26x2-to-cc23xx
General Considerations¶
FreeRTOS¶
The CC23xx devices exclusively support FreeRTOS. If a project needs to be migrated from the SimpleLink CC13xx and CC26xx SDK and uses TI-RTOS or TI-RTOS7, it will need to be converted to FreeRTOS during the migration process.
CC23xx LaunchPad support¶
All example applications are compatible with the CC23xx LaunchPad development kit. These features allow for a unified development experience and empowers developers to rapidly release to market.
Sensor Controller¶
The CC23xx does not support the Sensor Controller. Any applications being ported from the SimpleLink CC13xx and CC26xx SDK that make use of the Sensor Controller will need to be modified to not use the Sensor Controller in order to work with the CC23xx.
Migration Guides¶
Migrate to FreeRTOS¶
An important step that must be taken in order to port an example from the SimpleLink CC13xx and CC26xx SDK to the SimpleLink Low Power F3 SDK is to ensure that the project is implemented in FreeRTOS. The SimpleLink Low Power F3 SDK only supports FreeRTOS, so any projects running on TI-RTOS or TI-RTOS7 will not work unless they are converted to FreeRTOS. The best way to migrate is to use a new example project with similar functionality in the new SDK which already uses FreeRTOS. Proprietary RF also supports No-RTOS projects.
Migrate the RF stack¶
The SimpleLink Low Power F3 SDK RF stack uses RCL instead of rflib to control RF features. For more information, see rflib to RCL Migration Guide and Radio Control Layer (RCL)
Migrate the TI drivers¶
It is important to ensure that projects that are being ported are not using deprecated libraries. A few migration guides for libraries that should be updated as part of the SimpleLink CC13xx and CC26xx SDK to SimpleLink Low Power F3 SDK migration are shown below:
Example¶
The following section provides an example of how to port a project from the SimpleLink CC13xx and CC26xx SDK to the SimpleLink Low Power F3 SDK. All of the steps shown below are essentially putting into practice the theory discussed earlier in this document.
Porting RF Packet TX¶
For this porting guide, RF Packet TX will be ported from the SimpleLink CC13xx and CC26xx SDK using a CC26X2R1 device to the SimpleLink Low Power F3 SDK using a CC2340R5 device. To minimize project configuration differences, start with an example project in the CC23xx. The recommended approach is to start with a SimpleLink Low Power F3 SDK project that contains the same base functionality as the porting target project and merge in any custom functionality.
Warning
As the SimpleLink Low Power F3 SDK is still under active development, there is still some functionality missing that will be added as development continues. If you have any questions about what is currently supported or not supported in the latest version of the SimpleLink Low Power F3 SDK, please reach out to your TI representative.
Choose a SimpleLink Low Power F3 SDK FreeRTOS or No-RTOS example project that contains your target project’s base functionality.
Transfer all modified application files from SimpleLink CC13xx and CC26xx SDK project into the SimpleLink Low Power F3 SDK example project. In this example, the
rfPacketTx.c
file from SimpleLink CC13xx and CC26xx SDK project were moved into RF Packet TX SimpleLink Low Power F3 SDK example.Move any other custom files and services that the application is using to the SimpleLink Low Power F3 SDK project.
Perform all necessary conversions from rflib to RCL by leveraging Migrate the RF stack.
Transfer the SysConfig settings visually through the GUI. Custom RF Stacks are not included in the SimpleLink Low Power F3 SDK SysConfig version and thus the radio PHY must be selected through pre-definitions.
Predefined Symbol
PHY setting
None
Bluetooth LE 5.0 1Mbps
USE_250KBPS_MSK
250kbps MSK
USE_250KBPS_MSK_FEC
250kbps MSK with Forward Error Correction (FEC)
Note
Several other PHYs are supported as shown inside the
setup
folder which will require including the correct.h
file insiderfPacketx.c
along with other relevant RF setting changes in the application file.If necessary, update the project to use the newer TI drivers that are supplied with the SimpleLink Low Power F3 SDK.
The UART library has been deprecated and replaced by the UART2 library. Please follow the UART to UART2 Porting Guide
The Pin and GPIO libraries are deprecated and have been replaced by the GPIO++ library. To update Pin or GPIO code, please reference the following porting guide GPIO++ Driver Porting Guide
Refer to the Core SDK release notes for additional information and the FreeRTOS examples included with SimpleLink Low Power F3 SDK.
For additional information on how SimpleLink Low Power F3 SDK uses FreeRTOS see FreeRTOS (RTOS Kernel) Overview.
At this stage, most, if not all, of the modifications required have been completed. It is possible that some additional modifications may be required for the project to function as intended, but these changes can be relatively minor compared to the modifications already made by following this porting guide.