Custom Hardware¶
This section will explain how to adapt a BLE5-Stack application from the SimpleLink Low Power F3 SDK to run on custom hardware. In general, the steps required to migrate a BLE5-Stack application from a development kit to a custom board are minimal and involve changing the pin configuration as well as selecting the correct RF configuration. These steps, including a bring up guide, are detailed in the subsections below.
Designing a Custom Board¶
Design guidelines for CC13x2 and CC26x2 boards can be found in the CC13xx/CC26xx Hardware Configuration and PCB Design Considerations app note. This app note includes RF front-end, schematic, PCB, and antenna design considerations. The report also covers crystal oscillator tuning, optimum load impedance as well as a brief explanation of the different power supply configurations.
Note
A similar app note will be produced for the CC23xx devices. In the meantime, we recommend leveraging the reference designs available in the MSR folder.
Creating a Custom Board File¶
Board files are used by TI drivers to store device specific settings and I/O
mapping. The board file abstraction allows one TI-drivers implementation
to support many hardware implementations by just setting up new board files.
Examples utilize SysConfig to generate these board files. The generated
structures are placed in the ti_drivers_config.c
and ti_drivers_config.h
files. The SysConfig user interface can be utilized to determine pins and
resources used. Information on pins and resources used is also present in both
of these generated files. It is recommended to use SysConfig to generate the
board files for custom hardware as described
here.
Clock configuration for Bluetooth LE¶
Clock accuracies and Bluetooth LE¶
The Bluetooth Core Specifications Version 5.3 defines two clock accuracies, the “Active clock accuracy” (Bluetooth Core Specifications Version 5.3 Vol 6, Part B, §4.2.1) and the “Sleep clock accuracy” (Bluetooth Core Specifications Version 5.3 Vol 6, Part B, §4.2.1). In general, the HF XTAL (high frequency crystal oscillator) is used as active clock and the LF XTAL (low frequency crystal oscillator) is used as sleep clock. Tuning of the HF XTAL and LF XTAL is discussed in the HW Configuration Guide.
The Bluetooth Core Specifications Version 5.3 require the active clock to have a drift less than or equal to ±50 ppm and there is no way (nor need) to specify its accuracy to the TI BLE5-Stack.
The Bluetooth Core Specifications Version 5.3 require the sleep clock to have a drift less than or equal to ±500 ppm. The accuracy of this clock has a real impact on the timing of the radio operations. This is why its accuracy should be communicated to the TI BLE5-Stack using the function HCI_EXT_SetSCACmd().
As mentioned before, the accuracy of the sleep clock has an impact on the timing of the radio operations. This effect is called window widening and is described in details in the Bluetooth Core Specifications Version 5.3 Vol 6, Part B, §4.2.4.
The Link Layer is expecting to receive a packet within a certain window (extending from receiveWindowStart to receiveWindowEnd) or at a certain time (in which case receiveWindowStart and receiveWindowEnd are both that time) but, because of active clock accuracies and sleep clock accuracies there is uncertainty as to the exact timing of that window at the sending Link Layer. The recipient should therefore adjust its listening time to allow for this uncertainty. The increase in listening time is called the window widening. Assuming the clock inaccuracies are purely given in parts per million (ppm), it is calculated as follows:
where J shall be 2 when the active clock applies and 16 when the sleep clock applies and the other parameters are specified in Table 4.1. of Bluetooth Core Specifications Version 5.3 Vol 6, Part B, §4.2.4.
The connection parameters can be chosen independently of the clock accuracy – absolutely all the combinations of clock accuracy and connection parameters are allowed. As can be observed in the formula, for a given clock accuracy, the listening window length is proportional to the effective connection interval. At a certain point this might have a significant impact on the energy consumption.
Using 32-kHz Crystal-Less Mode (LF RCOSC)¶
BLE5-Stack 3.03.01.00 includes support for operating the CC23xx in a 32-kHz crystal-less mode for peripheral and broadcaster (beacon) role configurations. By using the internal low-frequency RC oscillator (LF RCOSC), the 32-kHz crystal can be removed from the board layout.
LF RCOSC should be enabled as Low Frequency clock
in SysConfig
-> TI Devices
-> Device Configuration
->
Low Frequency Clock Source
selecting LF RCOSC
.
This leads SysConfig to generate code to enable the usage of the
LF RCOSC by calling PowerLPF3_selectLFOSC()
in the Board_init()
function (ti_drivers_config.c
file). Other configurations are
set by SysConfig at the same time to ensure the stack accounts for the
lower LF clock accuracy obtained by applying the workaround described in
the CC23xx errata document for Advisory CLK_01.
The Sleep Clock Accuracy (SCA) obtained with the LF RCOSC is not as accurate as 32-kHz crystal. For this reason,
In accordance with the Bluetooth Core Specifications Version 5.3, the first listening (Rx) operation duration of the Bluetooth LE connections events are increased. The longer time between connection events, the more the Rx operations duration are increased, directly impacting the average power consumption (see Bluetooth Core Specifications Version 5.3 Vol 6, Part B, §4.2.2 for details on the Rx window calculation). The power consumption while advertising is not impacted, making the 32-kHz crystal-less mode particularly adapted for beacon-applications or requiring for use-cases requiring infrequent connections and/or short connection intervals.
Connection events are more likely to be missed. When a connection event is missed, the device enlarges its Rx window to increase chances to catch the next connection event. The Rx window duration is reverted to its regular duration after properly ack-ed connection events. The duration of the Rx window used after an unsuccessful connection event depends on the maximum inaccuracy expected on the LF RCOSC. The parameter
Peripheral Extra LFOSC PPM
inSysConfig
->BLE
->Advanced Settings
(only available when LF RCOSC has been selected) should be set with the maximum inaccuracy expected on the LF RCOSC. The default value set in SysConfig is expected to fit most of the use cases. Developers can consider adjusting this value based on the specific requirements of the use case targeted.The Sleep Clock Accuracy (SCA) is automatically set by the stack to the maximum value (500 ppm). Overwriting this value may lead to connection establishment issues and frequent disconnections.
RF Temperature Compensation¶
If the selected HFXT source is not accurate enough for the selected RF protocol,
RF temperature Compensation may be enabled via SysConfig
→ TI Devices
→ Device Configuration
. RF Temperature Compensation compensates HFXT frequency
for temperature during radio transmissions. This improves the accuracy of the
CLKSVT and CLKREF over temperature.
Note
Each crystal will have different parameters. You may request the parameters for your specific crystal by contacting the crystal vendor/manufacturer.
HFXT Compensation Threshold: HFXT will only be automatically compensated when the measured device temperature exceeds this threshold (in degrees Celsius). This can help to reduce power consumption if temperature compensation is not required below a certain temperature. If set to -41, then compensation will be enabled across the entire operating temperature range of [-40, +125].
HFXT Compensation Delta: HFXT will be automatically compensated if the temperature drifts more than this delta-value in either direction (in degrees Celsius). For example, if the temperature is measured to 30 degrees when the device boots (measured within
Board_init()
), but later drifts to 30 + delta or 30 - delta, then HFXT temperature compensation will be performed, and the temperature setpoint updated accordingly.
Note
Temperature is calculated using the Temperature driver. Please see Temperature.h for more information.
Configuring Device Parameters for Custom Hardware¶
Set parameters, such as the sleep clock accuracy of the 32.768-kHz crystal.
Define the CCFG parameters in Device Configuration in SysConfig.
Note
For a description of CCFG configuration parameters, see the CC23xx SimpleLink Wireless MCU Technical Reference Manual.
HFXT Amplitude Compensation¶
High Frequency Crystal (HFXT) Amplitude Compensation feature adjusts the power amplitude to ensure the high frequency crystal receives sufficient power. The standard HFXT Amplitude Compensation is always enabled - the CC23xx power driver takes care of this.
HFXT Amplitude Compensation: At boot within
Power_init()
, HFXT amplitude is configured to the highest possible value. After this, HFXT amplitude is adjusted to the optimal value each time the device enters standby. It will take up to five iterations after boot until the optimal amplitude is found. This process ensures that the amplitude remains in an optimal range if operating conditions change. This feature will always be enabled, unless Initial HFXT Amplitude Compensation is enabled.Initial HFXT Amplitude Compensation: If the application rarely enters standby, initial HFXT Amplitude Compensation can be enabled when the application requires the optimal amplitude to be found at or after boot. HFXT will take longer to be ready after boot, but when ready the amplitude is already in the optimal range. This process is done asynchronously and is enabled via
SysConfig
→TI Devices
→Device Configuration
→Initial HFXT Amplitude Compensation
.Note
Enabling initial HFXT amplitude compensation will result in more flash usage and a longer time from boot to first RF operation.
Initial Board Bring Up¶
When powering up a custom board with the CC23xx for the first time, it is recommended to follow the Board Bring-Up section on CC13xx/CC26xx Hardware Configuration and PCB Design Considerations. After confirming that the board is being powered correctly by the battery or power supply and can be identified by the SWD tool, programming the device with a minimal SW application to verify stability is also suggested.
TI recommends using the basic_ble sample application for initial board
bring up with modifications to the ti_drivers_config.c
file to:
Disable all GPIO pin access
Select the correct RF front end setting (done by SysConfig)
The TI BLE5-Stack does not require any GPIO pins to be configured in order to
establish and maintain a BLE connection. Ensure that Display_DISABLE_ALL
is defined in the application Predefined Symbols so that diagnostic logging
data is not routed to any GPIO pin. If your custom board uses a different device
configuration, such as the 32 kHz crystal-less RCOSC_LF configuration, be sure
to make these device changes to the project. With this minimal application
configuration you should be able to establish a BLE connection
(e.g., with a smart phone or BTool) to your board at the expected range.
If you are not able to complete this step, then it is likely there is a
misconfiguration of the RF front end or you have other board related or layout
issues.
After confirming that your board can maintain a BLE connection, you can now validate that your BLE application functions as expected on the custom board. Again, it is suggested to enable your GPIO pins one at a time in the board file and comment-out access to other GPIO pins in your application. If you do encounter a CPU exception (HWI abort) during this phase it is likely that a GPIO pin is incorrectly mapped in your custom board file or your application is attempting to access a GPIO pin that does not exist in your device package type.
Using the RGE QFN24 package variant¶
The CC23xx is also available with a 4-mm x 4-mm RGE QFN24 (12 GPIOs) package variant. See the CC23xx Datasheet for all the package options and IO descriptions.
In order to build SimpleLink Low Power F3 SDK project using the RGE package, a few settings must be made in SysConfig.
First open the SysConfig file, click the icon on the top right hand corner
Show Board View
Click the button
SWITCH
Select
NONE
in the Board | New Value fieldSelect the
CC2340R5RGE
device in the Device field. It automatically updates the package toRGE
.Finally click
CONFIRM
After clicking CONFIRM
, the pins of the SysConfig file may change. If error
messages appear, check that the pins changed in SysConfig are consistent with
the implemented hardware design.
For each error, review the suggested configuration value, and accept it or modify it.
Tuning HFXT capacitors¶
One of the features offered by SmartRF Studio 8 is the ability to tune the HFXT capacitors. Generally the RF link could be affected by variations in hardware, this is normally difficult to fix; however with HFXT the RF link can be adjusted by changing the two capacitor values in SmartRF Studio 8.
Tip
TI recommends tuning the HFXT capacitors values for the design. The RF performances improvements obtained by tuning the HFXT capacitors values for each unit on the production line generally do not justify the complexity and added costs.
- Download the latest SmartRF 8 Studio
Open SmartRF Studio 8 and open the target device
3. Select the RF settings used by your design. Once SmartRF Studio 8 is open you can view and select various PHYs, to edit a PHY you will need to create a new PHY by clicking on the box next to the PHY name.
4. You can edit various settings on the PHY properties page such as the custom name, frequency, sync word, and tx power.
To tune HFXT cap-array tuning change disable to enable and then edit values as needed.
6. To implement the HFXT capacitors values found in the embedded code, open the project in your favorite IDE open the SysConfig file -> Device Configuration and click on “Override HFXT Cap Array Trims” and input the two values found.