137 #ifndef ti_drivers_i2c_I2CLPF3__include   138 #define ti_drivers_i2c_I2CLPF3__include Power_NotifyObj i2cPostObj
Definition: I2CLPF3.h:271
uint8_t sclPin
Definition: I2CLPF3.h:246
uint8_t sdaPin
Definition: I2CLPF3.h:243
I2C_BASE_HWATTRS uint32_t swiPriority
Definition: I2CLPF3.h:237
uint8_t sclPin
Definition: I2CLPF3.h:267
uint8_t pinSCL
Definition: I2CLPF3.h:176
I2C_BASE_OBJECT SwiP_Struct swi
Definition: I2CLPF3.h:260
uint8_t sclPinMux
Definition: I2CLPF3.h:247
uint8_t sdaPinMux
Definition: I2CLPF3.h:244
uint32_t bitRate
Definition: I2CLPF3.h:263
I2CLPF3 Object. 
Definition: I2CLPF3.h:255
uint8_t sdaPin
Definition: I2CLPF3.h:266
Software Interrupt module for the RTOS Porting Interface. 
Power notify object structure. 
Definition: Power.h:441
PowerLPF3_Resource powerMngrId
Definition: I2CLPF3.h:240
void * i2cPostFxn
Definition: I2CLPF3.h:270
I2CLPF3 Hardware attributes. 
Definition: I2CLPF3.h:226
uint8_t pinSDA
Definition: I2CLPF3.h:175
I2CLPF3 Pin Configuration. 
Definition: I2CLPF3.h:173
SemaphoreP structure. 
Definition: SwiP.h:68
Inter-Integrated Circuit (I2C) Controller Driver.