72 #ifndef ti_drivers_aesccm_AESCCMLPF3__include 73 #define ti_drivers_aesccm_AESCCMLPF3__include 81 #include <ti/devices/DeviceFamily.h> 82 #if (DeviceFamily_PARENT != DeviceFamily_PARENT_CC35XX) 83 #include DeviceFamily_constructPath(driverlib/aes.h) 90 #define AESCCMLPF3_AAD_BUFFER_SIZE 2U 92 #if (DeviceFamily_PARENT == DeviceFamily_PARENT_CC27XX) || (DeviceFamily_PARENT == DeviceFamily_PARENT_CC35XX) 135 #if (DeviceFamily_PARENT == DeviceFamily_PARENT_CC27XX) || (DeviceFamily_PARENT == DeviceFamily_PARENT_CC35XX) 158 #if (DeviceFamily_PARENT == DeviceFamily_PARENT_CC27XX) || (DeviceFamily_PARENT == DeviceFamily_PARENT_CC35XX) AESCommonLPF3_HWAttrs AESCCMLPF3_HWAttrs
AESCCMLPF3 Hardware Attributes.
Definition: AESCCMLPF3.h:102
const uint8_t * input
Definition: AESCCMLPF3.h:114
AESCommonLPF3_Object common
Definition: AESCCMLPF3.h:112
#define AESCCMLPF3_AAD_BUFFER_SIZE
Definition: AESCCMLPF3.h:90
int_fast16_t AESCCMLPF3HSM_setMac(AESCCM_Handle handle, const uint8_t *mac, size_t macLength)
Function to set the mac for an AES CCM segmented operation. This API needs to be called only when the...
#define AES_BLOCK_SIZE
Block size in number of bytes.
Definition: AESCommonLPF3.h:85
volatile size_t totalCTRLengthRemaining
Definition: AESCCMLPF3.h:129
CryptoKeyKeyStore_PSA driver header.
AESCCM_CallbackFxn callbackFxn
Definition: AESCCMLPF3.h:120
AES Global configuration.
Definition: AESCommon.h:154
AESCCM_OperationUnion * operation
Definition: AESCCMLPF3.h:121
#define AES_IV_LENGTH_BYTES
Definition: AESCommonLPF3.h:92
size_t totalDataLength
Definition: AESCCMLPF3.h:126
volatile size_t totalAADLengthRemaining
Definition: AESCCMLPF3.h:142
const uint8_t * nonce
Definition: AESCCMLPF3.h:116
#define AESCommonLPF3_256_KEY_LENGTH_BYTES
Definition: AESCommonLPF3.h:78
#define AES_TAG_LENGTH_BYTES
Definition: AESCommonLPF3.h:93
size_t aadLength
Definition: AESCCMLPF3.h:140
AESCCMLPF3 Object.
Definition: AESCCMLPF3.h:109
size_t totalAADLength
Definition: AESCCMLPF3.h:125
size_t inputLength
Definition: AESCCMLPF3.h:122
uint8_t * output
Definition: AESCCMLPF3.h:115
AESCCM_OperationType operationType
Definition: AESCCMLPF3.h:130
void(* AESCCM_CallbackFxn)(AESCCM_Handle handle, int_fast16_t returnValue, AESCCM_OperationUnion *operation, AESCCM_OperationType operationType)
The definition of a callback function used by the AESCCM driver when used in AESCCM_RETURN_BEHAVIOR_C...
Definition: AESCCM.h:1148
AESCommonLPF3 Hardware Attributes.
Definition: AESCommonLPF3.h:103
psa_key_location_t KeyStore_PSA_KeyLocation
Definition: CryptoKeyKeyStore_PSA.h:251
const uint8_t * aad
Definition: AESCCMLPF3.h:113
bool segmentedOperationInProgress
Definition: AESCCMLPF3.h:154
volatile size_t totalDataLengthRemaining
Definition: AESCCMLPF3.h:141
Union containing a reference to a one step, segmented AAD, segmented data, or segmented finalize oper...
Definition: AESCCM.h:1106
AESCommon driver implementation for the Low Power F3 family.
volatile size_t inputCBCMACLengthRemaining
Definition: AESCCMLPF3.h:123
uint32_t tempAssetID
Definition: AESCCMLPF3.h:149
uint8_t macLength
Definition: AESCCMLPF3.h:133
volatile size_t totalCBCMACLengthRemaining
Definition: AESCCMLPF3.h:128
volatile size_t inputCTRLengthRemaining
Definition: AESCCMLPF3.h:124
size_t aadBytesProcessed
Definition: AESCCMLPF3.h:127
AESCCM_OperationType
Enum for the operation types supported by the driver.
Definition: AESCCM.h:1118
uint8_t * mac
Definition: AESCCMLPF3.h:117
uint32_t keyAssetID
Definition: AESCCMLPF3.h:150
int_fast16_t hsmStatus
The staus of the HSM Boot up process if HSMLPF3_STATUS_SUCCESS, the HSM booted properly. if HSMLPF3_STATUS_ERROR, the HSM did not boot properly.
Definition: AESCCMLPF3.h:148
uint8_t nonceLength
Definition: AESCCMLPF3.h:134
KeyStore_PSA_KeyLocation keyLocation
Definition: AESCCMLPF3.h:151
AESCommonLPF3 Object.
Definition: AESCommonLPF3.h:125
uint8_t bufferedAADLength
Definition: AESCCMLPF3.h:132