Create a Linux Bootable SD Card#
The simplest way to boot Linux is through a micro SD card flashed with a bootable Linux image. In this section, we will present two methods to create a micro SD card with a Linux image.
Warning
TI provides support for both the TDA4VM EVM and the TDA4VM Starter Kit. However the Starter Kit supports PROCESSOR-SDK-LINUX-SK-TDA4VM while the EVM supports the PROCESSOR-SDK-LINUX-J721E. So if you are running on the EVM, please refer to this Getting Started Guide. For Starter Kit, please go ahead and read this section.
Create SD Card Using balenaEtcher#
This method uses a popular GUI based tool, balenaEtcher, to write the Linux image to an SD card. It works on any platform (MS Windows, Linux, or Apple macOS). Please refer to the EVM Quick Start Guide provided in What is Needed to Evaluate Linux? for how to create an SD card using balenaEtcher.
Note
We have tested with Balena Etcher version 1.7.0 which can be found here, balena-io/etcher. There seems to be a known-issue with latest 1.7.2 version of Balena Etcher https://forums.balena.io/t/etcher-error-message-cannot-read-property-message-of-null/350471
Create SD Card Using Command Line#
This method uses Linux command line and the bmap tool to create an SD card with a Linux image. Follow the steps given below to flash the SD card:
Install the bmap tool if it’s not already installed:
$ sudo apt-get install bmap-tools
Insert a micro SD card to an SD card reader and plug the SD card reader into a Linux PC.
Unmount the SD card. Find the device name of the SD card using command “lsblk”, and then use command “umount” to unmout the SD card.
For example, if command “lsblk” returns:
$ lsblk NAME MAJ:MIN RM SIZE RO TYPE MOUNTPOINT : sdc 8:32 1 15G 0 disk ├─sdc1 8:33 1 131.8M 0 part /media/localUser/boot └─sdc2 8:34 1 765.9M 0 part /media/localUser/root
Then unmount sdc1 and sdc2 (the actual device name may be different on your Linux host):
$ sudo umount /media/localUser/boot $ sudo umount /media/localUser/root $ lsblk NAME MAJ:MIN RM SIZE RO TYPE MOUNTPOINT : sdc 8:32 1 15G 0 disk ├─sdc1 8:33 1 131.8M 0 part └─sdc2 8:34 1 765.9M 0 part
Flash the SD card with the Linux WIC image using the bmap tool. Make sure to use the correct image name and device name:
$ sudo bmaptool copy --nobmap tisdk-default-image-tda4vmx-evm.wic.xz /dev/sdc
Option “–nobmap” is used here to avoid needing to provide a bmap file.