The CC2652R7 LaunchPad™ (LP-CC2652R7) is a full-featured development kit for evaluating, developing and prototyping applications on the SimpleLink CC26x2R family of wireless MCUs. The CC2652R7 LaunchPad enables development of wireless applications for the SimpleLink CC2642R Bluetooth low energy wireless MCU supporting Bluetooth 5 LE, and both the CC2652R and CC2652R7 multi-standard wireless MCUs supporting IEEE 802.15.4 based protocols including Thread, ZigBee®, and TI 15.4 applications in addition to Bluetooth low energy (BLE). All SimpleLink CC26x2R wireless MCUs share the same memory layout, peripherals and processing capability with differences only in wireless protocol capability.
The CC26x2R family of wireless MCUs contain a 32-bit ARM® Cortex®-M4F processor running at 48 MHz as the main application processor, 704 kB of in-system programmable flash memory, 144 kB of low-leakage SRAM, a full complement of peripherals such as I2C, SPI and UART, advanced cryptography accelerators (ECC, AES256, SHA256, etc.) as well as a Sensor Controller Engine (SCE). The SCE is a 2nd programmable processor core ideal for ultra low-power sensor reading and data processing applications. The SCE runs independently from the main Cortex-M4F and handles sensor polling using just a few micro amps of average current. A dedicated Radio Controller (ARM Cortex-M0) handles low-level RF and physical layer (PHY) protocol commands that are stored in ROM or RAM, thus ensuring ultra-low power and great flexibility. A comprehensive list of capabilities can be found in the device data sheet and Technical Reference Manual.
The CC2652R7 LaunchPad kit is supported by the SimpleLink Starter app for iOS and Android. This app connects your LaunchPad to a smartphone using BLE and supports reading the LaunchPad button states, controlling LEDs and send strings of data to the UART backchannel. It also supports cloud connectivity to the IBM Quickstart server or to any cloud service via MQTT. This enables a cloud view where you can control your LaunchPad from any web browser in minutes after setting it up. Development with the CC2652R7 LaunchPad is supported by the SimpleLink CC13XX / CC26XX SDK containing protocol stack and sample application as well as a wide-range of free development tools such as Code Composer Studio™ (CCS) v10, SmartRF™ Studio and Sensor Controller Studio.
The CC2652R7 LaunchPad kit can also be upgraded to the latest firmware version or programmed with other wireless protocol demonstration firmware with the over-the-air download (OAD) capability in the SimpleLink Starter app, or programmed directly over USB from a PC using the Uniflash flash programming tool.
EnergyTrace is available on all CC13x2 and CC26x2 LaunchPads. The tool can be used stand-alone as a power profiling tool, or in EnergyTrace++ mode (4-pin JTAG required) within a debug session for state monitoring to help optimize the application for ultra-low-power consumption.
To use EnergyTrace the Power Jumper must be in the XDS110 Power position and the 3V3 jumper on the XDS header must be mounted to provide current to the target. The other jumpers on the XDS header are optional. EnergyTrace does only support 3.3 V supply voltage. Chapter 7 in the Measuring Current Consumption Application Report describes how to run EnergyTrace from CCS.
The LaunchPad is designed to be powered from a USB-compliant power source, either a USB charger or a computer. When used this way, jumpers need to be mounted on the 3V3 position of the central jumper block. An LDO powered from the USB VBUS supply supplies 3.3 V to the XDS110 debugger, the CC2652R7, and associated circuitry including the 3V3-marked pins for BoosterPacks.
The LaunchPad development kit is designed for operation from -25°C to +70°C. Note that other BoosterPack accessories and LaunchPads may have different temperature ranges, and when combined, the combination will be set by the most restrictive combined range. Also, if powering the LaunchPad from an external battery, ensure that you do not exceed the specified operating temperature of the battery.
The LP-CC2652R7 is pre-programmed with a Bluetooth 5 (BLE5-Stack) example peripheral project called Project Zero that allows wireless communication with smartphones and tablets over a BLE connection. Follow the few simple steps to get started with your new LaunchPad:
Follow the links below to explore the SimpleLink CC26XX MCU SDK in TI Resource Explorer.
Click the button below to flash your Launchpad and revert back to the out of the box functionality of your LaunchPad. When the flash tool is complete, it is required to reset the CC2652R7 by clicking on the reset button (next to the USB port). First time use of this tool will request a plug-in installation for flashing.
With Project Zero pre-programmed on LAUNCHXL-CC2652R7 you can change the stack with over-the-air download. The new Enhanched OAD lets you try out other compatible stacks in a few steps:
To restore to the factory image, press the left button during boot by:
To get up and running with your own application, head over to SimpleLink Academy which provides a comprehensive set of trainings for the SimpleLink MCU family. The table below shows Project Zero labs for the protocols that are supported by LAUNCHXL-CC2652R7.
| Stack | Lab | Description |
|---|---|---|
| BLE-5 | Bluetooth 5 Fundamentals | Setting up the BLE stack debug environment, connecting to Project Zero, performing basic reading and writing of GATT characteristic data, changing the advertisement/device name. |
| Thread | Thread CLI Project Zero | Introduction to TI-OpenThread using the command line example. |
| TI 15.4 | Sensor and Collector - TI 15.4-Stack Project Zero | Use TI 15.4-Stack and build the sensor and collector examples in order to create a star network. |
| Zigbee | Light and Switch - Zigbee Project Zero | Get started with Zigbee networking by forming a simple Zigbee network. |
| DMM | DMM Fundamentals | Use the Dynamic Multi-protocol Manager (DMM) to let multiple wireless stacks coexist and operate concurrently on one device. |
| Proprietary RF | Basic RX and TX | Use the RF driver, Code Composer Studio and SmartRF Studio to create a proprietary RF link. |
| Sensor Controller | Sensor Controller Fundamentals | Get up and running with the Sensor Controller and Sensor Controller Studio. |
The XDS jumper block in the middle of the board can be used to disconnect the upper section (XDS110 debugger) from the lower section containing the wireless MCU (CC2652R7). The jumpers are mounted by default. Which enables the CC2652R7 to be programmed and debugged by the XDS110.
The onboard XDS110 can be used to debug and program external MCU targets supported by the XDS110 debugger, such as CC13xx and CC26xx wireless MCUs. It is also possible to connect compatible external debuggers to the onboard CC2652R7. In either case, all the XDS jumpers on the jumper block must be removed.
With all the jumper block jumpers removed, the XDS110 Out header will work as debug output for the XDS110, and the Target In header will work as debug connector for the CC2652R7. The XDS110 output is level shifted and support target voltages between 1.8 V and 3.6 V. If the target board is powered externally, the Power Jumper must be moved to the external power position to set the correct level on the level shifters. The LaunchPad can also power the external board with 3.3 V, then the Power Jumper must be in the XDS110 Power position.
The CC2652R7 is by default powered from the LaunchPad's 3.3 V LDO. It is possible to run the device off different supply voltages by disconnecting the 3.3 V jumper and connecting a power supply between 1.8 V and 3.6 V to any of the pins marked 3V3. In this case the Power Jumper must be placed in the Extern Pwr position to connect the external supply to the XDS110 level shifters. Note that even though the supply voltage range of the CC2652R7 is up to 3.8 V, the maximum voltage in this case is limited by the level shifters at 3.6 V. When measuring current consumption, ensure that the serial (SPI) flash memory is placed into low power mode. Support for placing the serial flash into low power mode is provided in the LaunchPad board file included with the SimpleLink CC13XX / CC26XX SDK.
Texas Instruments declares that this product is in compliance with Directive 2014/53/EU. The compliance has been verified in the operating band of 2402 MHz to 2480 MHz at +5 dBm Tx Power setting. Should you choose to configure the EUT to operate outside of the test conditions, it should be operated inside a protected and controlled environment (such as, a shielded chamber). This evaluation board is only for development and not an end product. Developers and integrators that incorporate the chipset in any end products are responsible for obtaining applicable regulatory approvals for such end product.
Texas Instruments declares that this product is in compliance with the EU REACH regulation.