Introduction
This module is a study of the Angle of Arrival (AoA). AoA is a technique for finding the direction that an incoming packet is coming from. The estimated time to complete this lab is between 1-2 hours. It is assumed that the reader has a basic knowledge of embedded C tool chains and general C programming concepts.
This lab is based on the rtls_master, rtls_slave and rtls_passive projects that are part of
the SimpleLink™ CC2640R2 SDK.
First, the lab will cover an overview on how to get started with the AoA projects. Subsequent tasks of this lab will guide the user on how to customize these projects in order to answer most of the common AoA questions.
Prerequisites
Other SimpleLink Academy Labs
- Completion of Realtime Localization System Introduction
Required Training
It is required that users complete all steps of the RTLS Introduction lab before moving on to the Angle of Arrival lab. It is also assumed that the user has already installed the software, setup the hardware, and read the recommended chapters covered by the introduction lab. For brevity, only new content will be listed here.
Software for desktop development
- SimpleLink™ CC2640R2 SDK 3.30.00
- Required tools and version are listed in the CC2640R2 SDK 3.30.00 Release Notes
Hardware
This module requires the following kits:
- 3x CC2640R2-LAUNCHXL
- 1x BOOSTXL-AoA
Getting started with AoA booster pack
Getting started – Desktop
Install the Software
This lab requires that you have completed all the steps in the RTLS Introduction lab This means that you must have
- CC2640R2 SDK installed
- Working Python environment
- Used
rtls_example.pyscript that sets up an RTLS network.
Introduction to AoA
Bluetooth Core Specification Version 5.1 introduces AoA/AoD which are
covered under Direction Finding Using Bluetooth Low Energy section.
AoA is for receivers that have RF switches, multiple antennas, can switch antennas and capture I/Q samples when receiving direction finding packets.
AoD is for transmitters that have RF switches, multiple antennas and can switch antennas when transmitting direction finding packets. And recieivers only have one antenna but can capture I/Q samples when receiving direction finding packets.
In the table below and throughout this lab CTE is used in place of Constant Tone Extension as defined by the BLE specification.
| Direction Finding Method | Transmitter | Receiver |
|---|---|---|
| AoA | Single antenna, transmit CTE | Multiple antennas, RF switches, can switch antennas while capturing I/Q data of the CTE |
| AoD | Multiple antennas, RF switches, transmits CTE while switching antennas | Single antenna, can capture I/Q data of the CTE |
On top of that, the Bluetooth Core Specification version 5.1 specifies the following states can support sending direction finding packets:
- Periodic advertising; also called
Connectionless CTE - Connection; also called
Connection CTE
The theory behind AoA/AoD and Connectionless/Connection CTE is the same, therefore in this SimpleLink Academy training, we will only focus on Connection CTE AoA.
We will explain the AoA theory first and the walk through our SimpleLink CC2640R2F SDK offering.
AoA measurement is typically a 3-step process:
- Collect phase information by sampling the I/Q
- Calculate the phase difference among the antennas
- Covert the phase difference into Angle of Arrival
1. Collect phase information by sampling the I/Q
When two (or more) antennas are placed at a given distance apart from each other, their received RF signals will have a phase difference that is proportional to the difference between their respective distances from the transmitter.
Typically, the signal from one antenna will be a delayed version of the signal from the other antenna. If they are sufficiently close (less than Λ(wavelength)/2 between phase centers), you can always determine which is closest to the transmitter.
These path length differences will depend on the direction of the incoming RF waves relative to the antennas in the array. In order to measure the phase difference accurately, the radio wave packet must contain a section of constant tone with whitening disabled where there are no phase shifts caused by modulation.
Constant Tone Extension (CTE)
The constant tone extension is a section of consecutive 1's without whitening, which is effectively a +250kHz wave on top of the carrier wave. In the Bluetooth Core Specification Version 5.1, both periodic advertising packets and connection packets can contain a constant tone extension(CTE) after the CRC. The CTE can only be sent using uncoded PHY.

2. Calculate the phase difference among the antennas
Phase Difference (Φ) is measured by connecting at least two antennas to the same receiver sequentially (more antennas can be added).


In order to get a good estimate of Φ (phase), all other intentional phase shifts in the signal should be removed. Connection CTE AoA solution achieves this by adding CTE at the end of packets.
![]() |
|---|
| Connection CTE Packet Format |
Data Physical Packet format
The grey colored part of the packet shown above means
it's optional. The Constant Tone Extension is only enabled when the CP bit
in the Data Physical PDU header is set. The detail of the Constant Tone
Extension is then specified by the CTEInfo field in the in the Data
Physical PDU.
This gives the receiver time to synchronize the demodulator first, and then store the I/Q samples from the CTE into radio RAM. The I/Q data is then extracted by the application layer.
I/Q samples are used to estimate phase difference among antennas. When the receiver gets AoA packets, the RF core will trigger an event that will lead to start of the antenna switching. The RF core will start sampling the I/Q data after the guard period of the CTE and the sampled data will be stored in the radio RAM.
By comparing the I/Q data collected from different antennas, users can get the relative phase difference among antennas.
3. Convert the phase difference into Angle of Arrival
Last step is converting the phase shift (Φ) back to AoA (Θ).
If Φ is negative, this means that antenna 2 is ahead of antenna 1.
In this case Θ is negative too but this does not cause any
mathematical problem as sin() and arcsin() functions are defined
both for positive and negative numbers. To avoid any unnecessary complications
we will consider here Φ to be positive.
The angle between the incident wave and antenna array is Θ. Base on the picture below we know that the sin(Θ) = r/d, and d is the distance between antenna 1 and antenna 2 which is known. Then all we need to find out is r.
r is the distance to antenna 2 that the incident wave needs to travel after arriving at antenna 1. We have found that the phase difference between antenna 1 and antenna 2 is Φ, so the extra distance r is equal to wavelength of the incoming signal * Φ/(2Π).
r= Λ* Φ/(2Π)


Note
In rtls_passive example, you might notice that step 3 is not implemented.
The reason is simply because by step 2 using our
BOOSTXL-AoA we already have
linear result from +/-90 degree using antenna pair[1,2] and pair[2,3].
Therefore all we need is to have a look up table to do the fine tuning.
This saves computation time/current consumption compared to doing another arcsin function.
We also tried to do arcsin, but the result is pretty much the same as adding gain and offset after step 2.
What technique does AoA use to identify the direction of incident wave?
Task 1 – Running the AoA application
Have you moved the capacitor C51 of your LaunchPad to use external antenna?
If you have no idea what I am talking about, it's time for you to read the "Preparations" chapter of the Angle of Arrival BoosterPack Getting Started guide :)
The SimpleLink™ CC2640R2 SDK
has three examples dedicated to performing AoA (rtls_master,
rtls_slave and rtls_passive).
In the TI BLE-Stack User's Guide → RTLS Toolbox → Angle of Arrival → AoA application Overview, we have covered how the application works.
Therefore, after following the instruction on Realtime Localization System Introduction, you should be able to get it up and running.
Task 2 – Modify AoA application to use only one antenna array
The out of box SimpleLink™ CC2640R2 SDK
rtls_passive example will stay on one antenna array when receiving
one AoA packet and
then change to another antenna array for the next AoA packet.
Following code contains the logic for antenna array switching.
// Switch ant array
if (gAoaReport.antConfig == antA1Config)
{
gAoaReport.antConfig = antA2Config;
gAoaReport.antResult = antA2Result;
}
else if (gAoaReport.antConfig == antA2Config)
{
gAoaReport.antConfig = antA1Config;
gAoaReport.antResult = antA1Result;
}
else
{
// Should not get here
return;
}
AOA.c::AOA_setupNextRun()
The angle is then decided once both arrays have received AoA packets and judge by the rssi value of the received packet to decide whether the application should trust angle derived from array 1 or array 2.
// Signal strength is higher on A1 vs A2
if (antA1Result->rssi > antA2Result->rssi)
{
// Use AoA from Antenna Array A1
AoA_ma.array[AoA_ma.idx] = AoA_A1;
AoA_ma.currentAoA = AoA_A1;
AoA_ma.currentAntennaArray = 1;
AoA_ma.currentRssi = antA1Result->rssi;
AoA_ma.currentSignalStrength = signalStrength_A1;
AoA_ma.currentCh = antA1Result->ch;
AoA.currentangle = AoA_A1;
}
// Signal strength is higher on A2 vs A1
else
{
// Use AoA from Antenna Array A2
AoA_ma.array[AoA_ma.idx] = AoA_A2;
AoA_ma.currentAoA = AoA_A2;
AoA_ma.currentAntennaArray = 2;
AoA_ma.currentRssi = antA2Result->rssi;
AoA_ma.currentSignalStrength = signalStrength_A2;
AoA_ma.currentCh = antA2Result->ch;
AoA.currentangle = AoA_A2;
}
rtls_ctrl_aoa.c::RTLSCtrl_estimateAngle()
However, this might not be how you want to design or utilize your antennas. Therefore, this section we will walk you through the changes if you only want one antenna array, like Automotive Bluetooth low energy car access satellite node reference design
We will go from this configuration:

To this configuration (using antenna array #1):

The steps below will guide you through the process of removing one of the antenna
array. For this example we will be removing A2, but these steps are also
applicable in case that A1 needs to be removed.
- Start from the
rtls_passive_cc2640r2lp_appproject and rename it tortls_passive_cc2640r2lp_a1_app - Exclude the files
ant_array2_config_boostxl_rev1v1.candant_array2_config_boostxl_rev1v1.hfrom the build. - Comment out all of the antenna array 2 dependencies from
AOA.c
//Comment out all the followings lines
//line 64
#include "ant_array2_config_boostxl_rev1v1.h"
// Remove config and result declarations line ~170
AoA_AntennaConfig *antA2Config = &BOOSTXL_AoA_Config_ArrayA2;
AoA_AntennaResult *antA2Result = &BOOSTXL_AoA_Result_ArrayA2;
//line 399, 402 and 405 in AOA_init()
BOOSTXL_AoA_AntennaPattern_A2_init();
antA2Result->updated = false;
aoaResults->antA2Result = antA2Result;
//line 730~733 in AOA_getActiveAnt()
else if (gAoaReport.antConfig == antA2Config)
{
return 2;
}
//line 756~760 in AOA_setupNextRun()
else if (gAoaReport.antConfig == antA2Config)
{
gAoaReport.antConfig = antA1Config;
gAoaReport.antResult = antA1Result;
}
Change the following lines in AOA.c to take antenna 1 instead.
//line 753 and 754 in AOA_setupNextRun() // Switch ant array if (gAoaReport.antConfig == antA1Config) { gAoaReport.antConfig = antA1Config; gAoaReport.antResult = antA1Result; }c
Replace the content of RTLSCtrl_postProcessAoa in
rtls_ctrl_aoa.cwith the provided code snippet. What we have done here is to remove all the antenna array 2 dependency.void RTLSCtrl_postProcessAoa(rtlsAoa_t *aoaControlBlock, int8_t rssi, uint8_t channel) { uint8_t status; if (aoaControlBlock->aoaParams.aoaRole == AOA_ROLE_PASSIVE) { status = AOA_postProcess(rssi, channel); if (status) { switch(aoaControlBlock->aoaParams.resultMode) { case AOA_MODE_ANGLE: { AoA_Sample aoaTempResult; rtlsAoaResultAngle_t aoaResult; AOA_getPairAngles(); { gAoaResults.antA1Result->updated = false; const AoA_AntennaResult *antA1Result = gAoaResults.antA1Result; aoaTempResult = RTLSCtrl_estimateAngle(antA1Result); aoaResult.angle = aoaTempResult.angle; aoaResult.antenna = aoaTempResult.antenna; aoaResult.rssi = aoaTempResult.rssi; aoaResult.channel = aoaTempResult.channel; RTLSHost_sendMsg(RTLS_CMD_AOA_RESULT_ANGLE, HOST_ASYNC_RSP, (uint8_t *)&aoaResult, sizeof(rtlsAoaResultAngle_t)); } } break; case AOA_MODE_PAIR_ANGLES: { rtlsAoaResultPairAngles_t aoaResult; int16_t *pairAngle; uint8_t antenna; AOA_getPairAngles(); if (gAoaResults.antA1Result->updated == true) { pairAngle = gAoaResults.antA1Result->pairAngle; gAoaResults.antA1Result->updated = false; antenna = 1; } else { // Should not get here return; } aoaResult.rssi = rssi; aoaResult.channel = channel; aoaResult.antenna = antenna; for (int i = 0; i < AOA_NUM_ANTENNAS; i++) { aoaResult.pairAngle[i] = pairAngle[i]; } RTLSHost_sendMsg(RTLS_CMD_AOA_RESULT_PAIR_ANGLES, HOST_ASYNC_RSP, (uint8_t *)&aoaResult, sizeof(rtlsAoaResultPairAngles_t)); } break; case AOA_MODE_RAW: { rtlsAoaResultRaw_t *aoaResult; uint16_t numAoaSamples; uint16_t samplesToOutput; AoA_IQSample *pIter; aoaResult = RTLSCtrl_malloc(sizeof(rtlsAoaResultRaw_t) + (MAX_SAMPLES_SINGLE_CHUNK * sizeof(AoA_IQSample))); pIter = AOA_getRawSamples(); // If the array is not empty if (pIter != NULL && aoaResult != NULL) { // Calculate how many samples we will be outputting numAoaSamples = AOA_calcNumOfCteSamples(aoaControlBlock->aoaParams.cteTime, aoaControlBlock->aoaParams.cteScanOvs, aoaControlBlock->aoaParams.cteOffset); aoaResult->channel = channel; aoaResult->rssi = rssi; aoaResult->samplesLength = numAoaSamples; aoaResult->antenna = AOA_getActiveAnt(); aoaResult->offset = 0; do { // If the remainder is larger than buff size, tx maximum buff size if (aoaResult->samplesLength - aoaResult->offset > MAX_SAMPLES_SINGLE_CHUNK) { samplesToOutput = MAX_SAMPLES_SINGLE_CHUNK; } else { // If not, then output the remaining data samplesToOutput = aoaResult->samplesLength - aoaResult->offset; } // Copy the samples to output buffer for (int i = 0; i < samplesToOutput; i++) { aoaResult->samples[i] = pIter[i]; } RTLSHost_sendMsg(RTLS_CMD_AOA_RESULT_RAW, HOST_ASYNC_RSP, (uint8_t *)aoaResult, sizeof(rtlsAoaResultRaw_t) + (sizeof(AoA_IQSample) * samplesToOutput)); aoaResult->offset += samplesToOutput; pIter += MAX_SAMPLES_SINGLE_CHUNK; } while (aoaResult->offset < aoaResult->samplesLength); } if (aoaResult) { RTLSUTIL_FREE(aoaResult); } } break; default: break; } // Once all post processing is complete, set up the next run AOA_setupNextRun(); } } }rtls_ctrl_aoa.c:: RTLSCtrl_postProcessAoa
Replace the content of RTLSCtrl_estimateAngle in
rtls_ctrl_aoa.cwith the provided code snippet. What we have done here is to remove all the antenna array 2 dependency and modify the function call to take one array only when making an angle decision.//line 122 under local function section AoA_Sample RTLSCtrl_estimateAngle(const AoA_AntennaResult *antA1Result);// The function itself AoA_Sample RTLSCtrl_estimateAngle(const AoA_AntennaResult *antA1Result) { AoA_Sample AoA; static AoA_movingAverage AoA_ma; uint8_t AoA_ma_size = sizeof(AoA_ma.array) / sizeof(AoA_ma.array[0]); // Calculate AoA for each antenna array const int16_t AoA_A1 = ((antA1Result->pairAngle[0] + antA1Result->pairAngle[1]) / 2) + antA1Result->channelOffset[antA1Result->ch]; // Calculate average signal strength const int16_t signalStrength_A1 = (antA1Result->signalStrength[0] + antA1Result->signalStrength[1]) / 2; // Use AoA from Antenna Array A1 AoA_ma.array[AoA_ma.idx] = AoA_A1; AoA_ma.currentAoA = AoA_A1; AoA_ma.currentAntennaArray = 1; AoA_ma.currentRssi = antA1Result->rssi; AoA_ma.currentSignalStrength = signalStrength_A1; AoA_ma.currentCh = antA1Result->ch; AoA.currentangle = AoA_A1; // Add new AoA to moving average AoA_ma.array[AoA_ma.idx] = AoA_ma.currentAoA; // Calculate new moving average AoA_ma.AoAsum = 0; for(uint8_t i = 0; i < AoA_ma_size; i++) { AoA_ma.AoAsum += AoA_ma.array[i]; } AoA_ma.AoA = AoA_ma.AoAsum / AoA_ma_size; // Update moving average index if(AoA_ma.idx >= (AoA_ma_size - 1)) { AoA_ma.idx = 0; } else { AoA_ma.idx++; } // Return results AoA.angle = AoA_ma.AoA; AoA.rssi = AoA_ma.currentRssi; AoA.signalStrength = AoA_ma.currentSignalStrength; AoA.channel = AoA_ma.currentCh; AoA.antenna = AoA_ma.currentAntennaArray; return AoA; }rtls_ctrl_aoa.c::RTLSCtrl_estimateAngle
When complete, re-run the rtls_example_with_rtls_util.py, you will observe that all results show antenna 1. See below for example. Note the device address will be different for your launchpad.
[10:18:2019 10:08:13:829688] : {"name": "CC2640r2 AOA Passive", "type": "aoa", "identifier": "54:6C:0E:9F:D4:25", "payload": {"angle": 35, "rssi": -56, "antenna": 1, "channel": 7}}
[10:18:2019 10:08:13:982572] : {"name": "CC2640r2 AOA Passive", "type": "aoa", "identifier": "54:6C:0E:9F:D4:25", "payload": {"angle": 34, "rssi": -56, "antenna": 1, "channel": 0}}
[10:18:2019 10:08:14:184615] : {"name": "CC2640r2 AOA Passive", "type": "aoa", "identifier": "54:6C:0E:9F:D4:25", "payload": {"angle": 35, "rssi": -57, "antenna": 1, "channel": 30}}
[10:18:2019 10:08:14:385083] : {"name": "CC2640r2 AOA Passive", "type": "aoa", "identifier": "54:6C:0E:9F:D4:25", "payload": {"angle": 34, "rssi": -56, "antenna": 1, "channel": 8}}
[10:18:2019 10:08:14:587084] : {"name": "CC2640r2 AOA Passive", "type": "aoa", "identifier": "54:6C:0E:9F:D4:25", "payload": {"angle": 35, "rssi": -58, "antenna": 1, "channel": 16}}
[10:18:2019 10:08:14:789337] : {"name": "CC2640r2 AOA Passive", "type": "aoa", "identifier": "54:6C:0E:9F:D4:25", "payload": {"angle": 34, "rssi": -56, "antenna": 1, "channel": 9}}
[10:18:2019 10:08:14:991393] : {"name": "CC2640r2 AOA Passive", "type": "aoa", "identifier": "54:6C:0E:9F:D4:25", "payload": {"angle": 35, "rssi": -56, "antenna": 1, "channel": 2}}
[10:18:2019 10:08:15:194291] : {"name": "CC2640r2 AOA Passive", "type": "aoa", "identifier": "54:6C:0E:9F:D4:25", "payload": {"angle": 35, "rssi": -56, "antenna": 1, "channel": 32}}
[10:18:2019 10:08:15:395712] : {"name": "CC2640r2 AOA Passive", "type": "aoa", "identifier": "54:6C:0E:9F:D4:25", "payload": {"angle": 34, "rssi": -57, "antenna": 1, "channel": 10}}
[10:18:2019 10:08:15:597805] : {"name": "CC2640r2 AOA Passive", "type": "aoa", "identifier": "54:6C:0E:9F:D4:25", "payload": {"angle": 35, "rssi": -57, "antenna": 1, "channel": 3}}
Task 3 – Modify AoA application to use only two antennas
Now we have successfully moved from using 2 antenna arrays to 1. We will use the example from Task 2 as the baseline and make the proper changes so we only use 2 antennas from the antenna array 1.
Task 2 is using all 3 antennas from
A1:
And the end goal is using the following:

The following steps will guide you through this process:
Comment out the following in
ant_array1_config_boostxl_rev1v1.c(the file is in Drivers/AOA).//line 58 #define AOA_Ax_ANT3 AOA_PIN(IOID_30) //line 131~144 {// v23 .a = 1, .b = 2, .sign = 1, .offset = -5, .gain = 0.9, }, {// v13 .a = 0, .b = 2, .sign = 1, .offset = -20, .gain = 0.50, },Replace the antenna toggling patten
antennaPattern_A1in ant_array1_config_boostxl_rev1v1.c with the provided pattern to removeA1.3.AoA_Pattern antennaPattern_A1 = { .numPatterns = 32, .initialPattern = AOA_A1_SEL | AOA_Ax_ANT2, .toggles = { AOA_A1_SEL | AOA_Ax_ANT1, // A1.1 AOA_A1_SEL | AOA_Ax_ANT2, // A1.2 AOA_A1_SEL | AOA_Ax_ANT1, // A1.1 AOA_A1_SEL | AOA_Ax_ANT2, // A1.2 AOA_A1_SEL | AOA_Ax_ANT1, // A1.1 AOA_A1_SEL | AOA_Ax_ANT2, // A1.2 AOA_A1_SEL | AOA_Ax_ANT1, // A1.1 AOA_A1_SEL | AOA_Ax_ANT2, // A1.2 AOA_A1_SEL | AOA_Ax_ANT1, // A1.1 AOA_A1_SEL | AOA_Ax_ANT2, // A1.2 AOA_A1_SEL | AOA_Ax_ANT1, // A1.1 AOA_A1_SEL | AOA_Ax_ANT2, // A1.2 AOA_A1_SEL | AOA_Ax_ANT1, // A1.1 AOA_A1_SEL | AOA_Ax_ANT2, // A1.2 AOA_A1_SEL | AOA_Ax_ANT1, // A1.1 AOA_A1_SEL | AOA_Ax_ANT2, // A1.2 AOA_A1_SEL | AOA_Ax_ANT1, // A1.1 AOA_A1_SEL | AOA_Ax_ANT2, // A1.2 AOA_A1_SEL | AOA_Ax_ANT1, // A1.1 AOA_A1_SEL | AOA_Ax_ANT2, // A1.2 AOA_A1_SEL | AOA_Ax_ANT1, // A1.1 AOA_A1_SEL | AOA_Ax_ANT2, // A1.2 AOA_A1_SEL | AOA_Ax_ANT1, // A1.1 AOA_A1_SEL | AOA_Ax_ANT2, // A1.2 AOA_A1_SEL | AOA_Ax_ANT1, // A1.1 AOA_A1_SEL | AOA_Ax_ANT2, // A1.2 AOA_A1_SEL | AOA_Ax_ANT1, // A1.1 AOA_A1_SEL | AOA_Ax_ANT2, // A1.2 AOA_A1_SEL | AOA_Ax_ANT1, // A1.1 AOA_A1_SEL | AOA_Ax_ANT2, // A1.2 AOA_A1_SEL | AOA_Ax_ANT2, // A1.2 stay with antenna 2 at the end AOA_A1_SEL | AOA_Ax_ANT2, // A1.2 } };Using different antennas instead of A1.1 and A1.2
Our example code always uses antenna A1.2 or A2.2 to receive packets before the CTE. This is set by the code below
.initialPattern = AOA_A1_SEL | AOA_Ax_ANT2,antennaPattern_A1[] :: ant_array1_config_boostxl_rev1v1.c
Therefore, for users using antennas other than A1.2 or A2.2, you will need to modify the initialPattern too.
Change the AOA_NUM_ANTENNAS to 2 in
AOA.h// line 74 #define AOA_NUM_ANTENNAS 2The IOs that control the antenna switches are initialized in
AOA.c::AOA_openPinsTherefore, we need to modify this part of the code since we are using one less IO. Change the pinMask to the following//line 297 and line 323 pinMask = (1 << IOID_27 | 1 << IOID_28 | 1 << IOID_29 );
Fundamental done
Now the application only uses antenna A1.1 and A1.2! Very well done! And the updated software still works with RTLS_Monitor GUI and the python scripts provided
Task 4 – Export raw IQ samples to CSV file
Python solution
The goal of this task is to understand how the script
rtls_aoa_iq_with_rtls_util_export_into_csv.py (stored in your SDK
under tools\ble5stack\rtls_agent\examples)is made.
We will guide you step by step in order to rewrite it. You can directly
jump to the next task if you are not interested in this part...
however it is always cool to discover how the magic happens :)
1- Where does the I/Q Samples come from?
So far we have worked on the application code to modify the
rtls_passive to work with custom HW. We will now spend some
time looking into the I/Q data.
The reason for checking I/Q data is that different HW design will yield different result which will affect your own angle calculation algorithm. For example, if the rf switches you are using need longer settling time than the ones on BOOSTXL-AoA, then you will need to discard more I/Q samples when doing calculations.
To decide how many I/Q samples you can use, you will need to extract I/Q samples and calculate phase to determine at which samples antennas are changing.
We will first take a look at where I/Q samples are stored and in what format.
I/Q is stored in the radio core RAM(RFC_RAM_BASE + 0x0000C000) and each I/Q pair takes up 32 bits space where I is stored in the lower 16 bits and Q is stored in higher 16 bits.
void AOA_getRxIQ(uint8_t *packetId, AoA_IQSample **samples)
{
// Should only be called when RF Core is awake
*packetId = (*((uint8_t*)AOA_PACKET_RAM));
*samples = packetId ? (AoA_IQSample *)&HWREG(RFC_RAM_BASE + 0x0000C000):NULL;
}
In AOA.c
I/Q samples resolution
I and Q samples only have 13 bits resolution even though they occupy 16 bits space in radio core RAM. Since they only have 13 bits resolution, the maximum and minimum value you will observe as signed integers are [4095, -4096].
2- How to send the I/Q samples to the computer?
If you haven't done it yet, change the COM port used by the script.
{"com_port": "COM39", "baud_rate": 460800, "name": "CC2640r2 AOA Master"}, {"com_port": "COM55", "baud_rate": 460800, "name": "CC2640r2 AOA Passive"}Set up the COM ports used
To extract the I/Q data from embedded devices over UART, we need to make sure that we have enough time to flush the I/Q data before next AoA packet arrives.
To achieve this, there are two options:
Increase the connection interval. In the
rtls_masterreadme file, it's mentioned that the connection interval should be larger than 300ms to acommodate outputting all the samples.Increase the UART baurate
For SDK 3.30 and latter, the default UART baudrate is set to 460800. This value is set and can be modified in the function
RTLSHost_openHostIf(in the filertls_host_npi.c, stored in the folderRTLSCtrl.)npiPortParams.portParams.uartParams.baudRate = 921600;Change baudrate (for example) to 921600
If you modify the baudrate in the embedded code, don't forget to modify the baudrate used by the python script to communicate with the devices...
{"com_port": "COM39", "baud_rate": 921600, "name": "CC2640r2 AOA Master"}, {"com_port": "COM55", "baud_rate": 921600, "name": "CC2640r2 AOA Passive"}Set up the baudrates used
In this lab we will increase connection interval to 500ms and leave the baudrate as is.
→ Change the
connect_interval_mSecparameter to the following code inrtls_example_with_rtls_util.py.connect_interval_mSec = 500Set up connection interval to be 500ms
This parameter will later be used in the ble_connect API as shown below
rtlsUtil.ble_connect(slave_bd_addr, connect_interval_mSec)Post Processing on Embedded Device
For users that will do I/Q data post process on chip, there is no limitation on the connection interval.
Now we will build on top of the python script that is used in Realtime Localization System Introduction
First we create a csv file to store I/Q data for analyzing later if needed. Normally, this code is already written in your
rtls_aoa_iq_with_rtls_util_export_into_csv.pyfile, in the functioninitialize_csv_file. This function assumes that you have properly imported the csv package and declared the global variables csv_writer and csv_row. You can change thefilenameto whichever suits you better.global csv_writer global csv_row # Prepare csv file to save data data_time = datetime.datetime.now().strftime("%m_%d_%Y_%H_%M_%S") filename = f"{data_time}_rtls_raw_iq_samples.csv" outfile = open(filename, 'w', newline='') csv_fieldnames = ['pkt', 'sample_idx', 'rssi', 'ant_array', 'channel', 'i', 'q'] csv_row = namedtuple('csv_row', csv_fieldnames) csv_writer = csv.DictWriter(outfile, fieldnames=csv_fieldnames) csv_writer.writeheader()Create a csv file to log I/Q data
The devices must be reseted, then the master can scan and connect
## Reset the passive and the master rtlsUtil.reset_devices() ##... ## Ask the master to scan scan_results = rtlsUtil.scan(scan_time_sec) ##... ## Ask the master to connect a device rtlsUtil.ble_connect(scan_results[0], connect_interval_mSec)Set the parameter to configure the devices
Once the slave and the master are connected, we can start the setup of AoA parameters
To extract I/Q data, the AoA operation mode needs to be
AOA_MODE_RAW. If needed, modify in the aoa_params structure, modify the aoa_run_mode to the following:aoa_params = { "aoa_run_mode": "AOA_MODE_RAW", "aoa_cc2640r2": { "aoa_cte_scan_ovs": 4, "aoa_cte_offset": 4, "aoa_cte_length": 20 }, "aoa_cc26x2": { "aoa_slot_durations": 2, "aoa_sample_rate": 4, "aoa_sample_size": 2, "aoa_sampling_control": 0, "aoa_sampling_enable": 1, "aoa_num_of_ant": 3, "aoa_ant_array_switch": 27, "aoa_ant_array": [28, 29, 30] } }Set the parameter to configure the devices
Let's have a look to the mode that used after a BLE connection has been established. Basically, the data are written to the .csv file until a STOP command is received.
try: data = q.get(block=True, timeout=0.5) if isinstance(data, dict): data_time = datetime.datetime.now().strftime("[%m:%d:%Y %H:%M:%S:%f] :") print(f"{data_time} {json.dumps(data)}") offset = data['payload'].offset payload = data['payload'] # If we have data, and offset is 0, we are done with one dump if offset == 0 and len(dump_rows): pkt_cnt += 1 # Make sure the samples are in order dump_rows = sorted(dump_rows, key=lambda s: s.sample_idx) # Write to file for sample_row in dump_rows: csv_writer.writerow(sample_row._asdict()) # Reset payload storage dump_rows = [] # Save samples for writing when dump is complete for sub_idx, sample in enumerate(payload.samples): sample = csv_row(pkt=pkt_cnt, sample_idx=offset + sub_idx, rssi=payload.rssi, ant_array=payload.antenna, channel=payload.channel, i=sample.i, q=sample.q) dump_rows.append(sample) elif isinstance(data, str) and data == "STOP": print("STOP Command Received") # If we have data, and offset is 0, we are done with one dump if len(dump_rows): # Make sure the samples are in order dump_rows = sorted(dump_rows, key=lambda s: s.sample_idx) # Write to file for sample_row in dump_rows: csv_writer.writerow(sample_row._asdict()) break else: pass except queue.Empty: continueScript's main loop (in results_parsing subfunction)
Log file
By default, the script produces a log file. This file is stored in the same path as the .csv file (i.e. in the directory from where the script was run) and can be useful for debug.
After running the script, you can see the following format in the csv file.

Remark 1: The names of the columns when the CSV is iniatized.
csv_fieldnames = ['pkt', 'sample_idx', 'rssi', 'ant_array', 'channel', 'i', 'q']
csv_row = namedtuple('csv_row', csv_fieldnames)
csv_writer = csv.DictWriter(outfile, fieldnames=csv_fieldnames)
csv_writer.writeheader()
Remark 2: The data written in each column are chosen by the following code.
# Samples are prepared
sample = csv_row(pkt=pkt_cnt, sample_idx=offset + sub_idx, rssi=payload.rssi,
ant_array=payload.antenna, channel=payload.channel, i=sample.i, q=sample.q)
dump_rows.append(sample)
#...
# Samples are written to the CSV file latter
for sample_row in dump_rows:
csv_writer.writerow(sample_row._asdict())
3- How to treat the I/Q samples on the computer?
Here we are only interested in the payload part of the AOA_MODE_RAW command. The AOA_MODE_RAW payload has the following structure. In the python script provided above, we have extracted most of the information and save them to a csv file.
struct = Struct(
"rssi" / Int8sl,
"antenna" / Int8ul,
"channel" / Int8ul,
"offset" / Int16ul,
"samplesLength" / Int16ul,
"samples" / GreedyRange(Struct(
"q" / Int16sl,
"i" / Int16sl,
)),
)
ss_rtls.py::class AoaResultRaw
New Python Packages
For the script below you will have to install the following new Python packages
- pandas
- matplotlib
They can be installed with pip. Consult the RTLS Intro lab for more information on how to install packages from pip.
import matplotlib.pyplot as plt
import pandas as pd
import math
def cal_magnitude(q_value,i_value):
return math.sqrt(math.pow(q_value,2)+math.pow(i_value,2))
def cal_phase(q_value,i_value):
return math.degrees(math.atan2(q_value,i_value))
if __name__ == "__main__":
df = pd.read_csv('sla_rtls_raw_iq_samples.csv')
AOA_RES_MAX_SIZE=81
# We only want one set of data per channel
df = df.drop_duplicates(subset=['channel','sample_idx'] , keep='first')
# We Calculate the phase and the margin
df['phase'] = df.apply(lambda row: cal_phase(row['q'], row['i']), axis=1)
df['magnitude'] = df.apply(lambda row: cal_magnitude(row['q'], row['i']), axis=1)
# Plot all the I/Q collected. Each channel will have a plot which contains I/Q samples.
# If you have collected I/Q data on 37 data channels, then there will be 37 windows popped up
grouped = df.groupby('channel')
grouped[['i', 'q']].plot(title="I/Q samples", grid=True)
plt.show()
# Create 4 plots and each plot has x number of subplots. x = number of channels
indexed = df.set_index(['channel', 'sample_idx'])
indexed.unstack(level=0)[['phase']].plot(subplots=True, title="Phase information", xlim=[0,AOA_RES_MAX_SIZE], ylim=[-190,+190])
indexed.unstack(level=0)[['magnitude']].plot(subplots=True, title="Signal magnitude", xlim=[0,AOA_RES_MAX_SIZE])
indexed.unstack(level=0)[['i']].plot(subplots=True, title="I samples", xlim=[0,AOA_RES_MAX_SIZE])
indexed.unstack(level=0)[['q']].plot(subplots=True, title="Q samples", xlim=[0,AOA_RES_MAX_SIZE])
plt.show()
This script can be executed as is.
After executing the small script provided above, if the angle between rtls_passive
rtls_slave is not 0 degree, you can see that magnitude of the sine wave is not the same
when you swap betwen antenna 1 and antenna 2 as shown below.

Another alternative to observe the magnitude of received signal is to calculate it based on I/Q data. Since each I/Q pair is a vector, the magnitude of a vector can be calculated by sqrt(I^2+Q^2).
Using the script provided above, you will see a plot called Signal magnitude. In this plot, you can clear see that received signal magnitude from antenna 2 is almost double as from antenna 1.

More information!
If there is no antenna toggling, then the I/Q samples will form a perfect sine wave. To prove it, change the antenna toggling pattern from 2 antennas to 1 antenna(A1.2), and see how the I/Q plots look like.
AoA_Pattern antennaPattern_A1 = {
.numPatterns = 32,
.initialPattern = AOA_A1_SEL | AOA_Ax_ANT2,
.toggles =
{
AOA_A1_SEL | AOA_Ax_ANT2, // A1.2
AOA_A1_SEL | AOA_Ax_ANT2, // A1.2
AOA_A1_SEL | AOA_Ax_ANT2, // A1.2
AOA_A1_SEL | AOA_Ax_ANT2, // A1.2
AOA_A1_SEL | AOA_Ax_ANT2, // A1.2
AOA_A1_SEL | AOA_Ax_ANT2, // A1.2
AOA_A1_SEL | AOA_Ax_ANT2, // A1.2
AOA_A1_SEL | AOA_Ax_ANT2, // A1.2
AOA_A1_SEL | AOA_Ax_ANT2, // A1.2
AOA_A1_SEL | AOA_Ax_ANT2, // A1.2
AOA_A1_SEL | AOA_Ax_ANT2, // A1.2
AOA_A1_SEL | AOA_Ax_ANT2, // A1.2
AOA_A1_SEL | AOA_Ax_ANT2, // A1.2
AOA_A1_SEL | AOA_Ax_ANT2, // A1.2
AOA_A1_SEL | AOA_Ax_ANT2, // A1.2
AOA_A1_SEL | AOA_Ax_ANT2, // A1.2
AOA_A1_SEL | AOA_Ax_ANT2, // A1.2
AOA_A1_SEL | AOA_Ax_ANT2, // A1.2
AOA_A1_SEL | AOA_Ax_ANT2, // A1.2
AOA_A1_SEL | AOA_Ax_ANT2, // A1.2
AOA_A1_SEL | AOA_Ax_ANT2, // A1.2
AOA_A1_SEL | AOA_Ax_ANT2, // A1.2
AOA_A1_SEL | AOA_Ax_ANT2, // A1.2
AOA_A1_SEL | AOA_Ax_ANT2, // A1.2
AOA_A1_SEL | AOA_Ax_ANT2, // A1.2
AOA_A1_SEL | AOA_Ax_ANT2, // A1.2
AOA_A1_SEL | AOA_Ax_ANT2, // A1.2
AOA_A1_SEL | AOA_Ax_ANT2, // A1.2
AOA_A1_SEL | AOA_Ax_ANT2, // A1.2
AOA_A1_SEL | AOA_Ax_ANT2, // A1.2
AOA_A1_SEL | AOA_Ax_ANT2, // A1.2
AOA_A1_SEL | AOA_Ax_ANT2, // A1.2
}
};
Task 5 – Antenna Switch Settling Time
Now that we are equipped with all the needed tools to manipulate I/Q data, we will try to identify when the antenna is toggling in order to help determine which I/Q samples can be used.
As mentioned in Calculate the phase difference among the antennas, I/Q samples can be presented with constellation diagram, each I/Q pair is a vector and its angle is within a range of +180 ~ -180. Therefore when we have an I/Q pair, to obtain the angle information, we can use arctan to get angle of a vector. Then based on the I and Q value, we can find out the corresponding angle.
| I > 0 | I < 0 | |
|---|---|---|
| Q >=0 | angle = arctan(Q/I) | angle = 180 + arctan(Q/I) |
| Q < 0 | angle = arctan(Q/I) | angle = -180 + arctan(Q/I) |
Luckily in python, the math.atan2 function takes care of the aforementioned logic.
Let's take a look at the Phase Information plot.

A perfect sine wave, assuming it starts at 0 degree, the phase will first go towards +180 and then, once it crosses +180, it will start from -180 and then go back to 0 degrees. From the picture provided below, you can see that in the first 8us(32 samples), there is no abrupt phase change.
When the rf switches and the angle of incident wave is not 0 degree, you will see abrupt phase change. As shown below after 2 periods, we started to switch antennas. Then the phase we obtained is no long linear.
Hence by looking at the phase information plot, you will know how many I/Q samples you can keep per period.

Well done!
You can now modify the AoA demo to improve it! You can develop your own algorithms and antennas to do cool stuff!
This work is licensed under a Creative Commons Attribution-NonCommercial-NoDerivatives 4.0 International License.