Terms and Definitions¶
Bluetooth Low Energy Terms and Acronyms¶
- BLE
- Bluetooth Low Energy
- BR
- Basic Rate
- BR/EDR
- Basic Rate/Enhanced Data Rate
- CCCD
- Client Characteristic Configuration Descriptor
- Device Address
- A 48-bit value used to identify a device. A device address can be public, random static, or random private.
- GAP
- Generic Access Protocol
- GFSK
- Gaussian Frequency-Shift Keying
- HCI
- Host Control Interface
- Identity Address
- IA
- A Resolvable Private Address that is resolveable with an Identity Resolving Key yields an Identity Address.
- Identity Resolving Key
- IRK
- A key exchanged during Phase 3 of the bonding process. A Resolving List contains a local and a peer Identity Resolving Key as well as an Identity Address.
- ISM
- Industrial, Scientific, and Medical
- L2CAP
- Link Logical Control and Adaption Protocol
- LE
- Low Energy
- Link Layer
- LL
- A Bluetooth low energy stack layer in on the controller side.
- LTK
- Long Term Key
- A term defined by the Bluetooth Core Specification Version 4.2 referring to the key used for encypted connections.
- PHY
- Physical Layer
- Resolving List
- RL
- A Link Layer maintained table of one or more entries of a local and peer Identity Resolving Key associated to an Identity Address.
- Resolvable Private Address
- RPA
- A resolvable address is one that can be resolved given that the device has an Identity Resolving Key. By resolving a Resolvable Private Address one can determine its Identity Address.
- White List
- WL
- A filter policy in the Controller’s Link Layer that can prevent unwanted link layer events from waking up the host.
- Long Term Key
- LTK
- A symmetric 128-bit key that is used to encrypt an encrypted BLE link.
General Terms and Acronyms¶
- BIM
- Boot Image Manager, the software bootloader
- .bss
- Block started by symbol. This memory section usually contains uninitialized variables including the task stacks.
- CCA
- CCFG
- Customer Configuration
- CCFG
- Customer Configuration Area, contains lock-bits on flash page 31 and the Customer Configuration Table (.ccfg)
- CCS
- Code Composer Studio
- An integrated development environment to develop applications for Texas Instruments embedded processors. Download: Code Composer Studio
- cJTAG
- Class 4 IEEE 1149.7: Standard for Reduced-pin and Enhanced-functionality Test Access Port and Boundary-scan Architecture. This is known by acronym cJTAG (compact JTAG).
- GCC
- GNU Compiler Collection
- A compiler system produced by the GNU Project, which support various programming languages such as C and C++.
- GPRAM
- General purpose RAM. This memory area is used for the cache per default, but can be configured to be used as RAM.
- HIB
- Halt In Boot. A mechanism in CC26xx and CC13xx devices to ensure that the external emulator can take control of the device before it executes any application code.
- IAR
- IAR Systems
- JTAG
- IEEE standard 1149.1: Standard Test Access Port and Boundary Scan Architecture Test Access Port (TAP). This standard is known by the acronym JTAG (Joint Test Action Group).
- MCU
- Micro-controller Unit
- OAD
- Over the Air Download
- RCFG
- TI-RTOS in ROM Configuration Table
- ROM
- Read-only Memory
- SNV
- Simple Non-Volatile storage
- SNP
- Simple Network Processor, a BLE network processor implementation that supports the peripheral and broadcaster GAP Roles.
- Network Processor
- NP
- A device that contains the wireless protocol stack as well as RF hardware. Stack functionality is exposed via a serial interface.
- Application Processor
- AP
- An processor that implements the customer application as well the serial command interface to communicate with a network processor.
- UNPI
- Unified Network Processor Interface, a standardized serial transport format that is implemented by TI for the purposes of interfacing to network processor devices like the SNP. UNPI also manages the handshaking required for the serial interface.
- RTSC
- Real Time Software Components
- A toolset for creating reusable code, used by TI-RTOS. See RTSC and RTSC-Pedia.
- TI-CGT
- TI Code Generation Tools
- Set of C/C++ Compilers and Assembly Language tools for many TI microcontrollers and processors. For more information, see TI Code Generation Tools.
- VIMS
- Versatile Instruction Memory System. A system control module that handles access to the device memory areas from the CPU and system bus. You can read more in the CC13x0 CC26x0 SimpleLink Wireless MCU Technical Reference Manual.
- cJTAG
- Class 4 IEEE 1149.7: Standard for Reduced-pin and Enhanced-functionality Test Access Port and Boundary-scan Architecture. This is known by acronym cJTAG (compact JTAG).
- JTAG
- IEEE standard 1149.1: Standard Test Access Port and Boundary Scan Architecture Test Access Port (TAP). This standard is known by the acronym JTAG (Joint Test Action Group).
TI-RTOS Terms and Acronyms¶
- HWI
- Hardware Interrupts
- A TI-RTOS hardware interrupt.
- Idle Task
- A TI-RTOS default task that is executes when no other higher priority thread needs to run.
- RCFG
- TI-RTOS in ROM configuration table.
- ROV
- Runtime Object View
- A TI-RTOS kernel plugin for CCS and IAR to view a target’s instrumentation data.
- RTC
- Real-Time Clock
- An accurate computer clock which keeps track of the current time.
- RTOS
- Real Time Operating System
- An operating system intended to serve applications with real-time requirements.
- SWI
- Software Interrupts
- A TI-RTOS software interrupt.
- TI-RTOS
- Texas Instruments Real Time Operating System
- An RTOS developed by TI for TI microcontrollers.
- Zero-Latency Interrupts
- An interrupt that will not be routed through the TI-RTOS kernel’s Hwi dispatcher. For more information, see the Hwi module documentation in the TI-RTOS Kernel API Reference .
Over-the-Air Download (OAD) Terms and Acronyms¶
- BIM
- Boot Image Manager
- A bootloader that runs after the device’s ROM startup code. The BIM is responsible for analyzing the image header of all images and determining the most suitable image to run. Once the BIM has found the proper image, it will jump to it’s program entry.
- CRC
- Cyclic Redundancy Check
- An error-detecting code used to check the integrity of blocks of data.
- ECDSA
- Elliptic Curve Digital Signature Algorithm
- A variant of the Digital Signature Algorithm (DSA) which uses elliptic curve cryptography.
- Factory Image
- The factory image is a “golden” image that resides in external flash as a fail-safe mechanism.
- HIB
- Halt In Boot
- A mechanism in CC26xx and CC13xx devices to ensure that the external emulator can take control of the device before it executes any application code.
- OAD
- Over-the-Air Download
- The process of performing a device firmware update over the air.
- OAD Target
- The device whose firmware is being upgraded over the air. This is assumed to be a CC26xx or CC13xx device running the TI protocol-specific transport for OAD.
- OAD Distributor
- The device responsible for accepting an OAD enabled image from the compiler and transferring it over the air to the OAD Target.
Secure Firmware (SFW) Terms and Acronyms¶
- Secure Firmware
- SFW
- The process of verifying an image before running for improved integrity and security
- Secure Firmware Bootloader
- SFB
- The bootloader that verifies the secure firmware image
- Secure Firmware Image
- SFI
- The application image that needs to be verified
- ECC
- Elliptic Curve Cryptography
- SHA
- Secure Hash Algorithm
- AES CBC MAC
- Advanced Encryption Standard Cipher Block Chaining Message Authentication Code
- TLV
- Type Length Value
Sensor Controller Terms and Acronyms¶
- SC
- Sensor Controller
- A dedicated 16-bit CPU core on CC13xx and CC26xx devices, located in the auxiliary (AUX) power/clock domain. It can perform simple background tasks autonomously and independently of the System CPU and the MCU domain power states.
- SCS
- Sensor Controller Studio
- A stand-alone IDE used to write, test and debug code for the Sensor Controller.
NPI Terms and Acronyms¶
- NPI
- Network Processor Interface
- Abstraction level above serial interface for sending / receiving data power management, and data parsing
- MRDY
- Master Ready
- GPIO pin that indicates the state of the master
- SRDY
- Slave Ready
- GPIO pin that indicates the state of the slave
- AIND
- Asynchronous Indication
- An asynchronously received NPI message sent from the network processor to the host / application processor.
- AREQ
- Asynchronous Request
- An asynchronously received NPI message sent from the host / application processor to the network processor.
- FCS
- Frame Check Sequence
- An error-detecting code added to a frame
- SOF
- Start of Frame
- A specific known byte specifying the beginning of a frame
- SREQ
- Synchronous Request
- A blocking NPI request that expects an ((SRESP))
- SRESP
- Synchronous Response
- A response to a ((SREQ))
- UNPI
- Unified ((NPI))
- NPI used except for with HostTest
- Network Processor
- NP
- A device that contains the wireless protocol stack as well as RF hardware. Stack functionality is exposed via a serial interface.
- Application Processor
- AP
- An processor that implements the customer application as well the serial command interface to communicate with a network processor.