module xdc.runtime.Gate

Critical section support

Gates are used by clients to protect concurrent access to critical data structures. Critical data structures are those that must be updated by at most one thread at a time. All code that needs access to a critical data structure "enters" a gate (that's associated with the data structure) prior to accessing the data, modifies the data structure, then "leaves" the gate. [ more ... ]
C synopsis target-domain sourced in xdc/runtime/Gate.xdc
#include <xdc/runtime/Gate.h>
Functions
macro Gate_Ref 
macro Bool 
macro Bool 
macro IArg 
macro IArg 
IArg 
macro Void 
macro Void 
macro Void 
Void 
Functions common to all target modules
Typedefs
typedef opaque
 
DETAILS
Gates are used by clients to protect concurrent access to critical data structures. Critical data structures are those that must be updated by at most one thread at a time. All code that needs access to a critical data structure "enters" a gate (that's associated with the data structure) prior to accessing the data, modifies the data structure, then "leaves" the gate.
A gate is responsible for ensuring that at most one thread at a time can enter and execute "inside" the gate. There are several implementations of gates, with different system executation times and latency tradoffs. In addition, some gates must not be entered by certain thread types; e.g., a gate that is implemented via a "blocking" semaphore must not be called by an interrupt service routine (ISR).
A module can be declared "gated" by adding the @Gated attribute to the module's XDC spec file. A "gated" module is assigned a module-level gate at the configuration time, and that gate is then used to protect critical sections in the module's target code. A module-level gate is an instance of a module implementing IGateProvider interface. However, gated modules do not access their module-level gates directly. They use this module to access transparently their module-level gate.
Application code that is not a part of any module also has a module-level gate, configured through the module Main.
Each gated module can optionally create gates on an adhoc basis at runtime using the same gate module that was used to create the module level gate.
Gates that work by disabling all preemption while inside a gate can be used to protect data structures accessed by ISRs and other threads. But, if the time required to update the data structure is not a small constant, this type of gate may violate a system's real-time requirements.
Gates have two orthogonal attributes: "blocking" and "preemptible". In general, gates that are "blocking" can not be use by code that is called by ISRs and gates that are not "preemptible" should only be used to to protect data manipulated by code that has small constant execution time.
 
typedef Gate_Ref

Opaque reference to an allocated gate instance

C synopsis target-domain
typedef opaque Gate_Ref;
 
 
Gate_allocInstance()  // module-wide

Allocate a gate instance from the current module's gate

C synopsis target-domain
macro Gate_Ref Gate_allocInstance(Error_Block *eb);
 
ARGUMENTS
eb — Error block pointer
If NULL, any error in creating the instance will terminate the application.
DETAILS
This method is used by modules to create gates at runtime using the same IGateProvider that was used to create the module level gate. The parameters passed to the IGateProvider are specified at configuration time via the Types.Common$.gateParams configuration parameter.
RETURNS
Non-NULL instance handle is returned if no error occurs; otherwise an error is raised in eb and NULL is returned.
SEE
 
Gate_canBePreempted()  // module-wide

Check if the module level gate allows thread preemption

C synopsis target-domain
macro Bool Gate_canBePreempted();
 
DETAILS
This type of gate should always be used by clients that protect a data structure whose updates require more than a small constant amount of time; e.g., update of a memory allocator's free list.
RETURNS
Returns TRUE if the underlying gate does not disable thread preemption.
 
Gate_canBlock()  // module-wide

Check if the module level gate can block threads

C synopsis target-domain
macro Bool Gate_canBlock();
 
DETAILS
This type of gate should never be called by clients that must never call a "blocking" RTOS operation; e.g., interrupt service routines
RETURNS
Returns TRUE if the underlying gatekeeper's gate can block
 
Gate_enterInstance()  // module-wide

Enter a critical section protected by this gate instance

C synopsis target-domain
macro IArg Gate_enterInstance(Gate_Ref gate);
 
ARGUMENTS
gate — non-NULL return value from a prior call to allocInstance.
RETURNS
Returns a "key" value that must be used to leave gate via leaveInstance().
 
Gate_enterModule()  // module-wide

Enter a critical section protected by the current module's gate

C synopsis target-domain
macro IArg Gate_enterModule();
 
RETURNS
Returns a "key" value that must be used to leave the current module gate via leaveModule().
SEE
 
Gate_enterSystem()  // module-wide

Enter a critical section protected by the global System gate

C synopsis target-domain
IArg Gate_enterSystem();
 
RETURNS
Returns a "key" value that must be used to leave the System gate via leaveSystem().
SEE
 
Gate_freeInstance()  // module-wide

Free a gate instance to the current module's gatekeeper

C synopsis target-domain
macro Void Gate_freeInstance(Gate_Ref gate);
 
ARGUMENTS
gate — non-NULL return value from a prior call to allocInstance.
SEE
 
Gate_leaveInstance()  // module-wide

Leave a critical section protected by a gate

C synopsis target-domain
macro Void Gate_leaveInstance(Gate_Ref gate, IArg key);
 
ARGUMENTS
gate — non-NULL return value from a prior call to allocInstance.
key — the return value of a prior call to enterInstance
SEE
 
Gate_leaveModule()  // module-wide

Leave a critical section protected by the current module's gate

C synopsis target-domain
macro Void Gate_leaveModule(IArg key);
 
ARGUMENTS
key — the return value of a prior call to enterModule
SEE
 
Gate_leaveSystem()  // module-wide

Leave a critical section protected by the global System gate

C synopsis target-domain
Void Gate_leaveSystem(IArg key);
 
ARGUMENTS
key — the return value of a prior call to enterSystem
SEE
Module-Wide Built-Ins

C synopsis target-domain
Types_ModuleId Gate_Module_id();
// Get this module's unique id
 
Bool Gate_Module_startupDone();
// Test if this module has completed startup
 
IHeap_Handle Gate_Module_heap();
// The heap from which this module allocates memory
 
Bool Gate_Module_hasMask();
// Test whether this module has a diagnostics mask
 
Bits16 Gate_Module_getMask();
// Returns the diagnostics mask for this module
 
Void Gate_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module
 
Configuration settings sourced in xdc/runtime/Gate.xdc
var Gate = xdc.useModule('xdc.runtime.Gate');
module-wide config parameters
module-wide functions
 
 
metaonly config Gate.common$  // module-wide

Common module configuration parameters

Configuration settings
Gate.common$ = Types.Common$ undefined;
 
DETAILS
All modules have this configuration parameter. Its name contains the '$' character to ensure it does not conflict with configuration parameters declared by the module. This allows new configuration parameters to be added in the future without any chance of breaking existing modules.
 
metaonly Gate.staticAlloc()  // module-wide

Assign a statically-allocated gate instance to a state-object field

Configuration settings
Gate.staticAlloc(Any stateObj, String fldName) returns Void
 
ARGUMENTS
stateObj — the state object for the instance being created
fldName — a name of a field within the state object
This parameter names a field that will point to the created gate instance to be created. It is a caller's responsibility to ensure that the type of fldName is a handle to an IGateProvider instance.
DETAILS
This method is used to create a gate for static instance objects that require a gate.
generated on Fri, 18 May 2018 20:56:12 GMT