TI BLE-Stack for Bluetooth 4.2 API Documentation  3.02.03.00
Modules | Files | Functions
Micro Gap Layer

Modules

 Micro GAP Broadcaster Callbacks
 
 Micro GAP Broadcaster Structures
 
 Micro GAP Constants
 
 Micro GAP Monitor Callbacks
 
 Micro GAP Monitor Structures
 

Files

file  ugap.h
 Micro BLE GAP API.
 

Functions

bStatus_t ugap_bcastInit (ugapBcastCBs_t *pCBs)
 Initialize Micro Broadcaster. More...
 
bStatus_t ugap_bcastSetDuty (uint16 dutyOnTime, uint16 dutyOffTime)
 Set Broadcaster Duty On/Off time. More...
 
bStatus_t ugap_bcastStart (uint16 numAdvEvent)
 Start Broadcaster. Proceed the state from either Initialized or IDLE to Advertising. More...
 
bStatus_t ugap_bcastStop (void)
 Stop Broadcaster. Proceed the state from either Advertising or Waiting to IDLE. More...
 
bStatus_t ugap_monitorInit (ugapMonitorCBs_t *pCBs)
 Initialize Micro Monitor. More...
 
bStatus_t ugap_monitorRequest (uint8_t channel, uint32_t accessAddr, uint32_t startTime, uint16_t duration, uint32_t crcInit)
 uGAP monitor request More...
 
bStatus_t ugap_monitorStart (void)
 Start Monitor scanning. Proceed the state from either Initialized or Idle to Monitoring. More...
 
bStatus_t ugap_monitorStop (void)
 Stop Monitor scanning. Proceed the state from Monitoring to Idle. More...
 

Detailed Description

Function Documentation

§ ugap_bcastInit()

bStatus_t ugap_bcastInit ( ugapBcastCBs_t pCBs)

Initialize Micro Broadcaster.

Parameters
pCBs- a set of application callbacks for Broadcaster
Returns
SUCCESS
INVALIDPARAMETER
FAILURE

§ ugap_bcastSetDuty()

bStatus_t ugap_bcastSetDuty ( uint16  dutyOnTime,
uint16  dutyOffTime 
)

Set Broadcaster Duty On/Off time.

Parameters
dutyOnTime- Time period during which the Broadcaster is in Advertising state. 100 ms unit. This cannot be 0 unless dutyOffTime is also 0.
dutyOffTime- Time period during which the Broadcaster is in Waiting state. 100 ms unit. If this is 0, Duty Control is disabled regardless of dutyOnTime.
Returns
SUCCESS
INVALIDPARAMETER

§ ugap_bcastStart()

bStatus_t ugap_bcastStart ( uint16  numAdvEvent)

Start Broadcaster. Proceed the state from either Initialized or IDLE to Advertising.

Parameters
numAdvEvent- # of Advertising events to be performed before the Broadcaster state goes to IDLE. If this is 0, the Broadcaster will keep staying in Advertising or Advertising and Waiting alternately unless an error happens or the application requests to stop.
Returns
SUCCESS
FAILURE
INVALIDPARAMETER

§ ugap_bcastStop()

bStatus_t ugap_bcastStop ( void  )

Stop Broadcaster. Proceed the state from either Advertising or Waiting to IDLE.

Returns
SUCCESS
INVALIDPARAMETER
FAILURE

§ ugap_monitorInit()

bStatus_t ugap_monitorInit ( ugapMonitorCBs_t pCBs)

Initialize Micro Monitor.

Parameters
pCBs- a set of application callbacks for Monitor
Returns
SUCCESS
FAILURE
INVALIDPARAMETER

§ ugap_monitorRequest()

bStatus_t ugap_monitorRequest ( uint8_t  channel,
uint32_t  accessAddr,
uint32_t  startTime,
uint16_t  duration,
uint32_t  crcInit 
)

uGAP monitor request

Parameters
channel- Channels to monitor.
accessAddr- Access address. 0xFFFFFFFF is used as a wildcard access address. An error status will be returned if the channel is one of 37, 38, or 39 but the accessAddr is not 0x8E89BED6.
startTime- Absolute start time in RAT ticks.
duration- Scan window per scanChanIndexchanIndex. A monitor complete time-out statuscallback will be sent to the application. A zero indicates a continuous scan. Unit in 0.625 ms; range from 2.5 ms to 40.959375 s.
crcInit- crcInit value for this connection
Returns
SUCCESS
INVALIDPARAMETER

§ ugap_monitorStart()

bStatus_t ugap_monitorStart ( void  )

Start Monitor scanning. Proceed the state from either Initialized or Idle to Monitoring.

Returns
SUCCESS
FAILURE

§ ugap_monitorStop()

bStatus_t ugap_monitorStop ( void  )

Stop Monitor scanning. Proceed the state from Monitoring to Idle.

Returns
SUCCESS
FAILURE
© Copyright 1995-2019, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale