TI BLE-Stack for Bluetooth 4.2 API Documentation  3.02.03.00
Data Fields
linkDBInfo_t Struct Reference

linkDB info More...

Data Fields

uint8 addr [B_ADDR_LEN]
 Other Device's address.
 
uint8 addrPriv [B_ADDR_LEN]
 Other Device's Private address.
 
uint8 addrType
 Address type of connected device.
 
uint16 connInterval
 The connection's interval (n * 1.23 ms)
 
uint8 connRole
 Connection formed as Master or Slave.
 
uint16 MTU
 The connection's MTU size.
 
uint8 stateFlags
 LINK_CONNECTED, LINK_AUTHENTICATED...
 

Detailed Description

linkDB info


The documentation for this struct was generated from the following file:
© Copyright 1995-2019, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale