TI BLE-Stack for Bluetooth 4.2 API Documentation  3.02.03.00
Data Fields
snpGetStatusCmdRsp_t Struct Reference

Parameter Structure for the response to SNP_getStatus This is a packed structure. see Dealing with Parameters and Packed Structures for more information. More...

Data Fields

uint8_t advStatus
 1 Byte Current state of advertising : More...
 
uint8_t ATTmethod
 1 Byte Current GATT operation in progress if snpGetStatusCmdRsp_t::ATTstatus is set to TRUE
 
uint8_t ATTstatus
 1 Byte Current state of the GATT server More...
 
uint8_t gapRoleStatus
 1 Byte Current state of the GAP Role ( gaprole_States_t) More...
 

Detailed Description

Parameter Structure for the response to SNP_getStatus This is a packed structure. see Dealing with Parameters and Packed Structures for more information.


The documentation for this struct was generated from the following file:
© Copyright 1995-2019, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale