TI BLE-Stack for Bluetooth 4.2 API Documentation  3.02.03.00
Data Fields

Parameter Structure for SNP_HCI_CMD_RSP. More...

Data Fields

uint16_t opcode
 2 Byte HCI opcode that was executed in the request, list of all HCI commands allowed by the SNP.
 
uint8_t * pData
 
uint8_t status
 1 Byte status of the request (SUCCESS or Error, list of status generated by the SNP.)
 

Detailed Description

Parameter Structure for SNP_HCI_CMD_RSP.

This is a packed structure. see Dealing with Parameters and Packed Structures for more information.


The documentation for this struct was generated from the following file:
© Copyright 1995-2019, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale