TI BLE-Stack for Bluetooth 4.2 API Documentation  3.02.03.00
Data Fields
snpNotifIndReq_t Struct Reference

Parameter Structure for the Characteristic Notification and Indication Request data This is a packed structure. see Dealing with Parameters and Packed Structures for more information. More...

Data Fields

uint16_t attrHandle
 2 Byte Handle of the characteristic value attribute to notify/indicate
 
uint8_t authenticate
 1 Byte Reserved for future use
 
uint16_t connHandle
 2 Byte Handle of the connection
 
uint8_t * pData
 Pointer to.
 
uint8_t type
 1 Byte Type of the request, see SNP indication type
 

Detailed Description

Parameter Structure for the Characteristic Notification and Indication Request data This is a packed structure. see Dealing with Parameters and Packed Structures for more information.


The documentation for this struct was generated from the following file:
© Copyright 1995-2019, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale