TI BLE-Stack for Bluetooth 4.2 API Documentation  3.02.03.00
Data Fields
snpUpdateConnParamEvt_t Struct Reference

Parameter Structure for the Update Connection Parameter Event. More...

Data Fields

uint16_t connHandle
 2 Byte Handle of the connection
 
uint16_t connInterval
 2 Byte More...
 
uint16_t slaveLatency
 2 Byte More...
 
uint16_t supervisionTimeout
 2 Byte More...
 

Detailed Description

Parameter Structure for the Update Connection Parameter Event.

See SNP Event Indication for more information.

This is a packed structure. see Dealing with Parameters and Packed Structures for more information.


The documentation for this struct was generated from the following file:
© Copyright 1995-2019, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale