GAP Callback function pointer type for Connection Event notifications.
When registered via GAP_RegisterConnEventCb, this callback will return a pointer to a Gap_ConnEventRpt_t from the controller after each connection event
- Warning
- The application owns the memory pointed to by pReport. That is, it is responsible for freeing this memory.
-
This is called from the stack task context. Therefore, processing in this callback should be minimized. Any excessive processing should be done by posting an event to the application task context.