Functions
cpu.h File Reference
#include <stdint.h>

Go to the source code of this file.

Functions

uint32_t CPU_cpsid (void)
 
uint32_t CPU_cpsie (void)
 
uint32_t CPU_primask (void)
 
void CPU_wfi (void)
 
uint32_t CPU_basepriGet (void)
 
void CPU_basepriSet (uint32_t newBasepri)
 

Function Documentation

uint32_t CPU_cpsid ( void  )

Referenced by Interrupt_disableMaster().

uint32_t CPU_cpsie ( void  )
uint32_t CPU_primask ( void  )
void CPU_wfi ( void  )
uint32_t CPU_basepriGet ( void  )
void CPU_basepriSet ( uint32_t  newBasepri)

Copyright 2018, Texas Instruments Incorporated