Data Structures | Macros | Typedefs | Functions
LCD_F

Segment LCD module used to control/manipulate attached LCD display. More...

Data Structures

struct  LCD_F_initParam
 

Macros

#define LCD_F_CLOCKSOURCE_ACLK   (LCD_F_CTL_SSEL_0)
 
#define LCD_F_CLOCKSOURCE_VLOCLK   (LCD_F_CTL_SSEL_1)
 
#define LCD_F_CLOCKSOURCE_REFOCLK   (LCD_F_CTL_SSEL_2)
 
#define LCD_F_CLOCKSOURCE_LFXT   (LCD_F_CTL_SSEL_3)
 
#define LCD_F_CLOCKDIVIDER_1   0x0
 
#define LCD_F_CLOCKDIVIDER_2   0x800
 
#define LCD_F_CLOCKDIVIDER_3   0x1000
 
#define LCD_F_CLOCKDIVIDER_4   0x1800
 
#define LCD_F_CLOCKDIVIDER_5   0x2000
 
#define LCD_F_CLOCKDIVIDER_6   0x2800
 
#define LCD_F_CLOCKDIVIDER_7   0x3000
 
#define LCD_F_CLOCKDIVIDER_8   0x3800
 
#define LCD_F_CLOCKDIVIDER_9   0x4000
 
#define LCD_F_CLOCKDIVIDER_10   0x4800
 
#define LCD_F_CLOCKDIVIDER_11   0x5000
 
#define LCD_F_CLOCKDIVIDER_12   0x5800
 
#define LCD_F_CLOCKDIVIDER_13   0x6000
 
#define LCD_F_CLOCKDIVIDER_14   0x6800
 
#define LCD_F_CLOCKDIVIDER_15   0x7000
 
#define LCD_F_CLOCKDIVIDER_16   0x7800
 
#define LCD_F_CLOCKDIVIDER_17   0x8000
 
#define LCD_F_CLOCKDIVIDER_18   0x8800
 
#define LCD_F_CLOCKDIVIDER_19   0x9000
 
#define LCD_F_CLOCKDIVIDER_20   0x9800
 
#define LCD_F_CLOCKDIVIDER_21   0xa000
 
#define LCD_F_CLOCKDIVIDER_22   0xa800
 
#define LCD_F_CLOCKDIVIDER_23   0xb000
 
#define LCD_F_CLOCKDIVIDER_24   0xb800
 
#define LCD_F_CLOCKDIVIDER_25   0xc000
 
#define LCD_F_CLOCKDIVIDER_26   0xc800
 
#define LCD_F_CLOCKDIVIDER_27   0xd000
 
#define LCD_F_CLOCKDIVIDER_28   0xd800
 
#define LCD_F_CLOCKDIVIDER_29   0xe000
 
#define LCD_F_CLOCKDIVIDER_30   0xe800
 
#define LCD_F_CLOCKDIVIDER_31   0xf000
 
#define LCD_F_CLOCKDIVIDER_32   0xf800
 
#define LCD_F_CLOCKPRESCALER_1   (LCD_F_CTL_PRE_0)
 
#define LCD_F_CLOCKPRESCALER_2   (LCD_F_CTL_PRE_1)
 
#define LCD_F_CLOCKPRESCALER_4   (LCD_F_CTL_PRE_2)
 
#define LCD_F_CLOCKPRESCALER_8   (LCD_F_CTL_PRE_3)
 
#define LCD_F_CLOCKPRESCALER_16   (LCD_F_CTL_PRE_4)
 
#define LCD_F_CLOCKPRESCALER_32   (LCD_F_CTL_PRE_5)
 
#define LCD_F_STATIC   (LCD_F_CTL_MX_0)
 
#define LCD_F_2_MUX   (LCD_F_CTL_MX_1)
 
#define LCD_F_3_MUX   (LCD_F_CTL_MX_2)
 
#define LCD_F_4_MUX   (LCD_F_CTL_MX_3)
 
#define LCD_F_5_MUX   (LCD_F_CTL_MX_4)
 
#define LCD_F_6_MUX   (LCD_F_CTL_MX_5)
 
#define LCD_F_7_MUX   (LCD_F_CTL_MX_6)
 
#define LCD_F_8_MUX   (LCD_F_CTL_MX_7)
 
#define LCD_F_V2V3V4_GENERATED_INTERNALLY_NOT_SWITCHED_TO_PINS   (0x0)
 
#define LCD_F_V2V3V4_GENERATED_INTERNALLY_SWITCHED_TO_PINS   (LCD_F_VCTL_REXT)
 
#define LCD_F_V2V3V4_SOURCED_EXTERNALLY   (LCD_F_VCTL_EXTBIAS)
 
#define LCD_F_V5_VSS   (0x0)
 
#define LCD_F_V5_SOURCED_FROM_R03   (LCD_F_VCTL_R03EXT)
 
#define LCD_F_STANDARD_WAVEFORMS   (0x0)
 
#define LCD_F_LOW_POWER_WAVEFORMS   (LCD_F_CTL_LP)
 
#define LCD_F_SEGMENTS_DISABLED   (0x0)
 
#define LCD_F_SEGMENTS_ENABLED   (LCD_F_CTL_SON)
 
#define LCD_F_BLINKING_SEGMENTS_ON_INTERRUPT   (LCD_F_IE_BLKONIE)
 
#define LCD_F_BLINKING_SEGMENTS_OFF_INTERRUPT   (LCD_F_IE_BLKOFFIE)
 
#define LCD_F_FRAME_INTERRUPT   (LCD_F_IE_FRMIE)
 
#define LCD_F_ANIMATION_LOOP_INTERRUPT   (LCD_F_IE_ANMLOOPIE)
 
#define LCD_F_ANIMATION_STEP_INTERRUPT   (LCD_F_IE_ANMSTPIE)
 
#define LCD_F_DISPLAYSOURCE_MEMORY   (0x0)
 
#define LCD_F_DISPLAYSOURCE_BLINKINGMEMORY   (0x1)
 
#define LCD_F_BLINK_FREQ_CLOCK_PRESCALAR_512   LCD_F_BMCTL_BLKPRE_0
 
#define LCD_F_BLINK_FREQ_CLOCK_PRESCALAR_1024   LCD_F_BMCTL_BLKPRE_1
 
#define LCD_F_BLINK_FREQ_CLOCK_PRESCALAR_2048   LCD_F_BMCTL_BLKPRE_2
 
#define LCD_F_BLINK_FREQ_CLOCK_PRESCALAR_4096   LCD_F_BMCTL_BLKPRE_3
 
#define LCD_F_BLINK_FREQ_CLOCK_PRESCALAR_8162   LCD_F_BMCTL_BLKPRE_4
 
#define LCD_F_BLINK_FREQ_CLOCK_PRESCALAR_16384   LCD_F_BMCTL_BLKPRE_5
 
#define LCD_F_BLINK_FREQ_CLOCK_PRESCALAR_32768   LCD_F_BMCTL_BLKPRE_6
 
#define LCD_F_BLINK_FREQ_CLOCK_PRESCALAR_65536   LCD_F_BMCTL_BLKPRE_7
 
#define LCD_F_BLINK_FREQ_CLOCK_DIVIDER_1   LCD_F_BMCTL_BLKDIV_0
 
#define LCD_F_BLINK_FREQ_CLOCK_DIVIDER_2   LCD_F_BMCTL_BLKDIV_1
 
#define LCD_F_BLINK_FREQ_CLOCK_DIVIDER_3   LCD_F_BMCTL_BLKDIV_2
 
#define LCD_F_BLINK_FREQ_CLOCK_DIVIDER_4   LCD_F_BMCTL_BLKDIV_3
 
#define LCD_F_BLINK_FREQ_CLOCK_DIVIDER_5   LCD_F_BMCTL_BLKDIV_4
 
#define LCD_F_BLINK_FREQ_CLOCK_DIVIDER_6   LCD_F_BMCTL_BLKDIV_5
 
#define LCD_F_BLINK_FREQ_CLOCK_DIVIDER_7   LCD_F_BMCTL_BLKDIV_6
 
#define LCD_F_BLINK_FREQ_CLOCK_DIVIDER_8   LCD_F_BMCTL_BLKDIV_7
 
#define LCD_F_BLINK_MODE_DISABLED   (LCD_F_BMCTL_BLKMOD_0)
 
#define LCD_F_BLINK_MODE_INDIVIDUAL_SEGMENTS   (LCD_F_BMCTL_BLKMOD_1)
 
#define LCD_F_BLINK_MODE_ALL_SEGMENTS   (LCD_F_BMCTL_BLKMOD_2)
 
#define LCD_F_BLINK_MODE_SWITCHING_BETWEEN_DISPLAY_CONTENTS   (LCD_F_BMCTL_BLKMOD_3)
 
#define LCD_F_ANIMATION_FREQ_CLOCK_PRESCALAR_512   LCD_F_ANMCTL_ANMPRE_0
 
#define LCD_F_ANIMATION_FREQ_CLOCK_PRESCALAR_1024   LCD_F_ANMCTL_ANMPRE_1
 
#define LCD_F_ANIMATION_FREQ_CLOCK_PRESCALAR_2048   LCD_F_ANMCTL_ANMPRE_2
 
#define LCD_F_ANIMATION_FREQ_CLOCK_PRESCALAR_4096   LCD_F_ANMCTL_ANMPRE_3
 
#define LCD_F_ANIMATION_FREQ_CLOCK_PRESCALAR_8162   LCD_F_ANMCTL_ANMPRE_4
 
#define LCD_F_ANIMATION_FREQ_CLOCK_PRESCALAR_16384   LCD_F_ANMCTL_ANMPRE_5
 
#define LCD_F_ANIMATION_FREQ_CLOCK_PRESCALAR_32768   LCD_F_ANMCTL_ANMPRE_6
 
#define LCD_F_ANIMATION_FREQ_CLOCK_PRESCALAR_65536   LCD_F_ANMCTL_ANMPRE_7
 
#define LCD_F_ANIMATION_FREQ_CLOCK_DIVIDER_1   LCD_F_ANMCTL_ANMDIV_0
 
#define LCD_F_ANIMATION_FREQ_CLOCK_DIVIDER_2   LCD_F_ANMCTL_ANMDIV_1
 
#define LCD_F_ANIMATION_FREQ_CLOCK_DIVIDER_3   LCD_F_ANMCTL_ANMDIV_2
 
#define LCD_F_ANIMATION_FREQ_CLOCK_DIVIDER_4   LCD_F_ANMCTL_ANMDIV_3
 
#define LCD_F_ANIMATION_FREQ_CLOCK_DIVIDER_5   LCD_F_ANMCTL_ANMDIV_4
 
#define LCD_F_ANIMATION_FREQ_CLOCK_DIVIDER_6   LCD_F_ANMCTL_ANMDIV_5
 
#define LCD_F_ANIMATION_FREQ_CLOCK_DIVIDER_7   LCD_F_ANMCTL_ANMDIV_6
 
#define LCD_F_ANIMATION_FREQ_CLOCK_DIVIDER_8   LCD_F_ANMCTL_ANMDIV_7
 
#define LCD_F_ANIMATION_FRAMES_T0_TO_T7   LCD_F_ANMCTL_ANMSTP_7
 
#define LCD_F_ANIMATION_FRAMES_T0_TO_T6   LCD_F_ANMCTL_ANMSTP_6
 
#define LCD_F_ANIMATION_FRAMES_T0_TO_T5   LCD_F_ANMCTL_ANMSTP_5
 
#define LCD_F_ANIMATION_FRAMES_T0_TO_T4   LCD_F_ANMCTL_ANMSTP_4
 
#define LCD_F_ANIMATION_FRAMES_T0_TO_T3   LCD_F_ANMCTL_ANMSTP_3
 
#define LCD_F_ANIMATION_FRAMES_T0_TO_T2   LCD_F_ANMCTL_ANMSTP_2
 
#define LCD_F_ANIMATION_FRAMES_T0_TO_T1   LCD_F_ANMCTL_ANMSTP_1
 
#define LCD_F_ANIMATION_FRAMES_T0   LCD_F_ANMCTL_ANMSTP_0
 
#define LCD_F_SEGMENT_LINE_0   (0)
 
#define LCD_F_SEGMENT_LINE_1   (1)
 
#define LCD_F_SEGMENT_LINE_2   (2)
 
#define LCD_F_SEGMENT_LINE_3   (3)
 
#define LCD_F_SEGMENT_LINE_4   (4)
 
#define LCD_F_SEGMENT_LINE_5   (5)
 
#define LCD_F_SEGMENT_LINE_6   (6)
 
#define LCD_F_SEGMENT_LINE_7   (7)
 
#define LCD_F_SEGMENT_LINE_8   (8)
 
#define LCD_F_SEGMENT_LINE_9   (9)
 
#define LCD_F_SEGMENT_LINE_10   (10)
 
#define LCD_F_SEGMENT_LINE_11   (11)
 
#define LCD_F_SEGMENT_LINE_12   (12)
 
#define LCD_F_SEGMENT_LINE_13   (13)
 
#define LCD_F_SEGMENT_LINE_14   (14)
 
#define LCD_F_SEGMENT_LINE_15   (15)
 
#define LCD_F_SEGMENT_LINE_16   (16)
 
#define LCD_F_SEGMENT_LINE_17   (17)
 
#define LCD_F_SEGMENT_LINE_18   (18)
 
#define LCD_F_SEGMENT_LINE_19   (19)
 
#define LCD_F_SEGMENT_LINE_20   (20)
 
#define LCD_F_SEGMENT_LINE_21   (21)
 
#define LCD_F_SEGMENT_LINE_22   (22)
 
#define LCD_F_SEGMENT_LINE_23   (23)
 
#define LCD_F_SEGMENT_LINE_24   (24)
 
#define LCD_F_SEGMENT_LINE_25   (25)
 
#define LCD_F_SEGMENT_LINE_26   (26)
 
#define LCD_F_SEGMENT_LINE_27   (27)
 
#define LCD_F_SEGMENT_LINE_28   (28)
 
#define LCD_F_SEGMENT_LINE_29   (29)
 
#define LCD_F_SEGMENT_LINE_30   (30)
 
#define LCD_F_SEGMENT_LINE_31   (31)
 
#define LCD_F_SEGMENT_LINE_32   (32)
 
#define LCD_F_SEGMENT_LINE_33   (33)
 
#define LCD_F_SEGMENT_LINE_34   (34)
 
#define LCD_F_SEGMENT_LINE_35   (35)
 
#define LCD_F_SEGMENT_LINE_36   (36)
 
#define LCD_F_SEGMENT_LINE_37   (37)
 
#define LCD_F_SEGMENT_LINE_38   (38)
 
#define LCD_F_SEGMENT_LINE_39   (39)
 
#define LCD_F_SEGMENT_LINE_40   (40)
 
#define LCD_F_SEGMENT_LINE_41   (41)
 
#define LCD_F_SEGMENT_LINE_42   (42)
 
#define LCD_F_SEGMENT_LINE_43   (43)
 
#define LCD_F_SEGMENT_LINE_44   (44)
 
#define LCD_F_SEGMENT_LINE_45   (45)
 
#define LCD_F_SEGMENT_LINE_46   (46)
 
#define LCD_F_SEGMENT_LINE_47   (47)
 
#define LCD_F_MEMORY_COM0   (0x01)
 
#define LCD_F_MEMORY_COM1   (0x02)
 
#define LCD_F_MEMORY_COM2   (0x04)
 
#define LCD_F_MEMORY_COM3   (0x08)
 
#define LCD_F_MEMORY_COM4   (0x10)
 
#define LCD_F_MEMORY_COM5   (0x20)
 
#define LCD_F_MEMORY_COM6   (0x40)
 
#define LCD_F_MEMORY_COM7   (0x80)
 
#define LCD_F_BIAS_1_3   (0x0)
 
#define LCD_F_BIAS_1_2   (LCD_F_VCTL_LCD2B)
 
#define LCD_F_BIAS_1_4   (LCD_F_VCTL_LCD2B)
 
#define OFS_LCDM0W   0x120
 
#define OFS_LCDBM0W   0x160
 

Typedefs

typedef struct LCD_F_initParam LCD_F_Config
 

Functions

void LCD_F_initModule (LCD_F_Config *initParams)
 Initializes the LCD_F Module. More...
 
void LCD_F_turnOn (void)
 Turns on the LCD_F module. More...
 
void LCD_F_turnOff (void)
 Turns the LCD_F off. More...
 
void LCD_F_clearAllMemory (void)
 Clears all LCD_F memory registers. More...
 
void LCD_F_clearAllBlinkingMemory (void)
 Clears all LCD_F blinking memory registers. More...
 
void LCD_F_selectDisplayMemory (uint_fast16_t displayMemory)
 Selects display memory. More...
 
void LCD_F_setBlinkingControl (uint_fast16_t clockPrescalar, uint_fast16_t divider, uint_fast16_t mode)
 Sets the blinking control register. More...
 
void LCD_F_setAnimationControl (uint_fast16_t clockPrescalar, uint_fast16_t divider, uint_fast16_t frames)
 Sets the animation control register. More...
 
void LCD_F_enableAnimation (void)
 Enables animation on the LCD_F controller. More...
 
void LCD_F_disableAnimation (void)
 Enables animation on the LCD_F controller. More...
 
void LCD_F_clearAllAnimationMemory (void)
 Clears all LCD_F animation memory registers. More...
 
void LCD_F_setPinAsLCDFunction (uint_fast8_t pin)
 Sets the LCD_F pins as LCD function pin. More...
 
void LCD_F_setPinAsPortFunction (uint_fast8_t pin)
 Sets the LCD_F pins as port function pin. More...
 
void LCD_F_setPinsAsLCDFunction (uint_fast8_t startPin, uint8_t endPin)
 Sets the LCD_F pins as LCD function pin. More...
 
void LCD_F_setPinAsCOM (uint8_t pin, uint_fast8_t com)
 Sets the LCD_F pin as a common line. More...
 
void LCD_F_setPinAsSEG (uint_fast8_t pin)
 Sets the LCD_F pin as a segment line. More...
 
void LCD_F_selectBias (uint_fast16_t bias)
 Selects the bias level. More...
 
void LCD_F_setVLCDSource (uint_fast16_t v2v3v4Source, uint_fast16_t v5Source)
 Sets the voltage source for V2/V3/V4 and V5. More...
 
void LCD_F_clearInterrupt (uint32_t mask)
 Clears the LCD_F selected interrupt flags. More...
 
uint32_t LCD_F_getInterruptStatus (void)
 Returns the status of the selected interrupt flags. More...
 
uint32_t LCD_F_getEnabledInterruptStatus (void)
 Returns the status of the selected interrupt flags masked with the currently enabled interrupts. More...
 
void LCD_F_enableInterrupt (uint32_t mask)
 Enables the LCD_F selected interrupts. More...
 
void LCD_F_disableInterrupt (uint32_t mask)
 Disables the LCD_F selected interrupts. More...
 
void LCD_F_registerInterrupt (void(*intHandler)(void))
 
void LCD_F_unregisterInterrupt (void)
 

Detailed Description

Segment LCD module used to control/manipulate attached LCD display.


DriverLib LCD_F Module Operation


Macro Definition Documentation

#define LCD_F_CLOCKSOURCE_ACLK   (LCD_F_CTL_SSEL_0)
#define LCD_F_CLOCKSOURCE_VLOCLK   (LCD_F_CTL_SSEL_1)
#define LCD_F_CLOCKSOURCE_REFOCLK   (LCD_F_CTL_SSEL_2)
#define LCD_F_CLOCKSOURCE_LFXT   (LCD_F_CTL_SSEL_3)
#define LCD_F_CLOCKDIVIDER_1   0x0
#define LCD_F_CLOCKDIVIDER_2   0x800
#define LCD_F_CLOCKDIVIDER_3   0x1000
#define LCD_F_CLOCKDIVIDER_4   0x1800
#define LCD_F_CLOCKDIVIDER_5   0x2000
#define LCD_F_CLOCKDIVIDER_6   0x2800
#define LCD_F_CLOCKDIVIDER_7   0x3000
#define LCD_F_CLOCKDIVIDER_8   0x3800
#define LCD_F_CLOCKDIVIDER_9   0x4000
#define LCD_F_CLOCKDIVIDER_10   0x4800
#define LCD_F_CLOCKDIVIDER_11   0x5000
#define LCD_F_CLOCKDIVIDER_12   0x5800
#define LCD_F_CLOCKDIVIDER_13   0x6000
#define LCD_F_CLOCKDIVIDER_14   0x6800
#define LCD_F_CLOCKDIVIDER_15   0x7000
#define LCD_F_CLOCKDIVIDER_16   0x7800
#define LCD_F_CLOCKDIVIDER_17   0x8000
#define LCD_F_CLOCKDIVIDER_18   0x8800
#define LCD_F_CLOCKDIVIDER_19   0x9000
#define LCD_F_CLOCKDIVIDER_20   0x9800
#define LCD_F_CLOCKDIVIDER_21   0xa000
#define LCD_F_CLOCKDIVIDER_22   0xa800
#define LCD_F_CLOCKDIVIDER_23   0xb000
#define LCD_F_CLOCKDIVIDER_24   0xb800
#define LCD_F_CLOCKDIVIDER_25   0xc000
#define LCD_F_CLOCKDIVIDER_26   0xc800
#define LCD_F_CLOCKDIVIDER_27   0xd000
#define LCD_F_CLOCKDIVIDER_28   0xd800
#define LCD_F_CLOCKDIVIDER_29   0xe000
#define LCD_F_CLOCKDIVIDER_30   0xe800
#define LCD_F_CLOCKDIVIDER_31   0xf000
#define LCD_F_CLOCKDIVIDER_32   0xf800
#define LCD_F_CLOCKPRESCALER_1   (LCD_F_CTL_PRE_0)
#define LCD_F_CLOCKPRESCALER_2   (LCD_F_CTL_PRE_1)
#define LCD_F_CLOCKPRESCALER_4   (LCD_F_CTL_PRE_2)
#define LCD_F_CLOCKPRESCALER_8   (LCD_F_CTL_PRE_3)
#define LCD_F_CLOCKPRESCALER_16   (LCD_F_CTL_PRE_4)
#define LCD_F_CLOCKPRESCALER_32   (LCD_F_CTL_PRE_5)
#define LCD_F_STATIC   (LCD_F_CTL_MX_0)
#define LCD_F_2_MUX   (LCD_F_CTL_MX_1)
#define LCD_F_3_MUX   (LCD_F_CTL_MX_2)
#define LCD_F_4_MUX   (LCD_F_CTL_MX_3)
#define LCD_F_5_MUX   (LCD_F_CTL_MX_4)
#define LCD_F_6_MUX   (LCD_F_CTL_MX_5)
#define LCD_F_7_MUX   (LCD_F_CTL_MX_6)
#define LCD_F_8_MUX   (LCD_F_CTL_MX_7)
#define LCD_F_V2V3V4_GENERATED_INTERNALLY_NOT_SWITCHED_TO_PINS   (0x0)
#define LCD_F_V2V3V4_GENERATED_INTERNALLY_SWITCHED_TO_PINS   (LCD_F_VCTL_REXT)
#define LCD_F_V2V3V4_SOURCED_EXTERNALLY   (LCD_F_VCTL_EXTBIAS)
#define LCD_F_V5_VSS   (0x0)
#define LCD_F_V5_SOURCED_FROM_R03   (LCD_F_VCTL_R03EXT)
#define LCD_F_STANDARD_WAVEFORMS   (0x0)
#define LCD_F_LOW_POWER_WAVEFORMS   (LCD_F_CTL_LP)
#define LCD_F_SEGMENTS_DISABLED   (0x0)
#define LCD_F_SEGMENTS_ENABLED   (LCD_F_CTL_SON)
#define LCD_F_BLINKING_SEGMENTS_ON_INTERRUPT   (LCD_F_IE_BLKONIE)
#define LCD_F_BLINKING_SEGMENTS_OFF_INTERRUPT   (LCD_F_IE_BLKOFFIE)
#define LCD_F_FRAME_INTERRUPT   (LCD_F_IE_FRMIE)
#define LCD_F_ANIMATION_LOOP_INTERRUPT   (LCD_F_IE_ANMLOOPIE)
#define LCD_F_ANIMATION_STEP_INTERRUPT   (LCD_F_IE_ANMSTPIE)
#define LCD_F_DISPLAYSOURCE_MEMORY   (0x0)
#define LCD_F_DISPLAYSOURCE_BLINKINGMEMORY   (0x1)
#define LCD_F_BLINK_FREQ_CLOCK_PRESCALAR_512   LCD_F_BMCTL_BLKPRE_0
#define LCD_F_BLINK_FREQ_CLOCK_PRESCALAR_1024   LCD_F_BMCTL_BLKPRE_1
#define LCD_F_BLINK_FREQ_CLOCK_PRESCALAR_2048   LCD_F_BMCTL_BLKPRE_2
#define LCD_F_BLINK_FREQ_CLOCK_PRESCALAR_4096   LCD_F_BMCTL_BLKPRE_3
#define LCD_F_BLINK_FREQ_CLOCK_PRESCALAR_8162   LCD_F_BMCTL_BLKPRE_4
#define LCD_F_BLINK_FREQ_CLOCK_PRESCALAR_16384   LCD_F_BMCTL_BLKPRE_5
#define LCD_F_BLINK_FREQ_CLOCK_PRESCALAR_32768   LCD_F_BMCTL_BLKPRE_6
#define LCD_F_BLINK_FREQ_CLOCK_PRESCALAR_65536   LCD_F_BMCTL_BLKPRE_7
#define LCD_F_BLINK_FREQ_CLOCK_DIVIDER_1   LCD_F_BMCTL_BLKDIV_0
#define LCD_F_BLINK_FREQ_CLOCK_DIVIDER_2   LCD_F_BMCTL_BLKDIV_1
#define LCD_F_BLINK_FREQ_CLOCK_DIVIDER_3   LCD_F_BMCTL_BLKDIV_2
#define LCD_F_BLINK_FREQ_CLOCK_DIVIDER_4   LCD_F_BMCTL_BLKDIV_3
#define LCD_F_BLINK_FREQ_CLOCK_DIVIDER_5   LCD_F_BMCTL_BLKDIV_4
#define LCD_F_BLINK_FREQ_CLOCK_DIVIDER_6   LCD_F_BMCTL_BLKDIV_5
#define LCD_F_BLINK_FREQ_CLOCK_DIVIDER_7   LCD_F_BMCTL_BLKDIV_6
#define LCD_F_BLINK_FREQ_CLOCK_DIVIDER_8   LCD_F_BMCTL_BLKDIV_7
#define LCD_F_BLINK_MODE_DISABLED   (LCD_F_BMCTL_BLKMOD_0)
#define LCD_F_BLINK_MODE_INDIVIDUAL_SEGMENTS   (LCD_F_BMCTL_BLKMOD_1)
#define LCD_F_BLINK_MODE_ALL_SEGMENTS   (LCD_F_BMCTL_BLKMOD_2)
#define LCD_F_BLINK_MODE_SWITCHING_BETWEEN_DISPLAY_CONTENTS   (LCD_F_BMCTL_BLKMOD_3)
#define LCD_F_ANIMATION_FREQ_CLOCK_PRESCALAR_512   LCD_F_ANMCTL_ANMPRE_0
#define LCD_F_ANIMATION_FREQ_CLOCK_PRESCALAR_1024   LCD_F_ANMCTL_ANMPRE_1
#define LCD_F_ANIMATION_FREQ_CLOCK_PRESCALAR_2048   LCD_F_ANMCTL_ANMPRE_2
#define LCD_F_ANIMATION_FREQ_CLOCK_PRESCALAR_4096   LCD_F_ANMCTL_ANMPRE_3
#define LCD_F_ANIMATION_FREQ_CLOCK_PRESCALAR_8162   LCD_F_ANMCTL_ANMPRE_4
#define LCD_F_ANIMATION_FREQ_CLOCK_PRESCALAR_16384   LCD_F_ANMCTL_ANMPRE_5
#define LCD_F_ANIMATION_FREQ_CLOCK_PRESCALAR_32768   LCD_F_ANMCTL_ANMPRE_6
#define LCD_F_ANIMATION_FREQ_CLOCK_PRESCALAR_65536   LCD_F_ANMCTL_ANMPRE_7
#define LCD_F_ANIMATION_FREQ_CLOCK_DIVIDER_1   LCD_F_ANMCTL_ANMDIV_0
#define LCD_F_ANIMATION_FREQ_CLOCK_DIVIDER_2   LCD_F_ANMCTL_ANMDIV_1
#define LCD_F_ANIMATION_FREQ_CLOCK_DIVIDER_3   LCD_F_ANMCTL_ANMDIV_2
#define LCD_F_ANIMATION_FREQ_CLOCK_DIVIDER_4   LCD_F_ANMCTL_ANMDIV_3
#define LCD_F_ANIMATION_FREQ_CLOCK_DIVIDER_5   LCD_F_ANMCTL_ANMDIV_4
#define LCD_F_ANIMATION_FREQ_CLOCK_DIVIDER_6   LCD_F_ANMCTL_ANMDIV_5
#define LCD_F_ANIMATION_FREQ_CLOCK_DIVIDER_7   LCD_F_ANMCTL_ANMDIV_6
#define LCD_F_ANIMATION_FREQ_CLOCK_DIVIDER_8   LCD_F_ANMCTL_ANMDIV_7
#define LCD_F_ANIMATION_FRAMES_T0_TO_T7   LCD_F_ANMCTL_ANMSTP_7
#define LCD_F_ANIMATION_FRAMES_T0_TO_T6   LCD_F_ANMCTL_ANMSTP_6
#define LCD_F_ANIMATION_FRAMES_T0_TO_T5   LCD_F_ANMCTL_ANMSTP_5
#define LCD_F_ANIMATION_FRAMES_T0_TO_T4   LCD_F_ANMCTL_ANMSTP_4
#define LCD_F_ANIMATION_FRAMES_T0_TO_T3   LCD_F_ANMCTL_ANMSTP_3
#define LCD_F_ANIMATION_FRAMES_T0_TO_T2   LCD_F_ANMCTL_ANMSTP_2
#define LCD_F_ANIMATION_FRAMES_T0_TO_T1   LCD_F_ANMCTL_ANMSTP_1
#define LCD_F_ANIMATION_FRAMES_T0   LCD_F_ANMCTL_ANMSTP_0
#define LCD_F_SEGMENT_LINE_0   (0)
#define LCD_F_SEGMENT_LINE_1   (1)
#define LCD_F_SEGMENT_LINE_2   (2)
#define LCD_F_SEGMENT_LINE_3   (3)
#define LCD_F_SEGMENT_LINE_4   (4)
#define LCD_F_SEGMENT_LINE_5   (5)
#define LCD_F_SEGMENT_LINE_6   (6)
#define LCD_F_SEGMENT_LINE_7   (7)
#define LCD_F_SEGMENT_LINE_8   (8)
#define LCD_F_SEGMENT_LINE_9   (9)
#define LCD_F_SEGMENT_LINE_10   (10)
#define LCD_F_SEGMENT_LINE_11   (11)
#define LCD_F_SEGMENT_LINE_12   (12)
#define LCD_F_SEGMENT_LINE_13   (13)
#define LCD_F_SEGMENT_LINE_14   (14)
#define LCD_F_SEGMENT_LINE_15   (15)
#define LCD_F_SEGMENT_LINE_16   (16)
#define LCD_F_SEGMENT_LINE_17   (17)
#define LCD_F_SEGMENT_LINE_18   (18)
#define LCD_F_SEGMENT_LINE_19   (19)
#define LCD_F_SEGMENT_LINE_20   (20)
#define LCD_F_SEGMENT_LINE_21   (21)
#define LCD_F_SEGMENT_LINE_22   (22)
#define LCD_F_SEGMENT_LINE_23   (23)
#define LCD_F_SEGMENT_LINE_24   (24)
#define LCD_F_SEGMENT_LINE_25   (25)
#define LCD_F_SEGMENT_LINE_26   (26)
#define LCD_F_SEGMENT_LINE_27   (27)
#define LCD_F_SEGMENT_LINE_28   (28)
#define LCD_F_SEGMENT_LINE_29   (29)
#define LCD_F_SEGMENT_LINE_30   (30)
#define LCD_F_SEGMENT_LINE_31   (31)
#define LCD_F_SEGMENT_LINE_32   (32)
#define LCD_F_SEGMENT_LINE_33   (33)
#define LCD_F_SEGMENT_LINE_34   (34)
#define LCD_F_SEGMENT_LINE_35   (35)
#define LCD_F_SEGMENT_LINE_36   (36)
#define LCD_F_SEGMENT_LINE_37   (37)
#define LCD_F_SEGMENT_LINE_38   (38)
#define LCD_F_SEGMENT_LINE_39   (39)
#define LCD_F_SEGMENT_LINE_40   (40)
#define LCD_F_SEGMENT_LINE_41   (41)
#define LCD_F_SEGMENT_LINE_42   (42)
#define LCD_F_SEGMENT_LINE_43   (43)
#define LCD_F_SEGMENT_LINE_44   (44)
#define LCD_F_SEGMENT_LINE_45   (45)
#define LCD_F_SEGMENT_LINE_46   (46)
#define LCD_F_SEGMENT_LINE_47   (47)
#define LCD_F_MEMORY_COM0   (0x01)
#define LCD_F_MEMORY_COM1   (0x02)
#define LCD_F_MEMORY_COM2   (0x04)
#define LCD_F_MEMORY_COM3   (0x08)
#define LCD_F_MEMORY_COM4   (0x10)
#define LCD_F_MEMORY_COM5   (0x20)
#define LCD_F_MEMORY_COM6   (0x40)
#define LCD_F_MEMORY_COM7   (0x80)
#define LCD_F_BIAS_1_3   (0x0)
#define LCD_F_BIAS_1_2   (LCD_F_VCTL_LCD2B)
#define LCD_F_BIAS_1_4   (LCD_F_VCTL_LCD2B)
#define OFS_LCDM0W   0x120

Referenced by LCD_F_setPinAsCOM().

#define OFS_LCDBM0W   0x160

Referenced by LCD_F_setPinAsCOM().

Typedef Documentation

typedef struct LCD_F_initParam LCD_F_Config

Function Documentation

void LCD_F_initModule ( LCD_F_Config initParams)

Initializes the LCD_F Module.

This function initializes the LCD_F but without turning on. It bascially setup the clock source, clock divider, mux rate, low-power waveform and segments on/off. After calling this function, user can enable/disable internal reference voltage or pin SEG/COM configurations.

Parameters
initParamsis the pointer to LCD_F_Config structure.
Returns
None

References LCD_F_initParam::clockDivider, LCD_F_initParam::clockPrescaler, LCD_F_initParam::clockSource, LCD_F_initParam::muxRate, LCD_F_initParam::segments, and LCD_F_initParam::waveforms.

void LCD_F_turnOn ( void  )

Turns on the LCD_F module.

This function turns the LCD_F on.

Returns
None
void LCD_F_turnOff ( void  )

Turns the LCD_F off.

This function turns the LCD_F off.

Returns
None
void LCD_F_clearAllMemory ( void  )

Clears all LCD_F memory registers.

This function clears all LCD_F memory registers.

Returns
None
void LCD_F_clearAllBlinkingMemory ( void  )

Clears all LCD_F blinking memory registers.

This function clears all LCD_F blinking memory registers.

Returns
None
void LCD_F_selectDisplayMemory ( uint_fast16_t  displayMemory)

Selects display memory.

This function selects display memory either from memory or blinking memory. Please note if the blinking mode is selected as LCD_F_BLINKMODE_INDIVIDUALSEGMENTS or LCD_F_BLINKMODE_ALLSEGMENTS or mux rate >=5, display memory can not be changed. If LCD_F_BLINKMODE_SWITCHDISPLAYCONTENTS is selected, display memory bit reflects current displayed memory.

Parameters
displayMemoryis the desired displayed memory. Valid values are:
  • LCD_F_DISPLAYSOURCE_MEMORY [Default]
  • LCD_F_DISPLAYSOURCE_BLINKINGMEMORY
Returns
None
void LCD_F_setBlinkingControl ( uint_fast16_t  clockPrescalar,
uint_fast16_t  divider,
uint_fast16_t  mode 
)

Sets the blinking control register.

This function sets the blink control related parameter, including blink clock frequency prescalar and blink mode.

Parameters
clockPrescalaris the clock pre-scalar for blinking frequency. Valid values are:
  • LCD_F_BLINK_FREQ_CLOCK_PRESCALAR_512 [Default]
  • LCD_F_BLINK_FREQ_CLOCK_PRESCALAR_1024
  • LCD_F_BLINK_FREQ_CLOCK_PRESCALAR_2048
  • LCD_F_BLINK_FREQ_CLOCK_PRESCALAR_4096
  • LCD_F_BLINK_FREQ_CLOCK_PRESCALAR_8162
  • LCD_F_BLINK_FREQ_CLOCK_PRESCALAR_16384
  • LCD_F_BLINK_FREQ_CLOCK_PRESCALAR_32768
  • LCD_F_BLINK_FREQ_CLOCK_PRESCALAR_65536
clockDivideris the clock divider for blinking frequency. Valid values are:
  • LCD_F_BLINK_FREQ_CLOCK_DIVIDER_1 [Default]
  • LCD_F_BLINK_FREQ_CLOCK_DIVIDER_2
  • LCD_F_BLINK_FREQ_CLOCK_DIVIDER_3
  • LCD_F_BLINK_FREQ_CLOCK_DIVIDER_4
  • LCD_F_BLINK_FREQ_CLOCK_DIVIDER_5
  • LCD_F_BLINK_FREQ_CLOCK_DIVIDER_6
  • LCD_F_BLINK_FREQ_CLOCK_DIVIDER_7
  • LCD_F_BLINK_FREQ_CLOCK_DIVIDER_8
modeis the select for blinking mode. Valid values are:
  • LCD_F_BLINK_MODE_DISABLED [Default]
  • LCD_F_BLINK_MODE_INDIVIDUAL_SEGMENTS
  • LCD_F_BLINK_MODE_ALL_SEGMENTS
  • LCD_F_BLINK_MODE_SWITCHING_BETWEEN_DISPLAY_CONTENTS
Returns
None
void LCD_F_setAnimationControl ( uint_fast16_t  clockPrescalar,
uint_fast16_t  divider,
uint_fast16_t  frames 
)

Sets the animation control register.

This function sets the animation control related parameter, including animation clock frequency prescalar, divider, and frame settings

Parameters
clockPrescalaris the clock pre-scalar for animation frequency. Valid values are:
  • LCD_F_ANIMATION_FREQ_CLOCK_PRESCALAR_512 [Default]
  • LCD_F_ANIMATION_FREQ_CLOCK_PRESCALAR_1024
  • LCD_F_ANIMATION_FREQ_CLOCK_PRESCALAR_2048
  • LCD_F_ANIMATION_FREQ_CLOCK_PRESCALAR_4096
  • LCD_F_ANIMATION_FREQ_CLOCK_PRESCALAR_8162
  • LCD_F_ANIMATION_FREQ_CLOCK_PRESCALAR_16384
  • LCD_F_ANIMATION_FREQ_CLOCK_PRESCALAR_32768
  • LCD_F_ANIMATION_FREQ_CLOCK_PRESCALAR_65536
clockDivideris the clock divider for animation frequency. Valid values are:
  • LCD_F_ANIMATION_FREQ_CLOCK_DIVIDER_1 [Default]
  • LCD_F_ANIMATION_FREQ_CLOCK_DIVIDER_2
  • LCD_F_ANIMATION_FREQ_CLOCK_DIVIDER_3
  • LCD_F_ANIMATION_FREQ_CLOCK_DIVIDER_4
  • LCD_F_ANIMATION_FREQ_CLOCK_DIVIDER_5
  • LCD_F_ANIMATION_FREQ_CLOCK_DIVIDER_6
  • LCD_F_ANIMATION_FREQ_CLOCK_DIVIDER_7
  • LCD_F_ANIMATION_FREQ_CLOCK_DIVIDER_8
framesis number of animations frames to be repeated Valid values are:
  • LCD_F_ANIMATION_FRAMES_T0_TO_T7
  • LCD_F_ANIMATION_FRAMES_T0_TO_T6
  • LCD_F_ANIMATION_FRAMES_T0_TO_T5
  • LCD_F_ANIMATION_FRAMES_T0_TO_T4
  • LCD_F_ANIMATION_FRAMES_T0_TO_T3
  • LCD_F_ANIMATION_FRAMES_T0_TO_T2
  • LCD_F_ANIMATION_FRAMES_T0_TO_T1
  • LCD_F_ANIMATION_FRAMES_T0
Returns
None
void LCD_F_enableAnimation ( void  )

Enables animation on the LCD_F controller.

This function turns on animation for the LCD_F controller.

Returns
None
void LCD_F_disableAnimation ( void  )

Enables animation on the LCD_F controller.

This function turns on animation for the LCD_F controller.

Returns
None
void LCD_F_clearAllAnimationMemory ( void  )

Clears all LCD_F animation memory registers.

This function clears all LCD_F animation memory registers.

Returns
None
void LCD_F_setPinAsLCDFunction ( uint_fast8_t  pin)

Sets the LCD_F pins as LCD function pin.

This function sets the LCD_F pins as LCD function pin.

Parameters
pinis the select pin set as LCD function. Valid values are:
  • LCD_F_SEGMENT_LINE_0
  • LCD_F_SEGMENT_LINE_1
  • LCD_F_SEGMENT_LINE_2
  • LCD_F_SEGMENT_LINE_3
  • LCD_F_SEGMENT_LINE_4
  • LCD_F_SEGMENT_LINE_5
  • LCD_F_SEGMENT_LINE_6
  • LCD_F_SEGMENT_LINE_7
  • LCD_F_SEGMENT_LINE_8
  • LCD_F_SEGMENT_LINE_9
  • LCD_F_SEGMENT_LINE_10
  • LCD_F_SEGMENT_LINE_11
  • LCD_F_SEGMENT_LINE_12
  • LCD_F_SEGMENT_LINE_13
  • LCD_F_SEGMENT_LINE_14
  • LCD_F_SEGMENT_LINE_15
  • LCD_F_SEGMENT_LINE_16
  • LCD_F_SEGMENT_LINE_17
  • LCD_F_SEGMENT_LINE_18
  • LCD_F_SEGMENT_LINE_19
  • LCD_F_SEGMENT_LINE_20
  • LCD_F_SEGMENT_LINE_21
  • LCD_F_SEGMENT_LINE_22
  • LCD_F_SEGMENT_LINE_23
  • LCD_F_SEGMENT_LINE_24
  • LCD_F_SEGMENT_LINE_25
  • LCD_F_SEGMENT_LINE_26
  • LCD_F_SEGMENT_LINE_27
  • LCD_F_SEGMENT_LINE_28
  • LCD_F_SEGMENT_LINE_29
  • LCD_F_SEGMENT_LINE_30
  • LCD_F_SEGMENT_LINE_31
  • LCD_F_SEGMENT_LINE_32
  • LCD_F_SEGMENT_LINE_33
  • LCD_F_SEGMENT_LINE_34
  • LCD_F_SEGMENT_LINE_35
  • LCD_F_SEGMENT_LINE_36
  • LCD_F_SEGMENT_LINE_37
  • LCD_F_SEGMENT_LINE_38
  • LCD_F_SEGMENT_LINE_39
  • LCD_F_SEGMENT_LINE_40
  • LCD_F_SEGMENT_LINE_41
  • LCD_F_SEGMENT_LINE_42
  • LCD_F_SEGMENT_LINE_43
  • LCD_F_SEGMENT_LINE_44
  • LCD_F_SEGMENT_LINE_45
  • LCD_F_SEGMENT_LINE_46
  • LCD_F_SEGMENT_LINE_47
Returns
None
void LCD_F_setPinAsPortFunction ( uint_fast8_t  pin)

Sets the LCD_F pins as port function pin.

Parameters
baseAddressis the base address of the LCD_F module.
pinis the select pin set as Port function. Valid values are:
  • LCD_F_SEGMENT_LINE_0
  • LCD_F_SEGMENT_LINE_1
  • LCD_F_SEGMENT_LINE_2
  • LCD_F_SEGMENT_LINE_3
  • LCD_F_SEGMENT_LINE_4
  • LCD_F_SEGMENT_LINE_5
  • LCD_F_SEGMENT_LINE_6
  • LCD_F_SEGMENT_LINE_7
  • LCD_F_SEGMENT_LINE_8
  • LCD_F_SEGMENT_LINE_9
  • LCD_F_SEGMENT_LINE_10
  • LCD_F_SEGMENT_LINE_11
  • LCD_F_SEGMENT_LINE_12
  • LCD_F_SEGMENT_LINE_13
  • LCD_F_SEGMENT_LINE_14
  • LCD_F_SEGMENT_LINE_15
  • LCD_F_SEGMENT_LINE_16
  • LCD_F_SEGMENT_LINE_17
  • LCD_F_SEGMENT_LINE_18
  • LCD_F_SEGMENT_LINE_19
  • LCD_F_SEGMENT_LINE_20
  • LCD_F_SEGMENT_LINE_21
  • LCD_F_SEGMENT_LINE_22
  • LCD_F_SEGMENT_LINE_23
  • LCD_F_SEGMENT_LINE_24
  • LCD_F_SEGMENT_LINE_25
  • LCD_F_SEGMENT_LINE_26
  • LCD_F_SEGMENT_LINE_27
  • LCD_F_SEGMENT_LINE_28
  • LCD_F_SEGMENT_LINE_29
  • LCD_F_SEGMENT_LINE_30
  • LCD_F_SEGMENT_LINE_31
  • LCD_F_SEGMENT_LINE_32
  • LCD_F_SEGMENT_LINE_33
  • LCD_F_SEGMENT_LINE_34
  • LCD_F_SEGMENT_LINE_35
  • LCD_F_SEGMENT_LINE_36
  • LCD_F_SEGMENT_LINE_37
  • LCD_F_SEGMENT_LINE_38
  • LCD_F_SEGMENT_LINE_39
  • LCD_F_SEGMENT_LINE_40
  • LCD_F_SEGMENT_LINE_41
  • LCD_F_SEGMENT_LINE_42
  • LCD_F_SEGMENT_LINE_43
  • LCD_F_SEGMENT_LINE_44
  • LCD_F_SEGMENT_LINE_45
  • LCD_F_SEGMENT_LINE_46
  • LCD_F_SEGMENT_LINE_47
Returns
None
void LCD_F_setPinsAsLCDFunction ( uint_fast8_t  startPin,
uint8_t  endPin 
)

Sets the LCD_F pins as LCD function pin.

This function sets the LCD_F pins as LCD function pin. Instead of passing the all the possible pins, it just requires the start pin and the end pin.

Parameters
startPinis the starting pin to be configured as LCD function pin. Valid values are:
  • LCD_F_SEGMENT_LINE_0
  • LCD_F_SEGMENT_LINE_1
  • LCD_F_SEGMENT_LINE_2
  • LCD_F_SEGMENT_LINE_3
  • LCD_F_SEGMENT_LINE_4
  • LCD_F_SEGMENT_LINE_5
  • LCD_F_SEGMENT_LINE_6
  • LCD_F_SEGMENT_LINE_7
  • LCD_F_SEGMENT_LINE_8
  • LCD_F_SEGMENT_LINE_9
  • LCD_F_SEGMENT_LINE_10
  • LCD_F_SEGMENT_LINE_11
  • LCD_F_SEGMENT_LINE_12
  • LCD_F_SEGMENT_LINE_13
  • LCD_F_SEGMENT_LINE_14
  • LCD_F_SEGMENT_LINE_15
  • LCD_F_SEGMENT_LINE_16
  • LCD_F_SEGMENT_LINE_17
  • LCD_F_SEGMENT_LINE_18
  • LCD_F_SEGMENT_LINE_19
  • LCD_F_SEGMENT_LINE_20
  • LCD_F_SEGMENT_LINE_21
  • LCD_F_SEGMENT_LINE_22
  • LCD_F_SEGMENT_LINE_23
  • LCD_F_SEGMENT_LINE_24
  • LCD_F_SEGMENT_LINE_25
  • LCD_F_SEGMENT_LINE_26
  • LCD_F_SEGMENT_LINE_27
  • LCD_F_SEGMENT_LINE_28
  • LCD_F_SEGMENT_LINE_29
  • LCD_F_SEGMENT_LINE_30
  • LCD_F_SEGMENT_LINE_31
  • LCD_F_SEGMENT_LINE_32
  • LCD_F_SEGMENT_LINE_33
  • LCD_F_SEGMENT_LINE_34
  • LCD_F_SEGMENT_LINE_35
  • LCD_F_SEGMENT_LINE_36
  • LCD_F_SEGMENT_LINE_37
  • LCD_F_SEGMENT_LINE_38
  • LCD_F_SEGMENT_LINE_39
  • LCD_F_SEGMENT_LINE_40
  • LCD_F_SEGMENT_LINE_41
  • LCD_F_SEGMENT_LINE_42
  • LCD_F_SEGMENT_LINE_43
  • LCD_F_SEGMENT_LINE_44
  • LCD_F_SEGMENT_LINE_45
  • LCD_F_SEGMENT_LINE_46
  • LCD_F_SEGMENT_LINE_47
endPinis the ending pin to be configured as LCD function pin. Valid values are:
  • LCD_F_SEGMENT_LINE_0
  • LCD_F_SEGMENT_LINE_1
  • LCD_F_SEGMENT_LINE_2
  • LCD_F_SEGMENT_LINE_3
  • LCD_F_SEGMENT_LINE_4
  • LCD_F_SEGMENT_LINE_5
  • LCD_F_SEGMENT_LINE_6
  • LCD_F_SEGMENT_LINE_7
  • LCD_F_SEGMENT_LINE_8
  • LCD_F_SEGMENT_LINE_9
  • LCD_F_SEGMENT_LINE_10
  • LCD_F_SEGMENT_LINE_11
  • LCD_F_SEGMENT_LINE_12
  • LCD_F_SEGMENT_LINE_13
  • LCD_F_SEGMENT_LINE_14
  • LCD_F_SEGMENT_LINE_15
  • LCD_F_SEGMENT_LINE_16
  • LCD_F_SEGMENT_LINE_17
  • LCD_F_SEGMENT_LINE_18
  • LCD_F_SEGMENT_LINE_19
  • LCD_F_SEGMENT_LINE_20
  • LCD_F_SEGMENT_LINE_21
  • LCD_F_SEGMENT_LINE_22
  • LCD_F_SEGMENT_LINE_23
  • LCD_F_SEGMENT_LINE_24
  • LCD_F_SEGMENT_LINE_25
  • LCD_F_SEGMENT_LINE_26
  • LCD_F_SEGMENT_LINE_27
  • LCD_F_SEGMENT_LINE_28
  • LCD_F_SEGMENT_LINE_29
  • LCD_F_SEGMENT_LINE_30
  • LCD_F_SEGMENT_LINE_31
  • LCD_F_SEGMENT_LINE_32
  • LCD_F_SEGMENT_LINE_33
  • LCD_F_SEGMENT_LINE_34
  • LCD_F_SEGMENT_LINE_35
  • LCD_F_SEGMENT_LINE_36
  • LCD_F_SEGMENT_LINE_37
  • LCD_F_SEGMENT_LINE_38
  • LCD_F_SEGMENT_LINE_39
  • LCD_F_SEGMENT_LINE_40
  • LCD_F_SEGMENT_LINE_41
  • LCD_F_SEGMENT_LINE_42
  • LCD_F_SEGMENT_LINE_43
  • LCD_F_SEGMENT_LINE_44
  • LCD_F_SEGMENT_LINE_45
  • LCD_F_SEGMENT_LINE_46
  • LCD_F_SEGMENT_LINE_47
Returns
None
void LCD_F_setPinAsCOM ( uint8_t  pin,
uint_fast8_t  com 
)

Sets the LCD_F pin as a common line.

This function sets the LCD_F pin as a common line and assigns the corresponding memory pin to a specific COM line.

Parameters
pinis the selected pin to be configured as common line. Valid values are:
  • LCD_F_SEGMENT_LINE_0
  • LCD_F_SEGMENT_LINE_1
  • LCD_F_SEGMENT_LINE_2
  • LCD_F_SEGMENT_LINE_3
  • LCD_F_SEGMENT_LINE_4
  • LCD_F_SEGMENT_LINE_5
  • LCD_F_SEGMENT_LINE_6
  • LCD_F_SEGMENT_LINE_7
  • LCD_F_SEGMENT_LINE_8
  • LCD_F_SEGMENT_LINE_9
  • LCD_F_SEGMENT_LINE_10
  • LCD_F_SEGMENT_LINE_11
  • LCD_F_SEGMENT_LINE_12
  • LCD_F_SEGMENT_LINE_13
  • LCD_F_SEGMENT_LINE_14
  • LCD_F_SEGMENT_LINE_15
  • LCD_F_SEGMENT_LINE_16
  • LCD_F_SEGMENT_LINE_17
  • LCD_F_SEGMENT_LINE_18
  • LCD_F_SEGMENT_LINE_19
  • LCD_F_SEGMENT_LINE_20
  • LCD_F_SEGMENT_LINE_21
  • LCD_F_SEGMENT_LINE_22
  • LCD_F_SEGMENT_LINE_23
  • LCD_F_SEGMENT_LINE_24
  • LCD_F_SEGMENT_LINE_25
  • LCD_F_SEGMENT_LINE_26
  • LCD_F_SEGMENT_LINE_27
  • LCD_F_SEGMENT_LINE_28
  • LCD_F_SEGMENT_LINE_29
  • LCD_F_SEGMENT_LINE_30
  • LCD_F_SEGMENT_LINE_31
  • LCD_F_SEGMENT_LINE_32
  • LCD_F_SEGMENT_LINE_33
  • LCD_F_SEGMENT_LINE_34
  • LCD_F_SEGMENT_LINE_35
  • LCD_F_SEGMENT_LINE_36
  • LCD_F_SEGMENT_LINE_37
  • LCD_F_SEGMENT_LINE_38
  • LCD_F_SEGMENT_LINE_39
  • LCD_F_SEGMENT_LINE_40
  • LCD_F_SEGMENT_LINE_41
  • LCD_F_SEGMENT_LINE_42
  • LCD_F_SEGMENT_LINE_43
  • LCD_F_SEGMENT_LINE_44
  • LCD_F_SEGMENT_LINE_45
  • LCD_F_SEGMENT_LINE_46
  • LCD_F_SEGMENT_LINE_47
comis the selected COM number for the common line. Valid values are:
  • LCD_F_MEMORY_COM0
  • LCD_F_MEMORY_COM1
  • LCD_F_MEMORY_COM2
  • LCD_F_MEMORY_COM3
  • LCD_F_MEMORY_COM4 - only for 5-Mux/6-Mux/7-Mux/8-Mux
  • LCD_F_MEMORY_COM5 - only for 5-Mux/6-Mux/7-Mux/8-Mux
  • LCD_F_MEMORY_COM6 - only for 5-Mux/6-Mux/7-Mux/8-Mux
  • LCD_F_MEMORY_COM7 - only for 5-Mux/6-Mux/7-Mux/8-Mux
Returns
None

References HWREG8, OFS_LCDBM0W, and OFS_LCDM0W.

void LCD_F_setPinAsSEG ( uint_fast8_t  pin)

Sets the LCD_F pin as a segment line.

This function sets the LCD_F pin as segment line.

Parameters
pinis the selected pin to be configed as segment line. Valid values are:
  • LCD_F_SEGMENT_LINE_0
  • LCD_F_SEGMENT_LINE_1
  • LCD_F_SEGMENT_LINE_2
  • LCD_F_SEGMENT_LINE_3
  • LCD_F_SEGMENT_LINE_4
  • LCD_F_SEGMENT_LINE_5
  • LCD_F_SEGMENT_LINE_6
  • LCD_F_SEGMENT_LINE_7
  • LCD_F_SEGMENT_LINE_8
  • LCD_F_SEGMENT_LINE_9
  • LCD_F_SEGMENT_LINE_10
  • LCD_F_SEGMENT_LINE_11
  • LCD_F_SEGMENT_LINE_12
  • LCD_F_SEGMENT_LINE_13
  • LCD_F_SEGMENT_LINE_14
  • LCD_F_SEGMENT_LINE_15
  • LCD_F_SEGMENT_LINE_16
  • LCD_F_SEGMENT_LINE_17
  • LCD_F_SEGMENT_LINE_18
  • LCD_F_SEGMENT_LINE_19
  • LCD_F_SEGMENT_LINE_20
  • LCD_F_SEGMENT_LINE_21
  • LCD_F_SEGMENT_LINE_22
  • LCD_F_SEGMENT_LINE_23
  • LCD_F_SEGMENT_LINE_24
  • LCD_F_SEGMENT_LINE_25
  • LCD_F_SEGMENT_LINE_26
  • LCD_F_SEGMENT_LINE_27
  • LCD_F_SEGMENT_LINE_28
  • LCD_F_SEGMENT_LINE_29
  • LCD_F_SEGMENT_LINE_30
  • LCD_F_SEGMENT_LINE_31
  • LCD_F_SEGMENT_LINE_32
  • LCD_F_SEGMENT_LINE_33
  • LCD_F_SEGMENT_LINE_34
  • LCD_F_SEGMENT_LINE_35
  • LCD_F_SEGMENT_LINE_36
  • LCD_F_SEGMENT_LINE_37
  • LCD_F_SEGMENT_LINE_38
  • LCD_F_SEGMENT_LINE_39
  • LCD_F_SEGMENT_LINE_40
  • LCD_F_SEGMENT_LINE_41
  • LCD_F_SEGMENT_LINE_42
  • LCD_F_SEGMENT_LINE_43
  • LCD_F_SEGMENT_LINE_44
  • LCD_F_SEGMENT_LINE_45
  • LCD_F_SEGMENT_LINE_46
  • LCD_F_SEGMENT_LINE_47
Returns
None
void LCD_F_selectBias ( uint_fast16_t  bias)

Selects the bias level.

Parameters
biasis the select for bias level. Valid values are:
  • LCD_F_BIAS_1_3 [Default] - 1/3 bias
  • LCD_F_BIAS_1_4 - 1/4 bias
  • LCD_F_BIAS_1_2 - 1/2 bias
Note
Quarter (1/4) BIAS mode is only available in 5-mux to 8-mux. In 2-mux to 4-mux modes, this value will result in a third BIAS (1/3)
Returns
None
void LCD_F_setVLCDSource ( uint_fast16_t  v2v3v4Source,
uint_fast16_t  v5Source 
)

Sets the voltage source for V2/V3/V4 and V5.

Parameters
v2v3v4Sourceis the V2/V3/V4 source select. Valid values are:
  • LCD_F_V2V3V4_GENERATED_INTERNALLY_NOT_SWITCHED_TO_PINS [Default]
  • LCD_F_V2V3V4_GENERATED_INTERNALLY_SWITCHED_TO_PINS
  • LCD_F_V2V3V4_SOURCED_EXTERNALLY
v5Sourceis the V5 source select. Valid values are:
  • LCD_F_V5_VSS [Default]
  • LCD_F_V5_SOURCED_FROM_R03
Returns
None
void LCD_F_clearInterrupt ( uint32_t  mask)

Clears the LCD_F selected interrupt flags.

This function clears the specified interrupt flags.

Parameters
maskis the masked interrupt flag to be cleared. Mask value is the logical OR of any of the following:
  • LCD_F_BLINKING_SEGMENTS_ON_INTERRUPT
  • LCD_F_BLINKING_SEGMENTS_OFF_INTERRUPT
  • LCD_F_FRAME_INTERRUPT
  • LCD_F_ANIMATION_LOOP_INTERRUPT
  • LCD_F_ANIMATION_STEP_INTERRUPT
Returns
None
uint32_t LCD_F_getInterruptStatus ( void  )

Returns the status of the selected interrupt flags.

This function returns the status of the selected interrupt flags.

Returns
The current interrupt flag status. Can be a logical OR of:
  • LCD_F_BLINKING_SEGMENTS_ON_INTERRUPT
  • LCD_F_BLINKING_SEGMENTS_OFF_INTERRUPT
  • LCD_F_FRAME_INTERRUPT
  • LCD_F_ANIMATION_LOOP_INTERRUPT
  • LCD_F_ANIMATION_STEP_INTERRUPT
uint32_t LCD_F_getEnabledInterruptStatus ( void  )

Returns the status of the selected interrupt flags masked with the currently enabled interrupts.

Returns
The current interrupt flag status. Can be a logical OR of:
  • LCD_F_BLINKING_SEGMENTS_ON_INTERRUPT
  • LCD_F_BLINKING_SEGMENTS_OFF_INTERRUPT
  • LCD_F_FRAME_INTERRUPT
  • LCD_F_ANIMATION_LOOP_INTERRUPT
  • LCD_F_ANIMATION_STEP_INTERRUPT
void LCD_F_enableInterrupt ( uint32_t  mask)

Enables the LCD_F selected interrupts.

This function enables the specified interrupts

Parameters
maskis the variable containing interrupt flags to be enabled. Mask value is the logical OR of any of the following:
  • LCD_F_BLINKING_SEGMENTS_ON_INTERRUPT
  • LCD_F_BLINKING_SEGMENTS_OFF_INTERRUPT
  • LCD_F_FRAME_INTERRUPT
  • LCD_F_ANIMATION_LOOP_INTERRUPT
  • LCD_F_ANIMATION_STEP_INTERRUPT
Returns
None
void LCD_F_disableInterrupt ( uint32_t  mask)

Disables the LCD_F selected interrupts.

This function disables the specified interrupts.

Parameters
maskis the variable containing interrupt flags to be disabled Mask value is the logical OR of any of the following:
  • LCD_F_BLINKING_SEGMENTS_ON_INTERRUPT
  • LCD_F_BLINKING_SEGMENTS_OFF_INTERRUPT
  • LCD_F_FRAME_INTERRUPT
  • LCD_F_ANIMATION_LOOP_INTERRUPT
  • LCD_F_ANIMATION_STEP_INTERRUPT
Returns
None
void LCD_F_registerInterrupt ( void(*)(void)  intHandler)

Registers an interrupt handler for LCD_F interrupt.

Parameters
intHandleris a pointer to the function to be called when the LCD_F interrupt occurs.

This function registers the handler to be called when a LCD_F interrupt occurs. This function enables the global interrupt in the interrupt controller; specific LCD_F interrupts must be enabled via LCD_F_enableInterrupt(). It is the interrupt handler's responsibility to clear the interrupt source through LCD_F_clearInterruptFlag().

Returns
None.

References INT_LCD_F, Interrupt_enableInterrupt(), and Interrupt_registerInterrupt().

void LCD_F_unregisterInterrupt ( void  )

Unregisters the interrupt handler for the LCD_F interrupt

This function unregisters the handler to be called when LCD_F interrupt occurs. This function also masks off the interrupt in the interrupt controller so that the interrupt handler no longer is called.

See Also
Interrupt_registerInterrupt() for important information about registering interrupt handlers.
Returns
None.

References INT_LCD_F, Interrupt_disableInterrupt(), and Interrupt_unregisterInterrupt().


Copyright 2018, Texas Instruments Incorporated