Data Fields
__sFlashCtl_ProtectionRegister Struct Reference

#include <flash_a.h>

Data Fields

uint32_t B0_MAIN_R0
 
uint32_t B0_MAIN_R1
 
uint32_t B0_MAIN_R2
 
uint32_t B0_MAIN_R3
 
uint32_t B0_MAIN_R4
 
uint32_t B0_MAIN_R5
 
uint32_t B0_MAIN_R6
 
uint32_t B0_MAIN_R7
 
uint32_t B1_MAIN_R0
 
uint32_t B1_MAIN_R1
 
uint32_t B1_MAIN_R2
 
uint32_t B1_MAIN_R3
 
uint32_t B1_MAIN_R4
 
uint32_t B1_MAIN_R5
 
uint32_t B1_MAIN_R6
 
uint32_t B1_MAIN_R7
 
uint32_t B0_INFO_R0
 
uint32_t B1_INFO_R0
 

Field Documentation

uint32_t __sFlashCtl_ProtectionRegister::B0_MAIN_R0
uint32_t __sFlashCtl_ProtectionRegister::B0_MAIN_R1
uint32_t __sFlashCtl_ProtectionRegister::B0_MAIN_R2
uint32_t __sFlashCtl_ProtectionRegister::B0_MAIN_R3
uint32_t __sFlashCtl_ProtectionRegister::B0_MAIN_R4
uint32_t __sFlashCtl_ProtectionRegister::B0_MAIN_R5
uint32_t __sFlashCtl_ProtectionRegister::B0_MAIN_R6
uint32_t __sFlashCtl_ProtectionRegister::B0_MAIN_R7
uint32_t __sFlashCtl_ProtectionRegister::B1_MAIN_R0
uint32_t __sFlashCtl_ProtectionRegister::B1_MAIN_R1
uint32_t __sFlashCtl_ProtectionRegister::B1_MAIN_R2
uint32_t __sFlashCtl_ProtectionRegister::B1_MAIN_R3
uint32_t __sFlashCtl_ProtectionRegister::B1_MAIN_R4
uint32_t __sFlashCtl_ProtectionRegister::B1_MAIN_R5
uint32_t __sFlashCtl_ProtectionRegister::B1_MAIN_R6
uint32_t __sFlashCtl_ProtectionRegister::B1_MAIN_R7
uint32_t __sFlashCtl_ProtectionRegister::B0_INFO_R0
uint32_t __sFlashCtl_ProtectionRegister::B1_INFO_R0

The documentation for this struct was generated from the following file:

Copyright 2018, Texas Instruments Incorporated