Data Fields
_Timer_A_CaptureModeConfig Struct Reference

Type definition for _Timer_A_CaptureModeConfig structure. More...

#include <timer_a.h>

Data Fields

uint_fast16_t captureRegister
 
uint_fast16_t captureMode
 
uint_fast16_t captureInputSelect
 
uint_fast16_t synchronizeCaptureSource
 
uint_fast8_t captureInterruptEnable
 
uint_fast16_t captureOutputMode
 

Detailed Description

Type definition for _Timer_A_CaptureModeConfig structure.

ypedef Timer_A_CaptureModeConfig

Configuration structure for capture mode in the Timer_A module. See Timer_A_initCapture for parameter documentation.

Field Documentation

uint_fast16_t _Timer_A_CaptureModeConfig::captureRegister

Referenced by Timer_A_initCapture().

uint_fast16_t _Timer_A_CaptureModeConfig::captureMode

Referenced by Timer_A_initCapture().

uint_fast16_t _Timer_A_CaptureModeConfig::captureInputSelect

Referenced by Timer_A_initCapture().

uint_fast16_t _Timer_A_CaptureModeConfig::synchronizeCaptureSource

Referenced by Timer_A_initCapture().

uint_fast8_t _Timer_A_CaptureModeConfig::captureInterruptEnable

Referenced by Timer_A_initCapture().

uint_fast16_t _Timer_A_CaptureModeConfig::captureOutputMode

Referenced by Timer_A_initCapture().


The documentation for this struct was generated from the following file:

Copyright 2018, Texas Instruments Incorporated