Data Fields
_Timer_A_CompareModeConfig Struct Reference

Type definition for _Timer_A_CompareModeConfig structure. More...

#include <timer_a.h>

Data Fields

uint_fast16_t compareRegister
 
uint_fast16_t compareInterruptEnable
 
uint_fast16_t compareOutputMode
 
uint_fast16_t compareValue
 

Detailed Description

Type definition for _Timer_A_CompareModeConfig structure.

ypedef Timer_A_CompareModeConfig

Configuration structure for compare mode in the Timer_A module. See Timer_A_initCompare for parameter documentation.

Field Documentation

uint_fast16_t _Timer_A_CompareModeConfig::compareRegister

Referenced by Timer_A_initCompare().

uint_fast16_t _Timer_A_CompareModeConfig::compareInterruptEnable

Referenced by Timer_A_initCompare().

uint_fast16_t _Timer_A_CompareModeConfig::compareOutputMode

Referenced by Timer_A_initCompare().

uint_fast16_t _Timer_A_CompareModeConfig::compareValue

Referenced by Timer_A_initCompare().


The documentation for this struct was generated from the following file:

Copyright 2018, Texas Instruments Incorporated