Data Structures | Macros | Typedefs | Variables
I2CSlaveMSP432.h File Reference

Detailed Description

I2CSlave driver implementation for the EUSCI controller on MSP432.

============================================================================

This I2CSlave driver implementation is designed to operate on a EUCSI controller in I2CSlave mode. The I2CSlaveMSP432 header file should be included in an application as follows:

#include <ti/drivers/I2CSlaveMSP432.h>

#include <stdint.h>
#include <stdbool.h>
#include <ti/drivers/I2CSlave.h>
#include <ti/drivers/dpl/HwiP.h>
#include <ti/drivers/dpl/SemaphoreP.h>
#include <ti/drivers/Power.h>
Include dependency graph for I2CSlaveMSP432.h:

Go to the source code of this file.

Data Structures

struct  I2CSlaveMSP432_HWAttrs
 I2CSlaveMSP432 Hardware attributes These fields are used by driverlib APIs and therefore must be populated by driverlib macro definitions. For MSP432 driverlib these definitions are found in: More...
 
struct  I2CSlaveMSP432_Object
 I2CSlaveMSP432 Object. More...
 

Macros

#define I2CSLAVEMSP432_P1_6_UCB0SDA   0x00000116 /* Primary, port 1, pin 6 */
 
#define I2CSLAVEMSP432_P1_7_UCB0SCL   0x00000117 /* Primary, port 1, pin 7 */
 
#define I2CSLAVEMSP432_P2_0_UCB0SDA   ((PMAP_UCB0SDA << 10) | 0x20)
 
#define I2CSLAVEMSP432_P2_0_UCB0SCL   ((PMAP_UCB0SCL << 10) | 0x20)
 
#define I2CSLAVEMSP432_P2_0_UCB2SDA   ((PMAP_UCB2SDA << 10) | 0x20)
 
#define I2CSLAVEMSP432_P2_0_UCB2SCL   ((PMAP_UCB2SCL << 10) | 0x20)
 
#define I2CSLAVEMSP432_P2_1_UCB0SDA   ((PMAP_UCB0SDA << 10) | 0x21)
 
#define I2CSLAVEMSP432_P2_1_UCB0SCL   ((PMAP_UCB0SCL << 10) | 0x21)
 
#define I2CSLAVEMSP432_P2_1_UCB2SDA   ((PMAP_UCB2SDA << 10) | 0x21)
 
#define I2CSLAVEMSP432_P2_1_UCB2SCL   ((PMAP_UCB2SCL << 10) | 0x21)
 
#define I2CSLAVEMSP432_P2_2_UCB0SDA   ((PMAP_UCB0SDA << 10) | 0x22)
 
#define I2CSLAVEMSP432_P2_2_UCB0SCL   ((PMAP_UCB0SCL << 10) | 0x22)
 
#define I2CSLAVEMSP432_P2_2_UCB2SDA   ((PMAP_UCB2SDA << 10) | 0x22)
 
#define I2CSLAVEMSP432_P2_2_UCB2SCL   ((PMAP_UCB2SCL << 10) | 0x22)
 
#define I2CSLAVEMSP432_P2_3_UCB0SDA   ((PMAP_UCB0SDA << 10) | 0x23)
 
#define I2CSLAVEMSP432_P2_3_UCB0SCL   ((PMAP_UCB0SCL << 10) | 0x23)
 
#define I2CSLAVEMSP432_P2_3_UCB2SDA   ((PMAP_UCB2SDA << 10) | 0x23)
 
#define I2CSLAVEMSP432_P2_3_UCB2SCL   ((PMAP_UCB2SCL << 10) | 0x23)
 
#define I2CSLAVEMSP432_P2_4_UCB0SDA   ((PMAP_UCB0SDA << 10) | 0x24)
 
#define I2CSLAVEMSP432_P2_4_UCB0SCL   ((PMAP_UCB0SCL << 10) | 0x24)
 
#define I2CSLAVEMSP432_P2_4_UCB2SDA   ((PMAP_UCB2SDA << 10) | 0x24)
 
#define I2CSLAVEMSP432_P2_4_UCB2SCL   ((PMAP_UCB2SCL << 10) | 0x24)
 
#define I2CSLAVEMSP432_P2_5_UCB0SDA   ((PMAP_UCB0SDA << 10) | 0x25)
 
#define I2CSLAVEMSP432_P2_5_UCB0SCL   ((PMAP_UCB0SCL << 10) | 0x25)
 
#define I2CSLAVEMSP432_P2_5_UCB2SDA   ((PMAP_UCB2SDA << 10) | 0x25)
 
#define I2CSLAVEMSP432_P2_5_UCB2SCL   ((PMAP_UCB2SCL << 10) | 0x25)
 
#define I2CSLAVEMSP432_P2_6_UCB0SDA   ((PMAP_UCB0SDA << 10) | 0x26)
 
#define I2CSLAVEMSP432_P2_6_UCB0SCL   ((PMAP_UCB0SCL << 10) | 0x26)
 
#define I2CSLAVEMSP432_P2_6_UCB2SDA   ((PMAP_UCB2SDA << 10) | 0x26)
 
#define I2CSLAVEMSP432_P2_6_UCB2SCL   ((PMAP_UCB2SCL << 10) | 0x26)
 
#define I2CSLAVEMSP432_P2_7_UCB0SDA   ((PMAP_UCB0SDA << 10) | 0x27)
 
#define I2CSLAVEMSP432_P2_7_UCB0SCL   ((PMAP_UCB0SCL << 10) | 0x27)
 
#define I2CSLAVEMSP432_P2_7_UCB2SDA   ((PMAP_UCB2SDA << 10) | 0x27)
 
#define I2CSLAVEMSP432_P2_7_UCB2SCL   ((PMAP_UCB2SCL << 10) | 0x27)
 
#define I2CSLAVEMSP432_P3_0_UCB0SDA   ((PMAP_UCB0SDA << 10) | 0x30)
 
#define I2CSLAVEMSP432_P3_0_UCB0SCL   ((PMAP_UCB0SCL << 10) | 0x30)
 
#define I2CSLAVEMSP432_P3_0_UCB2SDA   ((PMAP_UCB2SDA << 10) | 0x30)
 
#define I2CSLAVEMSP432_P3_0_UCB2SCL   ((PMAP_UCB2SCL << 10) | 0x30)
 
#define I2CSLAVEMSP432_P3_1_UCB0SDA   ((PMAP_UCB0SDA << 10) | 0x31)
 
#define I2CSLAVEMSP432_P3_1_UCB0SCL   ((PMAP_UCB0SCL << 10) | 0x31)
 
#define I2CSLAVEMSP432_P3_1_UCB2SDA   ((PMAP_UCB2SDA << 10) | 0x31)
 
#define I2CSLAVEMSP432_P3_1_UCB2SCL   ((PMAP_UCB2SCL << 10) | 0x31)
 
#define I2CSLAVEMSP432_P3_2_UCB0SDA   ((PMAP_UCB0SDA << 10) | 0x32)
 
#define I2CSLAVEMSP432_P3_2_UCB0SCL   ((PMAP_UCB0SCL << 10) | 0x32)
 
#define I2CSLAVEMSP432_P3_2_UCB2SDA   ((PMAP_UCB2SDA << 10) | 0x32)
 
#define I2CSLAVEMSP432_P3_2_UCB2SCL   ((PMAP_UCB2SCL << 10) | 0x32)
 
#define I2CSLAVEMSP432_P3_3_UCB0SDA   ((PMAP_UCB0SDA << 10) | 0x33)
 
#define I2CSLAVEMSP432_P3_3_UCB0SCL   ((PMAP_UCB0SCL << 10) | 0x33)
 
#define I2CSLAVEMSP432_P3_3_UCB2SDA   ((PMAP_UCB2SDA << 10) | 0x33)
 
#define I2CSLAVEMSP432_P3_3_UCB2SCL   ((PMAP_UCB2SCL << 10) | 0x33)
 
#define I2CSLAVEMSP432_P3_4_UCB0SDA   ((PMAP_UCB0SDA << 10) | 0x34)
 
#define I2CSLAVEMSP432_P3_4_UCB0SCL   ((PMAP_UCB0SCL << 10) | 0x34)
 
#define I2CSLAVEMSP432_P3_4_UCB2SDA   ((PMAP_UCB2SDA << 10) | 0x34)
 
#define I2CSLAVEMSP432_P3_4_UCB2SCL   ((PMAP_UCB2SCL << 10) | 0x34)
 
#define I2CSLAVEMSP432_P3_5_UCB0SDA   ((PMAP_UCB0SDA << 10) | 0x35)
 
#define I2CSLAVEMSP432_P3_5_UCB0SCL   ((PMAP_UCB0SCL << 10) | 0x35)
 
#define I2CSLAVEMSP432_P3_5_UCB2SDA   ((PMAP_UCB2SDA << 10) | 0x35)
 
#define I2CSLAVEMSP432_P3_5_UCB2SCL   ((PMAP_UCB2SCL << 10) | 0x35)
 
#define I2CSLAVEMSP432_P3_6_UCB0SDA   ((PMAP_UCB0SDA << 10) | 0x36)
 
#define I2CSLAVEMSP432_P3_6_UCB0SCL   ((PMAP_UCB0SCL << 10) | 0x36)
 
#define I2CSLAVEMSP432_P3_6_UCB2SDA   ((PMAP_UCB2SDA << 10) | 0x36)
 
#define I2CSLAVEMSP432_P3_6_UCB2SCL   ((PMAP_UCB2SCL << 10) | 0x36)
 
#define I2CSLAVEMSP432_P3_7_UCB0SDA   ((PMAP_UCB0SDA << 10) | 0x37)
 
#define I2CSLAVEMSP432_P3_7_UCB0SCL   ((PMAP_UCB0SCL << 10) | 0x37)
 
#define I2CSLAVEMSP432_P3_7_UCB2SDA   ((PMAP_UCB2SDA << 10) | 0x37)
 
#define I2CSLAVEMSP432_P3_7_UCB2SCL   ((PMAP_UCB2SCL << 10) | 0x37)
 
#define I2CSLAVEMSP432_P6_4_UCB1SDA   0x00000164 /* Primary, port 6, pin 4 */
 
#define I2CSLAVEMSP432_P6_5_UCB1SCL   0x00000165 /* Primary, port 6, pin 5 */
 
#define I2CSLAVEMSP432_P6_6_UCB3SDA   0x00000266 /* Secondary, port 6, pin 6 */
 
#define I2CSLAVEMSP432_P6_7_UCB3SCL   0x00000267 /* Secondary, port 6, pin 7 */
 
#define I2CSLAVEMSP432_P7_0_UCB0SDA   ((PMAP_UCB0SDA << 10) | 0x70)
 
#define I2CSLAVEMSP432_P7_0_UCB0SCL   ((PMAP_UCB0SCL << 10) | 0x70)
 
#define I2CSLAVEMSP432_P7_0_UCB2SDA   ((PMAP_UCB2SDA << 10) | 0x70)
 
#define I2CSLAVEMSP432_P7_0_UCB2SCL   ((PMAP_UCB2SCL << 10) | 0x70)
 
#define I2CSLAVEMSP432_P7_1_UCB0SDA   ((PMAP_UCB0SDA << 10) | 0x71)
 
#define I2CSLAVEMSP432_P7_1_UCB0SCL   ((PMAP_UCB0SCL << 10) | 0x71)
 
#define I2CSLAVEMSP432_P7_1_UCB2SDA   ((PMAP_UCB2SDA << 10) | 0x71)
 
#define I2CSLAVEMSP432_P7_1_UCB2SCL   ((PMAP_UCB2SCL << 10) | 0x71)
 
#define I2CSLAVEMSP432_P7_2_UCB0SDA   ((PMAP_UCB0SDA << 10) | 0x72)
 
#define I2CSLAVEMSP432_P7_2_UCB0SCL   ((PMAP_UCB0SCL << 10) | 0x72)
 
#define I2CSLAVEMSP432_P7_2_UCB2SDA   ((PMAP_UCB2SDA << 10) | 0x72)
 
#define I2CSLAVEMSP432_P7_2_UCB2SCL   ((PMAP_UCB2SCL << 10) | 0x72)
 
#define I2CSLAVEMSP432_P7_3_UCB0SDA   ((PMAP_UCB0SDA << 10) | 0x73)
 
#define I2CSLAVEMSP432_P7_3_UCB0SCL   ((PMAP_UCB0SCL << 10) | 0x73)
 
#define I2CSLAVEMSP432_P7_3_UCB2SDA   ((PMAP_UCB2SDA << 10) | 0x73)
 
#define I2CSLAVEMSP432_P7_3_UCB2SCL   ((PMAP_UCB2SCL << 10) | 0x73)
 
#define I2CSLAVEMSP432_P7_4_UCB0SDA   ((PMAP_UCB0SDA << 10) | 0x74)
 
#define I2CSLAVEMSP432_P7_4_UCB0SCL   ((PMAP_UCB0SCL << 10) | 0x74)
 
#define I2CSLAVEMSP432_P7_4_UCB2SDA   ((PMAP_UCB2SDA << 10) | 0x74)
 
#define I2CSLAVEMSP432_P7_4_UCB2SCL   ((PMAP_UCB2SCL << 10) | 0x74)
 
#define I2CSLAVEMSP432_P7_5_UCB0SDA   ((PMAP_UCB0SDA << 10) | 0x75)
 
#define I2CSLAVEMSP432_P7_5_UCB0SCL   ((PMAP_UCB0SCL << 10) | 0x75)
 
#define I2CSLAVEMSP432_P7_5_UCB2SDA   ((PMAP_UCB2SDA << 10) | 0x75)
 
#define I2CSLAVEMSP432_P7_5_UCB2SCL   ((PMAP_UCB2SCL << 10) | 0x75)
 
#define I2CSLAVEMSP432_P7_6_UCB0SDA   ((PMAP_UCB0SDA << 10) | 0x76)
 
#define I2CSLAVEMSP432_P7_6_UCB0SCL   ((PMAP_UCB0SCL << 10) | 0x76)
 
#define I2CSLAVEMSP432_P7_6_UCB2SDA   ((PMAP_UCB2SDA << 10) | 0x76)
 
#define I2CSLAVEMSP432_P7_6_UCB2SCL   ((PMAP_UCB2SCL << 10) | 0x76)
 
#define I2CSLAVEMSP432_P7_7_UCB0SDA   ((PMAP_UCB0SDA << 10) | 0x77)
 
#define I2CSLAVEMSP432_P7_7_UCB0SCL   ((PMAP_UCB0SCL << 10) | 0x77)
 
#define I2CSLAVEMSP432_P7_7_UCB2SDA   ((PMAP_UCB2SDA << 10) | 0x77)
 
#define I2CSLAVEMSP432_P7_7_UCB2SCL   ((PMAP_UCB2SCL << 10) | 0x77)
 
#define I2CSLAVEMSP432_P10_2_UCB3SDA   0x000001A2 /* Primary, port 10, pin 2 */
 
#define I2CSLAVEMSP432_P10_3_UCB3SCL   0x000001A3 /* Primary, port 10, pin 3 */
 

Typedefs

typedef struct I2CSlaveMSP432_HWAttrs I2CSlaveMSP432_HWAttrs
 I2CSlaveMSP432 Hardware attributes These fields are used by driverlib APIs and therefore must be populated by driverlib macro definitions. For MSP432 driverlib these definitions are found in: More...
 
typedef struct I2CSlaveMSP432_Object I2CSlaveMSP432_Object
 I2CSlaveMSP432 Object. More...
 

Variables

const I2CSlave_FxnTable I2CSlaveMSP432_fxnTable
 

Macro Definition Documentation

§ I2CSLAVEMSP432_P1_6_UCB0SDA

#define I2CSLAVEMSP432_P1_6_UCB0SDA   0x00000116 /* Primary, port 1, pin 6 */

§ I2CSLAVEMSP432_P1_7_UCB0SCL

#define I2CSLAVEMSP432_P1_7_UCB0SCL   0x00000117 /* Primary, port 1, pin 7 */

§ I2CSLAVEMSP432_P2_0_UCB0SDA

#define I2CSLAVEMSP432_P2_0_UCB0SDA   ((PMAP_UCB0SDA << 10) | 0x20)

§ I2CSLAVEMSP432_P2_0_UCB0SCL

#define I2CSLAVEMSP432_P2_0_UCB0SCL   ((PMAP_UCB0SCL << 10) | 0x20)

§ I2CSLAVEMSP432_P2_0_UCB2SDA

#define I2CSLAVEMSP432_P2_0_UCB2SDA   ((PMAP_UCB2SDA << 10) | 0x20)

§ I2CSLAVEMSP432_P2_0_UCB2SCL

#define I2CSLAVEMSP432_P2_0_UCB2SCL   ((PMAP_UCB2SCL << 10) | 0x20)

§ I2CSLAVEMSP432_P2_1_UCB0SDA

#define I2CSLAVEMSP432_P2_1_UCB0SDA   ((PMAP_UCB0SDA << 10) | 0x21)

§ I2CSLAVEMSP432_P2_1_UCB0SCL

#define I2CSLAVEMSP432_P2_1_UCB0SCL   ((PMAP_UCB0SCL << 10) | 0x21)

§ I2CSLAVEMSP432_P2_1_UCB2SDA

#define I2CSLAVEMSP432_P2_1_UCB2SDA   ((PMAP_UCB2SDA << 10) | 0x21)

§ I2CSLAVEMSP432_P2_1_UCB2SCL

#define I2CSLAVEMSP432_P2_1_UCB2SCL   ((PMAP_UCB2SCL << 10) | 0x21)

§ I2CSLAVEMSP432_P2_2_UCB0SDA

#define I2CSLAVEMSP432_P2_2_UCB0SDA   ((PMAP_UCB0SDA << 10) | 0x22)

§ I2CSLAVEMSP432_P2_2_UCB0SCL

#define I2CSLAVEMSP432_P2_2_UCB0SCL   ((PMAP_UCB0SCL << 10) | 0x22)

§ I2CSLAVEMSP432_P2_2_UCB2SDA

#define I2CSLAVEMSP432_P2_2_UCB2SDA   ((PMAP_UCB2SDA << 10) | 0x22)

§ I2CSLAVEMSP432_P2_2_UCB2SCL

#define I2CSLAVEMSP432_P2_2_UCB2SCL   ((PMAP_UCB2SCL << 10) | 0x22)

§ I2CSLAVEMSP432_P2_3_UCB0SDA

#define I2CSLAVEMSP432_P2_3_UCB0SDA   ((PMAP_UCB0SDA << 10) | 0x23)

§ I2CSLAVEMSP432_P2_3_UCB0SCL

#define I2CSLAVEMSP432_P2_3_UCB0SCL   ((PMAP_UCB0SCL << 10) | 0x23)

§ I2CSLAVEMSP432_P2_3_UCB2SDA

#define I2CSLAVEMSP432_P2_3_UCB2SDA   ((PMAP_UCB2SDA << 10) | 0x23)

§ I2CSLAVEMSP432_P2_3_UCB2SCL

#define I2CSLAVEMSP432_P2_3_UCB2SCL   ((PMAP_UCB2SCL << 10) | 0x23)

§ I2CSLAVEMSP432_P2_4_UCB0SDA

#define I2CSLAVEMSP432_P2_4_UCB0SDA   ((PMAP_UCB0SDA << 10) | 0x24)

§ I2CSLAVEMSP432_P2_4_UCB0SCL

#define I2CSLAVEMSP432_P2_4_UCB0SCL   ((PMAP_UCB0SCL << 10) | 0x24)

§ I2CSLAVEMSP432_P2_4_UCB2SDA

#define I2CSLAVEMSP432_P2_4_UCB2SDA   ((PMAP_UCB2SDA << 10) | 0x24)

§ I2CSLAVEMSP432_P2_4_UCB2SCL

#define I2CSLAVEMSP432_P2_4_UCB2SCL   ((PMAP_UCB2SCL << 10) | 0x24)

§ I2CSLAVEMSP432_P2_5_UCB0SDA

#define I2CSLAVEMSP432_P2_5_UCB0SDA   ((PMAP_UCB0SDA << 10) | 0x25)

§ I2CSLAVEMSP432_P2_5_UCB0SCL

#define I2CSLAVEMSP432_P2_5_UCB0SCL   ((PMAP_UCB0SCL << 10) | 0x25)

§ I2CSLAVEMSP432_P2_5_UCB2SDA

#define I2CSLAVEMSP432_P2_5_UCB2SDA   ((PMAP_UCB2SDA << 10) | 0x25)

§ I2CSLAVEMSP432_P2_5_UCB2SCL

#define I2CSLAVEMSP432_P2_5_UCB2SCL   ((PMAP_UCB2SCL << 10) | 0x25)

§ I2CSLAVEMSP432_P2_6_UCB0SDA

#define I2CSLAVEMSP432_P2_6_UCB0SDA   ((PMAP_UCB0SDA << 10) | 0x26)

§ I2CSLAVEMSP432_P2_6_UCB0SCL

#define I2CSLAVEMSP432_P2_6_UCB0SCL   ((PMAP_UCB0SCL << 10) | 0x26)

§ I2CSLAVEMSP432_P2_6_UCB2SDA

#define I2CSLAVEMSP432_P2_6_UCB2SDA   ((PMAP_UCB2SDA << 10) | 0x26)

§ I2CSLAVEMSP432_P2_6_UCB2SCL

#define I2CSLAVEMSP432_P2_6_UCB2SCL   ((PMAP_UCB2SCL << 10) | 0x26)

§ I2CSLAVEMSP432_P2_7_UCB0SDA

#define I2CSLAVEMSP432_P2_7_UCB0SDA   ((PMAP_UCB0SDA << 10) | 0x27)

§ I2CSLAVEMSP432_P2_7_UCB0SCL

#define I2CSLAVEMSP432_P2_7_UCB0SCL   ((PMAP_UCB0SCL << 10) | 0x27)

§ I2CSLAVEMSP432_P2_7_UCB2SDA

#define I2CSLAVEMSP432_P2_7_UCB2SDA   ((PMAP_UCB2SDA << 10) | 0x27)

§ I2CSLAVEMSP432_P2_7_UCB2SCL

#define I2CSLAVEMSP432_P2_7_UCB2SCL   ((PMAP_UCB2SCL << 10) | 0x27)

§ I2CSLAVEMSP432_P3_0_UCB0SDA

#define I2CSLAVEMSP432_P3_0_UCB0SDA   ((PMAP_UCB0SDA << 10) | 0x30)

§ I2CSLAVEMSP432_P3_0_UCB0SCL

#define I2CSLAVEMSP432_P3_0_UCB0SCL   ((PMAP_UCB0SCL << 10) | 0x30)

§ I2CSLAVEMSP432_P3_0_UCB2SDA

#define I2CSLAVEMSP432_P3_0_UCB2SDA   ((PMAP_UCB2SDA << 10) | 0x30)

§ I2CSLAVEMSP432_P3_0_UCB2SCL

#define I2CSLAVEMSP432_P3_0_UCB2SCL   ((PMAP_UCB2SCL << 10) | 0x30)

§ I2CSLAVEMSP432_P3_1_UCB0SDA

#define I2CSLAVEMSP432_P3_1_UCB0SDA   ((PMAP_UCB0SDA << 10) | 0x31)

§ I2CSLAVEMSP432_P3_1_UCB0SCL

#define I2CSLAVEMSP432_P3_1_UCB0SCL   ((PMAP_UCB0SCL << 10) | 0x31)

§ I2CSLAVEMSP432_P3_1_UCB2SDA

#define I2CSLAVEMSP432_P3_1_UCB2SDA   ((PMAP_UCB2SDA << 10) | 0x31)

§ I2CSLAVEMSP432_P3_1_UCB2SCL

#define I2CSLAVEMSP432_P3_1_UCB2SCL   ((PMAP_UCB2SCL << 10) | 0x31)

§ I2CSLAVEMSP432_P3_2_UCB0SDA

#define I2CSLAVEMSP432_P3_2_UCB0SDA   ((PMAP_UCB0SDA << 10) | 0x32)

§ I2CSLAVEMSP432_P3_2_UCB0SCL

#define I2CSLAVEMSP432_P3_2_UCB0SCL   ((PMAP_UCB0SCL << 10) | 0x32)

§ I2CSLAVEMSP432_P3_2_UCB2SDA

#define I2CSLAVEMSP432_P3_2_UCB2SDA   ((PMAP_UCB2SDA << 10) | 0x32)

§ I2CSLAVEMSP432_P3_2_UCB2SCL

#define I2CSLAVEMSP432_P3_2_UCB2SCL   ((PMAP_UCB2SCL << 10) | 0x32)

§ I2CSLAVEMSP432_P3_3_UCB0SDA

#define I2CSLAVEMSP432_P3_3_UCB0SDA   ((PMAP_UCB0SDA << 10) | 0x33)

§ I2CSLAVEMSP432_P3_3_UCB0SCL

#define I2CSLAVEMSP432_P3_3_UCB0SCL   ((PMAP_UCB0SCL << 10) | 0x33)

§ I2CSLAVEMSP432_P3_3_UCB2SDA

#define I2CSLAVEMSP432_P3_3_UCB2SDA   ((PMAP_UCB2SDA << 10) | 0x33)

§ I2CSLAVEMSP432_P3_3_UCB2SCL

#define I2CSLAVEMSP432_P3_3_UCB2SCL   ((PMAP_UCB2SCL << 10) | 0x33)

§ I2CSLAVEMSP432_P3_4_UCB0SDA

#define I2CSLAVEMSP432_P3_4_UCB0SDA   ((PMAP_UCB0SDA << 10) | 0x34)

§ I2CSLAVEMSP432_P3_4_UCB0SCL

#define I2CSLAVEMSP432_P3_4_UCB0SCL   ((PMAP_UCB0SCL << 10) | 0x34)

§ I2CSLAVEMSP432_P3_4_UCB2SDA

#define I2CSLAVEMSP432_P3_4_UCB2SDA   ((PMAP_UCB2SDA << 10) | 0x34)

§ I2CSLAVEMSP432_P3_4_UCB2SCL

#define I2CSLAVEMSP432_P3_4_UCB2SCL   ((PMAP_UCB2SCL << 10) | 0x34)

§ I2CSLAVEMSP432_P3_5_UCB0SDA

#define I2CSLAVEMSP432_P3_5_UCB0SDA   ((PMAP_UCB0SDA << 10) | 0x35)

§ I2CSLAVEMSP432_P3_5_UCB0SCL

#define I2CSLAVEMSP432_P3_5_UCB0SCL   ((PMAP_UCB0SCL << 10) | 0x35)

§ I2CSLAVEMSP432_P3_5_UCB2SDA

#define I2CSLAVEMSP432_P3_5_UCB2SDA   ((PMAP_UCB2SDA << 10) | 0x35)

§ I2CSLAVEMSP432_P3_5_UCB2SCL

#define I2CSLAVEMSP432_P3_5_UCB2SCL   ((PMAP_UCB2SCL << 10) | 0x35)

§ I2CSLAVEMSP432_P3_6_UCB0SDA

#define I2CSLAVEMSP432_P3_6_UCB0SDA   ((PMAP_UCB0SDA << 10) | 0x36)

§ I2CSLAVEMSP432_P3_6_UCB0SCL

#define I2CSLAVEMSP432_P3_6_UCB0SCL   ((PMAP_UCB0SCL << 10) | 0x36)

§ I2CSLAVEMSP432_P3_6_UCB2SDA

#define I2CSLAVEMSP432_P3_6_UCB2SDA   ((PMAP_UCB2SDA << 10) | 0x36)

§ I2CSLAVEMSP432_P3_6_UCB2SCL

#define I2CSLAVEMSP432_P3_6_UCB2SCL   ((PMAP_UCB2SCL << 10) | 0x36)

§ I2CSLAVEMSP432_P3_7_UCB0SDA

#define I2CSLAVEMSP432_P3_7_UCB0SDA   ((PMAP_UCB0SDA << 10) | 0x37)

§ I2CSLAVEMSP432_P3_7_UCB0SCL

#define I2CSLAVEMSP432_P3_7_UCB0SCL   ((PMAP_UCB0SCL << 10) | 0x37)

§ I2CSLAVEMSP432_P3_7_UCB2SDA

#define I2CSLAVEMSP432_P3_7_UCB2SDA   ((PMAP_UCB2SDA << 10) | 0x37)

§ I2CSLAVEMSP432_P3_7_UCB2SCL

#define I2CSLAVEMSP432_P3_7_UCB2SCL   ((PMAP_UCB2SCL << 10) | 0x37)

§ I2CSLAVEMSP432_P6_4_UCB1SDA

#define I2CSLAVEMSP432_P6_4_UCB1SDA   0x00000164 /* Primary, port 6, pin 4 */

§ I2CSLAVEMSP432_P6_5_UCB1SCL

#define I2CSLAVEMSP432_P6_5_UCB1SCL   0x00000165 /* Primary, port 6, pin 5 */

§ I2CSLAVEMSP432_P6_6_UCB3SDA

#define I2CSLAVEMSP432_P6_6_UCB3SDA   0x00000266 /* Secondary, port 6, pin 6 */

§ I2CSLAVEMSP432_P6_7_UCB3SCL

#define I2CSLAVEMSP432_P6_7_UCB3SCL   0x00000267 /* Secondary, port 6, pin 7 */

§ I2CSLAVEMSP432_P7_0_UCB0SDA

#define I2CSLAVEMSP432_P7_0_UCB0SDA   ((PMAP_UCB0SDA << 10) | 0x70)

§ I2CSLAVEMSP432_P7_0_UCB0SCL

#define I2CSLAVEMSP432_P7_0_UCB0SCL   ((PMAP_UCB0SCL << 10) | 0x70)

§ I2CSLAVEMSP432_P7_0_UCB2SDA

#define I2CSLAVEMSP432_P7_0_UCB2SDA   ((PMAP_UCB2SDA << 10) | 0x70)

§ I2CSLAVEMSP432_P7_0_UCB2SCL

#define I2CSLAVEMSP432_P7_0_UCB2SCL   ((PMAP_UCB2SCL << 10) | 0x70)

§ I2CSLAVEMSP432_P7_1_UCB0SDA

#define I2CSLAVEMSP432_P7_1_UCB0SDA   ((PMAP_UCB0SDA << 10) | 0x71)

§ I2CSLAVEMSP432_P7_1_UCB0SCL

#define I2CSLAVEMSP432_P7_1_UCB0SCL   ((PMAP_UCB0SCL << 10) | 0x71)

§ I2CSLAVEMSP432_P7_1_UCB2SDA

#define I2CSLAVEMSP432_P7_1_UCB2SDA   ((PMAP_UCB2SDA << 10) | 0x71)

§ I2CSLAVEMSP432_P7_1_UCB2SCL

#define I2CSLAVEMSP432_P7_1_UCB2SCL   ((PMAP_UCB2SCL << 10) | 0x71)

§ I2CSLAVEMSP432_P7_2_UCB0SDA

#define I2CSLAVEMSP432_P7_2_UCB0SDA   ((PMAP_UCB0SDA << 10) | 0x72)

§ I2CSLAVEMSP432_P7_2_UCB0SCL

#define I2CSLAVEMSP432_P7_2_UCB0SCL   ((PMAP_UCB0SCL << 10) | 0x72)

§ I2CSLAVEMSP432_P7_2_UCB2SDA

#define I2CSLAVEMSP432_P7_2_UCB2SDA   ((PMAP_UCB2SDA << 10) | 0x72)

§ I2CSLAVEMSP432_P7_2_UCB2SCL

#define I2CSLAVEMSP432_P7_2_UCB2SCL   ((PMAP_UCB2SCL << 10) | 0x72)

§ I2CSLAVEMSP432_P7_3_UCB0SDA

#define I2CSLAVEMSP432_P7_3_UCB0SDA   ((PMAP_UCB0SDA << 10) | 0x73)

§ I2CSLAVEMSP432_P7_3_UCB0SCL

#define I2CSLAVEMSP432_P7_3_UCB0SCL   ((PMAP_UCB0SCL << 10) | 0x73)

§ I2CSLAVEMSP432_P7_3_UCB2SDA

#define I2CSLAVEMSP432_P7_3_UCB2SDA   ((PMAP_UCB2SDA << 10) | 0x73)

§ I2CSLAVEMSP432_P7_3_UCB2SCL

#define I2CSLAVEMSP432_P7_3_UCB2SCL   ((PMAP_UCB2SCL << 10) | 0x73)

§ I2CSLAVEMSP432_P7_4_UCB0SDA

#define I2CSLAVEMSP432_P7_4_UCB0SDA   ((PMAP_UCB0SDA << 10) | 0x74)

§ I2CSLAVEMSP432_P7_4_UCB0SCL

#define I2CSLAVEMSP432_P7_4_UCB0SCL   ((PMAP_UCB0SCL << 10) | 0x74)

§ I2CSLAVEMSP432_P7_4_UCB2SDA

#define I2CSLAVEMSP432_P7_4_UCB2SDA   ((PMAP_UCB2SDA << 10) | 0x74)

§ I2CSLAVEMSP432_P7_4_UCB2SCL

#define I2CSLAVEMSP432_P7_4_UCB2SCL   ((PMAP_UCB2SCL << 10) | 0x74)

§ I2CSLAVEMSP432_P7_5_UCB0SDA

#define I2CSLAVEMSP432_P7_5_UCB0SDA   ((PMAP_UCB0SDA << 10) | 0x75)

§ I2CSLAVEMSP432_P7_5_UCB0SCL

#define I2CSLAVEMSP432_P7_5_UCB0SCL   ((PMAP_UCB0SCL << 10) | 0x75)

§ I2CSLAVEMSP432_P7_5_UCB2SDA

#define I2CSLAVEMSP432_P7_5_UCB2SDA   ((PMAP_UCB2SDA << 10) | 0x75)

§ I2CSLAVEMSP432_P7_5_UCB2SCL

#define I2CSLAVEMSP432_P7_5_UCB2SCL   ((PMAP_UCB2SCL << 10) | 0x75)

§ I2CSLAVEMSP432_P7_6_UCB0SDA

#define I2CSLAVEMSP432_P7_6_UCB0SDA   ((PMAP_UCB0SDA << 10) | 0x76)

§ I2CSLAVEMSP432_P7_6_UCB0SCL

#define I2CSLAVEMSP432_P7_6_UCB0SCL   ((PMAP_UCB0SCL << 10) | 0x76)

§ I2CSLAVEMSP432_P7_6_UCB2SDA

#define I2CSLAVEMSP432_P7_6_UCB2SDA   ((PMAP_UCB2SDA << 10) | 0x76)

§ I2CSLAVEMSP432_P7_6_UCB2SCL

#define I2CSLAVEMSP432_P7_6_UCB2SCL   ((PMAP_UCB2SCL << 10) | 0x76)

§ I2CSLAVEMSP432_P7_7_UCB0SDA

#define I2CSLAVEMSP432_P7_7_UCB0SDA   ((PMAP_UCB0SDA << 10) | 0x77)

§ I2CSLAVEMSP432_P7_7_UCB0SCL

#define I2CSLAVEMSP432_P7_7_UCB0SCL   ((PMAP_UCB0SCL << 10) | 0x77)

§ I2CSLAVEMSP432_P7_7_UCB2SDA

#define I2CSLAVEMSP432_P7_7_UCB2SDA   ((PMAP_UCB2SDA << 10) | 0x77)

§ I2CSLAVEMSP432_P7_7_UCB2SCL

#define I2CSLAVEMSP432_P7_7_UCB2SCL   ((PMAP_UCB2SCL << 10) | 0x77)

§ I2CSLAVEMSP432_P10_2_UCB3SDA

#define I2CSLAVEMSP432_P10_2_UCB3SDA   0x000001A2 /* Primary, port 10, pin 2 */

§ I2CSLAVEMSP432_P10_3_UCB3SCL

#define I2CSLAVEMSP432_P10_3_UCB3SCL   0x000001A3 /* Primary, port 10, pin 3 */

Typedef Documentation

§ I2CSlaveMSP432_HWAttrs

I2CSlaveMSP432 Hardware attributes These fields are used by driverlib APIs and therefore must be populated by driverlib macro definitions. For MSP432 driverlib these definitions are found in:

A sample structure is shown below:

const I2CSlaveMSP432_HWAttrs i2cslaveMSP432HWAttrs[] = {
{
.baseAddr = EUSCI_B0_BASE,
.intNum = INT_EUSCIB0,
.intPriority = ~0,
.slaveAddress = 0x48
}
};

§ I2CSlaveMSP432_Object

I2CSlaveMSP432 Object.

The application must not access any member variables of this structure!

Variable Documentation

§ I2CSlaveMSP432_fxnTable

const I2CSlave_FxnTable I2CSlaveMSP432_fxnTable
© Copyright 1995-2018, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale