Non-Volatile Storage driver implementation for SPI flash peripherals.
The NVSSPI25X module allows you to manage SPI flash memory. This driver works with most 256 byte/page SPI flash memory devices such as:
Winbond W25xx family Macronics MX25Rxx family Micron N25Qxx family
The SPI flash commands used by this driver are as follows:
It is assumed that the SPI flash device used by this driver supports the byte programmability of the SPIFLASH_PAGE_WRITE command and that write page size is 256 bytes. The erase sector and subsector sizes are assumed to be 64K and 4K respectively.
The NVS_erase() command will issue a sector or subsector erase command based on the input size and offset.
The driver must query the SPI flash to ensure that the part is ready before commands are issued. If the part responds as busy, the poll function sleeps for a number of microseconds determined by the NVSSPI25X_HWAttrs.statusPollDelayUs field. A value of 0 means that the driver will continuously poll the external flash until it is ready, which may affect other threads ability to execute.
For each managed flash region, a corresponding SPI instance must be provided to the NVSSPI25X driver.
The SPI instance can be opened and closed internally by the NVSSPI25X driver, or alternatively, a SPI handle can be provided to the NVSSPI25X driver, indicating that the SPI instance is being opened and closed elsewhere within the application. This mode is useful when the SPI bus is share by more than just the SPI flash device.
If the SPI instance is to be managed internally by the NVSSPI25X driver, a SPI instance index and bit rate must be configured in the region's HWAttrs. If the same SPI instance is referenced by multiple flash regions the driver will ensure that SPI_open() is invoked only once, and that SPI_close() will only be invoked when all flash regions using the SPI instance have been closed.
If the SPI bus that the SPI flash device is on is shared with other devices accessed by an application, then the SPI handle used to manage a SPI flash region can be provided in the region's HWAttrs "spiHandle" field. Keep in mind that the "spiHandle" field is a POINTER to a SPI Handle, NOT a SPI Handle. This allows the user to simply initialize this field with the name of the global variable used for the SPI handle. In this mode, the user MUST open the SPI instance prior to opening the NVS region instance so that the referenced spiHandle is valid.
By default, the "spiHandle" field is set to NULL, indicating that the user expects the NVS driver to open and close the SPI instance internally using the 'spiIndex' and 'spiBitRate' provided in the HWAttrs.
By default, the NVSSPI25X driver will assert and de-assert a GPIO driver managed pin to select the SPI flash device before and after each SPI transfer to and from the device.
To enable this behavior, a valid GPIO driver instance index must be provided in the NVS region's spiCsnGpioIndex field of the NVSSPI25X_HWAttrs structure. The corresponding GPIO pin will be configured at runtime by the NVSSPI25X driver as "GPIO_CFG_OUT_STD" and assertion of this pin is assumed to be active LOW.
Some SPI peripherals can be configured to manage their own chip select. Setting the spiCsnGpioIndex field of the NVSSPI25X_HWAttrs structure to NVSSPI25X_SPI_MANAGES_CS informs the NVSSPI25X driver that the SPI peripheral used by the NVS driver has been configured that way.
Alternatively, the user can manage the assertion and de-assertion of the SPI flash chip select entirely themselves by providing implementations of the following 4 APIs in their application code:
Go to the source code of this file.
Data Structures | |
struct | NVSSPI25X_HWAttrs |
NVSSPI25X attributes. More... | |
struct | NVSSPI25X_Object |
Macros | |
#define | NVSSPI25X_CMD_MASS_ERASE (NVS_CMD_RESERVED + 0) |
Command to perform mass erase of entire flash. More... | |
#define | NVSSPI25X_SPI_MANAGES_CS ((uint16_t)(~0)) |
Disable internal management of SPI chip select. More... | |
Typedefs | |
typedef struct NVSSPI25X_HWAttrs | NVSSPI25X_HWAttrs |
NVSSPI25X attributes. More... | |
typedef struct NVSSPI25X_Object | NVSSPI25X_Object |
Variables | |
const NVS_FxnTable | NVSSPI25X_fxnTable |
#define NVSSPI25X_CMD_MASS_ERASE (NVS_CMD_RESERVED + 0) |
Command to perform mass erase of entire flash.
As this command can erase flash memory outside the region associated with the NVS_Handle passed to the control command, the user must carefully orchestrate the use of the command.
Mass Erase is the only control command supported.
#define NVSSPI25X_SPI_MANAGES_CS ((uint16_t)(~0)) |
Disable internal management of SPI chip select.
Some SPI peripherals can be configured to manage their own chip select. Setting the spiCsnGpioIndex field of the NVSSPI25X_HWAttrs structure to NVSSPI25X_SPI_MANAGES_CS informs the NVSSPI25X driver that the SPI peripheral used by the NVS driver is configured to manage its own chip select signal.
typedef struct NVSSPI25X_HWAttrs NVSSPI25X_HWAttrs |
NVSSPI25X attributes.
The 'regionBaseOffset' is the offset, in bytes, from the base of the SPI flash, of the flash region to be managed.
The 'regionSize' must be an integer multiple of the flash sector size.
The 'sectorSize' is SPI flash device specific. This parameter should correspond to the number of bytes erased when the 'SPIFLASH_SUBSECTOR_ERASE' (0x20) command is issued to the device.
The 'verifyBuf' and 'verifyBufSize' parameters are used by the NVS_write() command when either 'NVS_WRITE_PRE_VERIFY' or 'NVS_WRITE_POST_VERIFY' functions are requested in the 'flags' argument. The 'verifyBuf' is used to successively read back portions of the flash to compare with the data being written to it.
typedef struct NVSSPI25X_Object NVSSPI25X_Object |
const NVS_FxnTable NVSSPI25X_fxnTable |