Modules | Macros
ADC_control command and status codes
Collaboration diagram for ADC_control command and status codes:

Modules

 Command Codes
 

Macros

#define ADC_CMD_RESERVED   (32)
 
#define ADC_STATUS_RESERVED   (-32)
 
#define ADC_STATUS_SUCCESS   (0)
 Successful status code returned by ADC_control(). More...
 
#define ADC_STATUS_ERROR   (-1)
 Generic error status code returned by ADC_control(). More...
 
#define ADC_STATUS_UNDEFINEDCMD   (-2)
 An error status code returned by ADC_control() for undefined command codes. More...
 

Detailed Description

These ADC macros are reservations for ADC.h

Macro Definition Documentation

§ ADC_CMD_RESERVED

#define ADC_CMD_RESERVED   (32)

Common ADC_control command code reservation offset. ADC driver implementations should offset command codes with ADC_CMD_RESERVED growing positively

Example implementation specific command codes:

#define ADCXYZ_CMD_COMMAND0 ADC_CMD_RESERVED + 0
#define ADCXYZ_CMD_COMMAND1 ADC_CMD_RESERVED + 1

§ ADC_STATUS_RESERVED

#define ADC_STATUS_RESERVED   (-32)

Common ADC_control status code reservation offset. ADC driver implementations should offset status codes with ADC_STATUS_RESERVED growing negatively.

Example implementation specific status codes:

#define ADCXYZ_STATUS_ERROR0 ADC_STATUS_RESERVED - 0
#define ADCXYZ_STATUS_ERROR1 ADC_STATUS_RESERVED - 1
#define ADCXYZ_STATUS_ERROR2 ADC_STATUS_RESERVED - 2

§ ADC_STATUS_SUCCESS

#define ADC_STATUS_SUCCESS   (0)

Successful status code returned by ADC_control().

ADC_control() returns ADC_STATUS_SUCCESS if the control code was executed successfully.

§ ADC_STATUS_ERROR

#define ADC_STATUS_ERROR   (-1)

Generic error status code returned by ADC_control().

ADC_control() returns ADC_STATUS_ERROR if the control code was not executed successfully.

§ ADC_STATUS_UNDEFINEDCMD

#define ADC_STATUS_UNDEFINEDCMD   (-2)

An error status code returned by ADC_control() for undefined command codes.

ADC_control() returns ADC_STATUS_UNDEFINEDCMD if the control code is not recognized by the driver implementation.

© Copyright 1995-2018, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale