Modules | Macros
SD_control command and status codes
Collaboration diagram for SD_control command and status codes:

Modules

 Status Codes
 
 Command Codes
 

Macros

#define SD_CMD_RESERVED   (32)
 
#define SD_STATUS_RESERVED   (-32)
 

Detailed Description

Macro Definition Documentation

§ SD_CMD_RESERVED

#define SD_CMD_RESERVED   (32)

Common SD_control command code reservation offset. SD driver implementations should offset command codes with SD_CMD_RESERVED growing positively.

Example implementation specific command codes:

#define SDXYZ_CMD_COMMAND0 (SD_CMD_RESERVED + 0)
#define SDXYZ_CMD_COMMAND1 (SD_CMD_RESERVED + 1)

§ SD_STATUS_RESERVED

#define SD_STATUS_RESERVED   (-32)

Common SD_control status code reservation offset. SD driver implementations should offset status codes with SD_STATUS_RESERVED growing negatively.

Example implementation specific status codes:

#define SDXYZ_STATUS_ERROR0 (SD_STATUS_RESERVED - 0)
#define SDXYZ_STATUS_ERROR1 (SD_STATUS_RESERVED - 1)
#define SDXYZ_STATUS_ERROR2 (SD_STATUS_RESERVED - 2)
© Copyright 1995-2018, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale