Data Fields
PWMTimerMSP432_Status Struct Reference

PWMTimerMSP432_Status. More...

#include <PWMTimerMSP432.h>

Collaboration diagram for PWMTimerMSP432_Status:
Collaboration graph
[legend]

Data Fields

Power_NotifyObj perfChangeNotify
 
PWM_Period_Units periodUnits
 
uint32_t perfConstraintMask
 
uint32_t clockSource
 
uint32_t duties [PWMTimerMSP432_NUM_PWM_OUTPUTS]
 
uint32_t periodCounts
 
uint32_t period
 
uint8_t prescalar
 
uint8_t activeOutputsMask
 
uint8_t openMask
 

Detailed Description

PWMTimerMSP432_Status.

The application must not access any member variables of this structure!

Field Documentation

§ perfChangeNotify

Power_NotifyObj PWMTimerMSP432_Status::perfChangeNotify

§ periodUnits

PWM_Period_Units PWMTimerMSP432_Status::periodUnits

§ perfConstraintMask

uint32_t PWMTimerMSP432_Status::perfConstraintMask

§ clockSource

uint32_t PWMTimerMSP432_Status::clockSource

§ duties

uint32_t PWMTimerMSP432_Status::duties[PWMTimerMSP432_NUM_PWM_OUTPUTS]

§ periodCounts

uint32_t PWMTimerMSP432_Status::periodCounts

§ period

uint32_t PWMTimerMSP432_Status::period

§ prescalar

uint8_t PWMTimerMSP432_Status::prescalar

§ activeOutputsMask

uint8_t PWMTimerMSP432_Status::activeOutputsMask

§ openMask

uint8_t PWMTimerMSP432_Status::openMask

The documentation for this struct was generated from the following file:
© Copyright 1995-2018, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale