Data Fields
Timer_FxnTable_ Struct Reference

The definition of a timer function table that contains the required set of functions to control a specific timer driver implementation. More...

#include <Timer.h>

Collaboration diagram for Timer_FxnTable_:
Collaboration graph
[legend]

Data Fields

Timer_CloseFxn closeFxn
 
Timer_ControlFxn controlFxn
 
Timer_GetCountFxn getCountFxn
 
Timer_InitFxn initFxn
 
Timer_OpenFxn openFxn
 
Timer_StartFxn startFxn
 
Timer_StopFxn stopFxn
 

Detailed Description

The definition of a timer function table that contains the required set of functions to control a specific timer driver implementation.

Field Documentation

§ closeFxn

Timer_CloseFxn Timer_FxnTable_::closeFxn

Function to close the specified peripheral.

§ controlFxn

Timer_ControlFxn Timer_FxnTable_::controlFxn

Function to implementation specific control function.

§ getCountFxn

Timer_GetCountFxn Timer_FxnTable_::getCountFxn

Function to get the count of the specified peripheral.

§ initFxn

Timer_InitFxn Timer_FxnTable_::initFxn

Function to initialize the given data object.

§ openFxn

Timer_OpenFxn Timer_FxnTable_::openFxn

Function to open the specified peripheral.

§ startFxn

Timer_StartFxn Timer_FxnTable_::startFxn

Function to start the specified peripheral.

§ stopFxn

Timer_StopFxn Timer_FxnTable_::stopFxn

Function to stop the specified peripheral.


The documentation for this struct was generated from the following file:
© Copyright 1995-2018, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale