Porting From EasyLink 2.40.2 to EasyLink 2.40.3¶
EasyLink 2.40.2 is bundled with the SimpleLink CC13x0 2.30 SDK. EasyLink 2.40.3 is bundled with the SimpleLink CC13x0 2.40 SDK.
For this migration guide, the rfEasyLinkTx project will be ported from EasyLink 2.40.2 to EasyLink 2.40.3. The steps should be transferable for any EasyLink example project.
Attention
SimpleLink CC13x2_26x2 2.40 SDK can only be run on CC13x2 and CC26x2 devices with chip revision E.
Because the directory structure is nearly identical between the two releases, the recommended approach is to start with a EasyLink 2.40.3 project that contains the same base functionality as the porting target project and merge in any custom functionality.
Note
For the SimpleLink CC13x2_26x2 2.40 SDK, the previous CC13x2 and CC26x2 SDKs were merged to one. This does not impact individual example projects, so no migration steps are needed.
Choose a EasyLink 2.40.3 example project that contains your target project’s base functionality.
For this example, we will use rfEasyLinkTx as the starting EasyLink 2.40.3 example project.
Transfer all modified application files from EasyLink 2.40.2 into the EasyLink 2.40.3 example project.
In this example, the following files from EasyLink 2.40.2 were moved into rfEasyLinkTx EasyLink 2.40.3 example:
rfEasyLinkTx.c
smartrf_settings
files
Change Driverlib include paths.
The driverlib include path has changes. Find any file in your project that uses the following path:
#include <ti/devices/cc13x2_cc26x2_v1/
, and update it to#include <ti/devices/cc13x2_cc26x2/
. E.g., if you have a file that includes IOC and UDMA driverlib files, change the include paths to the following.#include <ti/devices/cc13x2_cc26x2/driverlib/ioc.h> #include <ti/devices/cc13x2_cc26x2/driverlib/udma.h> #include <ti/devices/cc13x2_cc26x2/inc/hw_ints.h> #include <ti/devices/cc13x2_cc26x2/inc/hw_memmap.h>
Remove unnecessary patches.
This step is only applicable for CC13x2 devices. Since the CC13x2 chip revision E has an updated version of ROM compared to chip revision C, fewer RF patches are needed. If a patch you are using is not found in the rf_patches folder (
{SDK_INSTALL_DIR}\source\ti\devices\cc13x2_cc26x2\rf_patches
), it is no longer needed and you must delete references to this patch insmartrf_settings
files. (Both the include statements at the beginning of the file, and the assignation of patches in the RF Mode setup.)Adjust to
easylink_config
files.New in EasyLink 2.40.3 are two files,
easylink_config.c
andeasylink_config.h
. These files are used to configure various EasyLink parameters. You can add this file to your project and configure the settings.Note
These files were added as part of SysConfig, which is available on CC13x2 devices. If you are working on a CC13x2 device, you can use SysConfig to configure the following settings. If you want to use SysConfig, please start with an example from the syscfg_preview folder. More information: SysConfig.
The following settings should be configured in
easylink_config.h
:easylink_config.h
DefineDefault Value 2.30 SDK Location/API EASYLINK_API_VERSION “EasyLink-v2.40.03” EasyLink.h
EASYLINK_MAX_DATA_LENGTH 128 EasyLink.h
EASYLINK_ADDR_SIZE 1 EasyLink_Ctrl_AddSize in EasyLink_CtrlOption. EASYLINK_ENABLE_ADDR_FILTERING TRUE EasyLink_enableRxAddrFilter() EASYLINK_NUM_ADDR_FILTER 1 EasyLink_enableRxAddrFilter() EASYLINK_ADDR_FILTER_TABLE {0xAA} EasyLink_enableRxAddrFilter() EASYLINK_IDLE_TIMEOUT 1 ms EasyLink_Ctrl_Idle_TimeOut in EasyLink_CtrlOption. EASYLINK_ENABLE_MULTI_CLIENT FALSE EasyLink_Ctrl_MultiClient_Mode in EasyLink_CtrlOption EASYLINK_ASYNC_RX_TIMEOUT 0 ms EasyLink_Ctrl_AsyncRx_TimeOut in EasyLink_CtrlOption EASYLINK_WHITENING_MODE 2 EasyLink.h
EASYLINK_MIN_CCA_BACKOFF_WINDOW 5 EasyLink.h
EASYLINK_MAX_CCA_BACKOFF_WINDOW 8 EasyLink.h
EASYLINK_CCA_BACKOFF_TIMEUNITS 250 EasyLink.h
EASYLINK_CS_RSSI_THRESHOLD_DBM -80 EasyLink.h
EASYLINK_CHANNEL_IDLE_TIME_US 5000 EasyLink.h
Rename RF Command pointers.
In
easylink_config.c
, the pointers to the RF commands are listed. Rename the RF commands in thesmartrf_settings
files to match the commands ineasylink_config.c
.Define supported PHYs.
Make sure the correct PHY support defines are set. (You can set these in
easylink_config.h
or in the project predefined symbols.) E.g. if you want your project to support the 50 kbps PHY and the 200 kbps PHY, make sure the following defines are set:SUPPORT_PHY_50KBPS2GFSK SUPPORT_PHY_200KBPS2GFSK
Make sure the RF objects for each supported PHY is set in
easylink_config.c
and points to a set of commands in asmartrf_settings
file.