Porting From EasyLink 2.40.3 to EasyLink 2.50.1¶
EasyLink 2.40.3 is bundled with the SimpleLink CC13x0 2.40 SDK. EasyLink 2.50.1 is bundled with the SimpleLink CC13x0 3.10 SDK.
For this migration guide, the rfEasyLinkTx project will be ported from EasyLink 2.40.3 to EasyLink 2.50.1. The steps should be transferable for any EasyLink example project.
Because the directory structure is nearly identical between the two releases, the recommended approach is to start with a EasyLink 2.50.1 project that contains the same base functionality as the porting target project and merge in any custom functionality.
Choose a EasyLink 2.50.1 example project that contains your target project’s base functionality.
For this example, we will use rfEasyLinkTx as the starting EasyLink 2.50.1 example project.
Transfer all modified application files from EasyLink 2.40.3 into the EasyLink 2.50.1 example project.
In this example, the following files from EasyLink 2.40.3 were moved into rfEasyLinkTx EasyLink 2.50.1 example:
rfEasyLinkTx.c
smartrf_settings
files
Configure the default address.
In EasyLink 2.50.1 there are two new parameter in
easylink_config.h
called EASYLINK_USE_DEFAULT_ADDR and EASYLINK_DEFAULT_ADDR. Their usage is documented ineasylink_config.h