![]() |
![]() |
TI BLE-Stack for Bluetooth API Documentation
3.03.00.00
|
Data Structures | |
struct | ugapMonitorCBs_t |
Set of Observer callbacks - must be setup by the application. More... | |
Typedefs | |
typedef void(* | ugapMonitorCompleteCb_t) (bStatus_t status, uint8_t sessionId) |
Callback of when a scan monitoring has just been done. More... | |
typedef void(* | ugapMonitorIndicationCb_t) (bStatus_t status, uint8_t sessionId, uint8_t len, uint8_t *pPayload) |
Callback of when a packet is received. More... | |
typedef void(* | ugapMonitorStateChangeCb_t) (ugapMonitorState_t state) |
Callback of when the Monitor's state changes. More... | |
typedef void(* ugapMonitorCompleteCb_t) (bStatus_t status, uint8_t sessionId) |
Callback of when a scan monitoring has just been done.
status | status of a scan |
sessionId | session ID |
typedef void(* ugapMonitorIndicationCb_t) (bStatus_t status, uint8_t sessionId, uint8_t len, uint8_t *pPayload) |
Callback of when a packet is received.
status | status of a monitoring scan |
sessionId | session ID |
len | length of the payload |
pPayload | pointer to payload |
typedef void(* ugapMonitorStateChangeCb_t) (ugapMonitorState_t state) |
Callback of when the Monitor's state changes.
state | Micro GAP Monitor Structures |