TI BLE5-Stack API Documentation
1.01.09.00
|
Structure definition for image header and segments, these are prepended to the over the air images. More...
Modules | |
OAD Image Header offsets | |
OAD image lengths | |
OAD image types | |
OAD segment op codes | |
OAD wireless technology fields | |
Files | |
file | oad_image_header.h |
Structure definition for image header and segments, these are prepended to the over the air images. | |
Macros | |
#define | BIM_VER 0x3 |
#define | COPY_DONE 0xFC |
#define | CRC_INVALID 0xFC |
#define | CRC_VALID 0xFE |
#define | DEFAULT_CRC 0xFFFFFFFF |
#define | DEFAULT_STATE 0xFF |
#define | EFL_MATADATA_HDR_LEN OAD_IMG_HDR_LEN + 8 |
#define | INVALID_ADDR 0xFFFFFFFF |
#define | INVALID_LEN INVALID_ADDR |
#define | META_VER 0x1 |
#define | NEED_COPY 0xFE |
#define | OAD_EXTFL_ID_VAL {'O', 'A', 'D', ' ', 'N', 'V', 'M', '1'} |
Variables | |
uint8_t | bimVer |
BIM version. | |
boundarySeg_t | |
uint32_t | boundarySegLen |
Boundary segment length. | |
uint32_t | crc32 |
Image's 32-bit CRC value. | |
uint8_t | crcStat |
CRC status. | |
uint16_t | hdrLen |
Total length of the image header. | |
uint8_t | imgCpStat |
Image copy status. | |
uint32_t | imgEndAddr |
Address of the last byte of a contiguous image. | |
imgFixedHdr_t | |
imgHdr_t | |
uint8_t | imgNo |
Image number of 'image type'. | |
imgPayloadSeg_t | imgPayload |
Required contiguous image segment. | |
imgPayloadSeg_t | |
uint32_t | imgSegLen |
Payload segment length. | |
uint8_t | imgType |
Image Type. | |
uint32_t | imgVld |
This field is RFU. | |
uint32_t | len |
Image length in bytes. | |
uint8_t | metaVer |
Metadata version. | |
uint32_t | prgEntry |
Program entry address. | |
uint32_t | ram0EndAddr |
RAM entry end address. | |
uint32_t | ram0StartAddr |
RAM entry start address. | |
uint16_t | rfu |
Reserved bytes. More... | |
uint8_t | softVer [4] |
Software version of the image. | |
uint32_t | stackEntryAddr |
Stack start address. | |
uint32_t | stackStartAddr |
Start address of stack image on internal flash. | |
uint32_t | startAddr |
Start address of image on internal flash. | |
uint16_t | techType |
Wireless protocol type BLE/TI-MAC/ZIGBEE etc. | |
TYPEDEF_STRUCT_PACKED | |
User-defined Image Identification bytes. More... | |
uint16_t | wirelessTech |
Wireless technology type. | |
Structure definition for image header and segments, these are prepended to the over the air images.
============================================================================
The OAD Image header file should be included in an OAD enabled application as follows:
The OAD image header is a combined structure that is intended to be prepdended to a binary image before sending over the air. This file defines the structures that are used to build up an image header. Additionally, this header file can be used by the application to read fields within an image header.
For code examples, see the use cases below.
#define BIM_VER 0x3 |
Version of BIM this image is intended to work with
#define COPY_DONE 0xFC |
FlagimgCpStat indicating the image is already copied
#define CRC_INVALID 0xFC |
Flag for crcStat indicating the CRC of the image is invalid
#define CRC_VALID 0xFE |
Flag for crcStat indicating the CRC of the image is valid
#define DEFAULT_CRC 0xFFFFFFFF |
An invalid address as shown by unprogrammed flash.
#define DEFAULT_STATE 0xFF |
Default state of unprogrammed flash in an image header field
#define EFL_MATADATA_HDR_LEN OAD_IMG_HDR_LEN + 8 |
Length of image external flash image header
#define INVALID_ADDR 0xFFFFFFFF |
An invalid address as shown by unprogrammed flash
#define INVALID_LEN INVALID_ADDR |
An invalid length as shown by unprogrammed flash.
#define META_VER 0x1 |
Version of metadata that defined this image header
#define NEED_COPY 0xFE |
FlagimgCpStat indicating the image should be copied
#define OAD_EXTFL_ID_VAL {'O', 'A', 'D', ' ', 'N', 'V', 'M', '1'} |
Magic number used by entries in the image header table at the beginning of external flash. Note this is different from OAD_IMG_ID_VAL so that the application can determine the difference between an entry in the header table and the start of an OAD image
uint8_t rfu |
Reserved bytes.
Reserved byte.
TYPEDEF_STRUCT_PACKED |
User-defined Image Identification bytes.
Required core image header.
Segment type - for boundary segment.
Segment type - for Contiguous image payload.
OAD Core image header structure definition
OAD continuous image payload segment
This segment is used to describe a contiguous region of an image The code data in this blob will be flashed to sequential addresses
OAD boundary segment
This segment is used to describe the RAM and Flash boundaries in a split image system.
OAD Image Header
This structure represents the complete header to be prepended to an OAD image
It is an amalgamation of the structures defined above, and must contain a core header