![]() |
![]() |
#include "stdbool.h"
#include "stdint.h"
#include "string.h"
Go to the source code of this file.
Data Structures | |
struct | _cplx_int_least8_t |
Define the complex data type for at least 8 bit signed real and imaginary components. More... | |
struct | _cplx_uint_least8_t |
Define the complex data type for at least 8 bit unsigned real and imaginary components. More... | |
struct | _cplx_least16_t |
Define the complex data type for at least 16 bit signed real and imaginary components. More... | |
struct | _cplx_uleast16_t |
Define the complex data type for at least 16 bit unsigned real and imaginary components. More... | |
struct | _cplx_int_least32_t_ |
Define the complex data type for at least 32 bit signed real and imaginary components. More... | |
struct | _cplx_uint_least32_t_ |
Define the complex data type for at least 32 bit unsigned real and imaginary components. More... | |
struct | _cplx_int16_t_ |
Define the complex data type for 16 bit signed real and imaginary components. More... | |
struct | _cplx_uint16_t_ |
Define the complex data type for 16 bit unsigned real and imaginary components. More... | |
struct | _cplx_int32_t |
Define the complex data type for 32 bit signed real and imaginary components. More... | |
struct | _cplx_uint32_t |
Define the complex data type for 32 bit unsigned real and imaginary components. More... | |
struct | _cplx_float_t |
Define the complex data type for float real and imaginary components. More... | |
Macros | |
#define | C2000_IEEE754_TYPES |
#define | HIGH 1 |
Defines high. More... | |
#define | LOW 0 |
Defines low. More... | |
#define | OFF 0 |
Defines off. More... | |
#define | OK 0 |
Defines ok. More... | |
#define | ON 1 |
Defines on. More... | |
#define | ERROR 1 |
Defines generic error. More... | |
#define | PASS 1 |
Defines pass. More... | |
#define | FAIL 0 |
Defines fails. More... | |
Typedefs | |
typedef float | float32_t |
typedef long double | float64_t |
typedef unsigned int | status |
Defines the portable data type for a status result. More... | |
typedef float | float_t |
Defines the portable data type for 32 bit, signed floating-point data. More... | |
typedef double | double_t |
Defines the portable data type for 64 bit, signed floating-point data. More... | |
typedef struct _cplx_int_least8_t | cplx_int_least8_t |
Define the complex data type for at least 8 bit signed real and imaginary components. More... | |
typedef struct _cplx_uint_least8_t | cplx_uint_least8_t |
Define the complex data type for at least 8 bit unsigned real and imaginary components. More... | |
typedef struct _cplx_least16_t | cplx_int_least16_t |
Define the complex data type for at least 16 bit signed real and imaginary components. More... | |
typedef struct _cplx_uleast16_t | cplx_uint_least16_t |
Define the complex data type for at least 16 bit unsigned real and imaginary components. More... | |
typedef struct _cplx_int_least32_t_ | cplx_int_least32_t |
Define the complex data type for at least 32 bit signed real and imaginary components. More... | |
typedef struct _cplx_uint_least32_t_ | cplx_uint_least32_t |
Define the complex data type for at least 32 bit unsigned real and imaginary components. More... | |
typedef struct _cplx_int16_t_ | cplx_int16_t |
Define the complex data type for 16 bit signed real and imaginary components. More... | |
typedef struct _cplx_uint16_t_ | cplx_uint16_t |
Define the complex data type for 16 bit unsigned real and imaginary components. More... | |
typedef struct _cplx_int32_t | cplx_int32_t |
Define the complex data type for 32 bit signed real and imaginary components. More... | |
typedef struct _cplx_uint32_t | cplx_uint32_t |
Define the complex data type for 32 bit unsigned real and imaginary components. More... | |
typedef struct _cplx_float_t | cplx_float_t |
Define the complex data type for float real and imaginary components. More... | |