C_ANGLE_GEN_Obj_ | Defines the angle generator (ANGLE_COMP) object |
C_BLDC_Obj_t_ | |
C_CLARKE_Obj_ | Defines the CLARKE object |
C_cplx_float_t | Define the complex data type for float real and imaginary components |
C_cplx_int16_t_ | Define the complex data type for 16 bit signed real and imaginary components |
C_cplx_int32_t | Define the complex data type for 32 bit signed real and imaginary components |
C_cplx_int_least32_t_ | Define the complex data type for at least 32 bit signed real and imaginary components |
C_cplx_int_least8_t | Define the complex data type for at least 8 bit signed real and imaginary components |
C_cplx_least16_t | Define the complex data type for at least 16 bit signed real and imaginary components |
C_cplx_uint16_t_ | Define the complex data type for 16 bit unsigned real and imaginary components |
C_cplx_uint32_t | Define the complex data type for 32 bit unsigned real and imaginary components |
C_cplx_uint_least32_t_ | Define the complex data type for at least 32 bit unsigned real and imaginary components |
C_cplx_uint_least8_t | Define the complex data type for at least 8 bit unsigned real and imaginary components |
C_cplx_uleast16_t | Define the complex data type for at least 16 bit unsigned real and imaginary components |
C_CPU_TIME_Obj_ | Defines the CPU usage (CPU_TIME) object |
C_CTRL_Obj_ | Defines the controller (CTRL) object |
C_CTRL_Version_ | Defines the controller (CTRL) version number |
C_DAC128S_Obj_ | Object for the DAC128S registers and commands |
C_DATALOG_OBJ_ | Defines the data logging (DATALOG) object |
C_DCLINK_SS_Obj_ | Defines the DC_Link Single-Shunt Object |
C_DRV8316_Obj_ | Defines the DRV8316 object |
C_DRV8316_VARS_t_ | Object for the DRV8316 registers and commands |
C_DRV8323_Obj_ | Defines the DRV8323 object |
C_DRV8323_VARS_t_ | Object for the DRV8323 registers and commands |
C_DRV8353_Obj_ | Defines the DRV8353 object |
C_DRV8353_VARS_t_ | Object for the DRV8353 registers and commands |
C_ENC_Obj_ | Defines the ENC controller object |
C_ESMO_Obj_ | Defines the ESMO controller object |
C_EST_InputData_ | Defines the estimator (EST) input data |
C_EST_OutputData_ | Defines the estimator (EST) output data |
C_EVENT_ArgList_ | Defines the event argument list |
C_EVENT_Obj_ | Defines the event queue object |
C_FCL_Parameters_ | |
C_FCL_Parameters_t_ | Typedefs for motorVars |
C_FCL_Vars_t_ | Typedefs for motorVars Variables for CLA tasks |
C_FILTER_FO_Obj_ | Defines the first-order filter (FILTER_FO) object |
C_FILTER_NOTCH_CoeffObj_ | Defines the notch filter coefficient (FILTER_COEFF) object |
C_FILTER_NOTCH_Obj_ | Defines the notch filter (FILTER_NOTCH) object |
C_FILTER_SO_Obj_ | Defines the second-order filter (FILTER_SO) object |
C_FWC_Obj_ | Defines the Field Weakening Control (FWC) object |
C_GRAPH_Buffer_t_ | |
C_GRAPH_StepVars_t_ | |
C_GRAPH_Vars_t_ | |
C_HALL_Obj_ | Defines the HALL controller object |
C_IPARK_Obj_ | Defines the IPARK object |
C_ISBLDC_Obj_ | |
C_MATH_cplx_vec2_ | Defines a two element vector |
C_MATH_cplx_vec3_ | Defines a three element vector |
C_MATH_ui_Vec2_ | Defines unsigned integer two element vector |
C_MATH_ui_Vec3_ | Defines unsigned integer three element vector |
C_MATH_Vec2_ | Defines a two element vector |
C_MATH_Vec3_ | Defines a three element vector |
C_MOD6CNT_Obj_ | Defines the angle generator (ANGLE_COMP) object |
C_MOTOR_Params_ | Defines the motor parameters |
C_MOTOR_Vars_t_ | Typedefs for motorVars |
C_MTPA_Obj_ | Defines the MTPA object |
C_OFFSET_Obj_ | Defines the offset (OFFSET) object |
C_PARK_Obj_ | Defines the PARK object |
C_PHVOLC_Obj_ | Defines the PHVOLC controller object |
C_PI_Obj_ | Defines the PI controller object |
C_PID_Obj_ | Defines the PID controller object |
C_QUEUE_Obj_ | Defines the queue object structure |
C_RIMPULSE_Obj_ | Defines the ramp control and impulse (RIMPULSE) object |
C_SLIP_Obj_ | Defines the slip object |
C_SPD_OBSERVER_obj_ | |
C_SPDCALC_obj_ | |
C_SPDFR_obj_ | |
C_SSIPD_obj_ | Defines the SSIPD_Obj object |
C_SVGEN2_t_ | |
C_SVGEN_Obj_ | Defines the Space Vector Generator (SVGEN) object |
C_SVGENCURRENT_Obj_ | Defines the Svgen Current object |
C_TRAJ_Obj_ | Defines the trajectory (TRAJ) object |
C_USER_Params_ | Defines a structure for the user parameters |
C_VIB_COMP_Obj_ | Defines the Vibration Compensation object |
C_VOLREC_Obj_ | Defines the VOLREC controller object |
C_VS_FREQ_Obj_ | Defines the angle generator (ANGLE_COMP) object |
C_VSF_Obj_ | Defines the VSF handle |
CCLA_QEP_PTR | |
CDLOG_2CH_F | |
CDLOG_4CH_F | |
CDLOG_6CH_F | |
CDRV8316_CTRL01_BITS | Object for the DRV8316 CTRL01 register |
CDRV8316_CTRL01_REG | |
CDRV8316_CTRL02_BITS | Object for the DRV8316 CTRL03 register |
CDRV8316_CTRL02_REG | |
CDRV8316_CTRL03_BITS | Object for the DRV8316 CTRL03 register |
CDRV8316_CTRL03_REG | |
CDRV8316_CTRL04_BITS | Object for the DRV8316 CTRL04 register |
CDRV8316_CTRL04_REG | |
CDRV8316_CTRL05_BITS | Object for the DRV8316 CTRL05 register |
CDRV8316_CTRL05_REG | |
CDRV8316_CTRL06_BITS | Object for the DRV8316 CTRL06 register |
CDRV8316_CTRL06_REG | |
CDRV8316_CTRL10_BITS | Object for the DRV8316 CTRL10 register |
CDRV8316_CTRL10_REG | |
CDRV8316_STAT00_BITS | Object for the DRV8316 STATUS00 register |
CDRV8316_STAT00_REG | |
CDRV8316_STAT01_BITS | Object for the DRV8316 STATUS01 register |
CDRV8316_STAT01_REG | |
CDRV8316_STAT02_BITS | Object for the DRV8316 STATUS02 register |
CDRV8316_STAT02_REG | |
CDRV8323_CTRL02_BITS | Object for the DRV8323 CTRL02 register |
CDRV8323_CTRL02_REG | |
CDRV8323_CTRL03_BITS | Object for the DRV8323 CTRL03 register |
CDRV8323_CTRL03_REG | |
CDRV8323_CTRL04_BITS | Object for the DRV8323 CTRL04 register |
CDRV8323_CTRL04_REG | |
CDRV8323_CTRL05_BITS | Object for the DRV8323 CTRL05 register |
CDRV8323_CTRL05_REG | |
CDRV8323_CTRL06_BITS | Object for the DRV8323 CTRL05 register |
CDRV8323_CTRL06_REG | |
CDRV8323_STAT00_BITS | Object for the DRV8323 STATUS00 register |
CDRV8323_STAT00_REG | |
CDRV8323_STAT01_BITS | Object for the DRV8323 STATUS01 register |
CDRV8323_STAT01_REG | |
CDRV8353_CTRL02_BITS | Object for the DRV8353 CTRL02 register |
CDRV8353_CTRL02_REG | |
CDRV8353_CTRL03_BITS | Object for the DRV8353 CTRL03 register |
CDRV8353_CTRL03_REG | |
CDRV8353_CTRL04_BITS | Object for the DRV8353 CTRL04 register |
CDRV8353_CTRL04_REG | |
CDRV8353_CTRL05_BITS | Object for the DRV8353 CTRL05 register |
CDRV8353_CTRL05_REG | |
CDRV8353_CTRL06_BITS | Object for the DRV8353 CTRL06 register |
CDRV8353_CTRL06_REG | |
CDRV8353_CTRL07_BITS | Object for the DRV8353 CTRL06 register |
CDRV8353_CTRL07_REG | |
CDRV8353_STAT00_BITS | Object for the DRV8353 STATUS00 register |
CDRV8353_STAT00_REG | |
CDRV8353_STAT01_BITS | Object for the DRV8353 STATUS01 register |
CDRV8353_STAT01_REG | |
CEMAVG | Defines the Exponential Moving Average (EMAVG) structure |
CFCL_cmplxCtrl_t | |
CFCL_PIController_t | |
CmotPars | |
CPM_tformat_DataStruct | [TFORMAT_API_DATA_STRUCT_SNIPPET] |
CPOWER_MEAS_FAST | Defines the POWER_MEAS_SINE_ANALYZER structure |
CPOWER_MEAS_SINE_ANALYZER | Defines the POWER_MEAS_SINE_ANALYZER structure |
CQEP | |
CSFRA_F32 | Defines the SFRA_F32 structure |
CSPLL_1PH_NOTCH | Defines the SPLL_1PH_NOTCH structure |
CSPLL_1PH_NOTCH_COEFF | Defines the SPLL_1PH_NOTCH_COEFF structure |
CSPLL_1PH_NOTCH_LPF_COEFF | Defines the SPLL_1PH_NOTCH_LPF_COEFF structure |
CSPLL_1PH_SOGI | Defines the Orthogonal Signal Generator SPLL_1PH_SOGI structure |
CSPLL_1PH_SOGI_FLL | Defines the Orthogonal Signal Generator SPLL_1PH_SOGI_FLL structure |
CSPLL_1PH_SOGI_FLL_LPF_COEFF | Defines the SPLL_1PH_SOGI_FLL_LPF_COEFF structure |
CSPLL_1PH_SOGI_FLL_OSG_COEFF | Defines the SPLL_1PH_SOGI_FLL_OSG_COEFF structure |
CSPLL_1PH_SOGI_LPF_COEFF | Defines the SPLL_1PH_SOGI_LPF_COEFF structure |
CSPLL_1PH_SOGI_OSG_COEFF | Defines the SPLL_1PH_SOGI_OSG_COEFF structure |
CSPLL_3PH_DDSRF | Defines the SPLL_3PH_DDSRF structure |
CSPLL_3PH_DDSRF_LPF_COEFF | Defines the coefficients for a loop filter |
CSPLL_3PH_SRF | Defines the SPLL_3PH_SRF structure |
CSPLL_3PH_SRF_LPF_COEFF | Defines the coefficients for a loop filter |