3.4. Build KernelΒΆ
During Linux development, the kernel source code might require modification and recompile, for example, in the cases of
- Enabling features which are disabled in the kernel defconfig
- Disabling features which are enabled in the kernel defconfig
- Modifying kernel source code to port kernel to a custom board
Once the Processor SDK Linux package is installed, the kernel source code is
under <SDK_INSTALL_DIR>/board-support/linux-<version>/. Please refer to
Processor SDK Documentation Kernel User Guide
for how to compile the kernel for AM64x.