AM263x MCU+ SDK  08.02.01

Detailed Description

Unregulated traffic (no classifier hit) policing params.

Data Fields

uint32_t peakRateInBitsPerSec
 
uint32_t commitRateInBitsPerSec
 

Field Documentation

◆ peakRateInBitsPerSec

uint32_t CpswAle_UnregulatedTrafficPolicer::peakRateInBitsPerSec

Peak rate in bits per second. 0 indicates rate limit is disabled

◆ commitRateInBitsPerSec

uint32_t CpswAle_UnregulatedTrafficPolicer::commitRateInBitsPerSec

Commit rate in bits per second. 0 indicates rate limit is disabled