AM263x MCU+ SDK  08.02.01
EnetPer_Obj Struct Reference

Detailed Description

Ethernet Peripheral object.

Data Fields

const char * name
 
Enet_Type enetType
 
uint32_t instId
 
Enet_Magic magic
 
uint64_t physAddr
 
void * virtAddr
 
uint64_t physAddr2
 
void * virtAddr2
 
uint32_t features
 
uint32_t errata
 
EnetPer_InitCfg initCfg
 
EnetPer_Open open
 
EnetPer_Rejoin rejoin
 
EnetPer_Ioctl ioctl
 
EnetPer_Poll poll
 
EnetPer_ConvertTs convertTs
 
EnetPer_PeriodicTick periodicTick
 
EnetPer_RegisterEventCb registerEventCb
 
EnetPer_UnregisterEventCb unregisterEventCb
 
EnetPer_Close close
 

Field Documentation

◆ name

const char* EnetPer_Obj::name

Peripheral name

◆ enetType

Enet_Type EnetPer_Obj::enetType

Peripheral type

◆ instId

uint32_t EnetPer_Obj::instId

Peripheral instance id

◆ magic

Enet_Magic EnetPer_Obj::magic

Peripheral initialization magic

◆ physAddr

uint64_t EnetPer_Obj::physAddr

Peripheral's physical address. Used for peripherals that have registers that are not part of any module (i.e. peripherals that have a wrapper subsystem). It can be set to 0 for peripherals that don't have have additional registers other than those of their modules.

◆ virtAddr

void* EnetPer_Obj::virtAddr

Peripheral's virtual address

◆ physAddr2

uint64_t EnetPer_Obj::physAddr2

Peripheral's second physical address, if needed

◆ virtAddr2

void* EnetPer_Obj::virtAddr2

Peripheral's second virtual address, if needed

◆ features

uint32_t EnetPer_Obj::features

Peripheral features

◆ errata

uint32_t EnetPer_Obj::errata

Peripheral applicable errata

◆ initCfg

EnetPer_InitCfg EnetPer_Obj::initCfg

Pointer to the EnetPer config initialization function

◆ open

EnetPer_Open EnetPer_Obj::open

Pointer to the EnetPer open function

◆ rejoin

EnetPer_Rejoin EnetPer_Obj::rejoin

Pointer to the EnetPer rejoin function

◆ ioctl

EnetPer_Ioctl EnetPer_Obj::ioctl

Pointer to the EnetPer ioctl function

◆ poll

EnetPer_Poll EnetPer_Obj::poll

Pointer to the EnetPer poll function

◆ convertTs

EnetPer_ConvertTs EnetPer_Obj::convertTs

Pointer to the EnetPer timestamp conversion function

◆ periodicTick

EnetPer_PeriodicTick EnetPer_Obj::periodicTick

Pointer to the EnetPer periodic tick function

◆ registerEventCb

EnetPer_RegisterEventCb EnetPer_Obj::registerEventCb

Pointer to the EnetPer register event callback function

◆ unregisterEventCb

EnetPer_UnregisterEventCb EnetPer_Obj::unregisterEventCb

Pointer to the EnetPer unregister event callback function

◆ close

EnetPer_Close EnetPer_Obj::close

Pointer to the EnetPer close function