OSPI Driver SFDP API/interface file.
Go to the source code of this file.
Data Structures | |
struct | OSPI_SfdpMainHeader |
struct | OSPI_SfdpParamHeader |
struct | OSPI_SfdpBasicFlashParamTable |
struct | OSPI_SfdpXspiProfile1ParamTable |
struct | OSPI_SfdpSectorMapParamTable |
struct | OSPI_SfdpSCCRParamTable |
struct | OSPI_Sfdp4ByteAddressingParamTable |
struct | OSPI_SfdpHeader |
OSPI SFDP Structure. More... | |
Functions | |
char * | OSPI_Sfdp_getParameterTableName (uint32_t paramTableId) |
This function returns the name of the parameter table given the table ID. More... | |
uint32_t | OSPI_Sfdp_getPtp (OSPI_SfdpParamHeader *paramHeader) |
This function returns the Parameter Table Pointer (PTP) of the parameter table given the parameter header. More... | |
int32_t | OSPI_Sfdp_parseBfpt (OSPI_SfdpBasicFlashParamTable *bfpt, OSPI_GenericXspiDevDefines *xspiDefines, uint32_t numDwords) |
This function parses the Basic Flash Parameter Table (BFPT) and fills the xspiDevDefines structure with the parsed information. More... | |
int32_t | OSPI_Sfdp_parseXpt1 (OSPI_SfdpXspiProfile1ParamTable *xpt1, OSPI_GenericXspiDevDefines *xspiDefines, uint32_t numDwords) |
This function parses the xSPI Flash Profile 1.0 Table and fills the xspiDevDefines structure with the parsed information. More... | |
int32_t | OSPI_Sfdp_parse4bait (OSPI_Sfdp4ByteAddressingParamTable *fourBait, OSPI_GenericXspiDevDefines *xspiDefines, uint32_t numDwords) |
This function parses the 4 Byte Addressing Information Table (4BAIT) and fills the xspiDevDefines structure with the parsed information. More... | |
int32_t | OSPI_Sfdp_parseSccr (OSPI_SfdpSCCRParamTable *sccr, OSPI_GenericXspiDevDefines *xspiDefines, uint32_t numDwords) |
This function parses the Status, Control and Configuration Registers (SCCR) Table and fills the xspiDevDefines structure with the parsed information. More... | |
int32_t | OSPI_Sfdp_parseSmpt (OSPI_SfdpSectorMapParamTable *smpt, OSPI_GenericXspiDevDefines *xspiDefines, uint32_t numDwords) |
This function parses the Sector Map Parameter Table (SMPT) and fills the xspiDevDefines structure with the parsed information. More... | |