|
MSP DSP Library
|
Parameter structure for LEACMD__IIRBQ1 command. More...
#include <DSPLib_lea.h>
Data Fields | |
| uint16_t | vectorSizeBy2 |
| Length of data vector divided by two. | |
| uint16_t | output |
| Output data vector. | |
| uint16_t | state |
| Biquad state structure. | |
| uint16_t | coeffs |
| Biquad coefficient structure. | |
| uint16_t | direction |
| Input increment direction. | |
| uint16_t | reserved |
| Reserved padding. | |
Parameter structure for LEACMD__IIRBQ1 command.