|
MSP DSP Library
|
Parameter structure for the real matrix multiply function. More...
#include <DSPLib_matrix.h>
Data Fields | |
| uint16_t | srcARows |
| Number of rows in source A matrix, must be a multiple of two. | |
| uint16_t | srcACols |
| Number of columns in source A matrix, must be a multiple of two. | |
| uint16_t | srcBRows |
| Number of rows in source B matrix, must be a multiple of two. | |
| uint16_t | srcBCols |
| Number of columns in source B matrix, must be a multiple of two. | |
Parameter structure for the real matrix multiply function.