CC13xx Driver Library
OscHfGlobals_t Struct Reference

Data Fields

uint32_t previousStartupTimeInUs
 
uint32_t timeXoscOff_CV
 
uint32_t timeXoscOn_CV
 
uint32_t timeXoscStable_CV
 
int32_t tempXoscOff
 

Field Documentation

uint32_t OscHfGlobals_t::previousStartupTimeInUs
int32_t OscHfGlobals_t::tempXoscOff
uint32_t OscHfGlobals_t::timeXoscOff_CV
uint32_t OscHfGlobals_t::timeXoscOn_CV
uint32_t OscHfGlobals_t::timeXoscStable_CV